Defines all error handling strctures and macro.
Go to the source code of this file.
Macros | |
#define | DCL_clearError(ptr) ((ptr)->css->err = dcl_none) |
Macro to clear stored error code in CSS. More... | |
#define | DCL_setError(ptr, code) ((ptr)->css->err |= code) |
Macro to set error code in CSS. More... | |
#define | DCL_getErrorLine(ptr) ((ptr)->css->err_line = ((ptr)->css->err) ? __LINE__ : 0) |
Macro to store line location of error in CSS. More... | |
#define | DCL_getErrorFunc(ptr) ((ptr)->css->err_func = ((ptr)->css->err) ? __FUNCTION__ : NULL) |
Macro to store function location of error in CSS. More... | |
#define | DCL_getErrorInfo(ptr) |
Macro to store error info in CSS. More... | |
#define | DCL_runErrorHandler(ptr) |
Prototype for basic error handler. More... | |
Enumerations | |
enum | DCL_error_codes { dcl_none = 0U, dcl_param_range_err = (1U << 0), dcl_param_invalid_err = (1U << 1), dcl_param_warn_err = (1U << 2), dcl_input_range_err = (1U << 3), dcl_overflow_err = (1U << 4), dcl_underflow_err = (1U << 5), dcl_controller_err = (1U << 6), dcl_timing_err = (1U << 7), dcl_comp_err = (1U << 8) } |
Defines the library enumerated error codes. These will be applied as bit masks in the error handler. More... | |