AM243x Motor Control SDK  09.01.00
SDFM_Ctrl Struct Reference

Detailed Description

Structure defining SDFM control fields.

Firmware control & status interface exposed through PRU data
memory - used by driver to enable SDFM operations and to select
between continuous and triggered mode

Data Fields

volatile uint8_t sdfm_en
 
volatile uint8_t sdfm_en_ack
 
volatile uint8_t sdfm_pru_id
 

Field Documentation

◆ sdfm_en

volatile uint8_t SDFM_Ctrl::sdfm_en

< SDFM Enable SDFM Enable Ack

◆ sdfm_en_ack

volatile uint8_t SDFM_Ctrl::sdfm_en_ack

SDFM PRU ID

◆ sdfm_pru_id

volatile uint8_t SDFM_Ctrl::sdfm_pru_id