AM243x Motor Control SDK  09.00.00
SDFM_ThresholdParms Struct Reference

Detailed Description

Structure defining SDFM thresholds parametrs.

High, Low & zero cross thresholds for sdfm channel

Data Fields

volatile uint32_t high_threshold
 
volatile uint32_t low_threshold
 
volatile uint32_t reserved3
 

Field Documentation

◆ high_threshold

volatile uint32_t SDFM_ThresholdParms::high_threshold

< High threshold value Low threshold value

◆ low_threshold

volatile uint32_t SDFM_ThresholdParms::low_threshold

reserved for zero crossing

◆ reserved3

volatile uint32_t SDFM_ThresholdParms::reserved3