Structure defining SDFM control fields.
Firmware control & status interface exposed through PRU data
memory - used by driver to enable SDFM operations and to select
between continuous and triggered mode
Data Fields | |
volatile uint8_t | sdfm_en |
volatile uint8_t | sdfm_en_ack |
volatile uint8_t | sdfm_pru_id |
volatile uint8_t SDFM_Ctrl::sdfm_en_ack |
SDFM PRU ID
volatile uint8_t SDFM_Ctrl::sdfm_pru_id |