Go to the source code of this file.
Functions | |
int32_t | endat_recvd_process (struct endat_priv *priv, int32_t cmd, union endat_format_data *u) |
process raw recieved data and format based on the command More... | |
uint32_t | endat_recvd_validate (struct endat_priv *priv, int32_t cmd, union endat_format_data *u) |
CRC result indicated in return value as follows, 0th bit high position/address/params/test CRC success 0th bit low position/address/params/test CRC failure 1st bit high if addinfo 1 present, addinfo 1 CRC success 1st bit low if addinfo 1 present, addinfo 1 CRC failure 2nd bit high if addinfo 2 present, addinfo 2 CRC success 2nd bit low if addinfo 2 present, addinfo 2 CRC failure. More... | |
int32_t | endat_command_process (struct endat_priv *priv, int32_t cmd, struct cmd_supplement *cmd_supplement) |
send the EnDat command and wait till firmware acknowledges More... | |
int32_t | endat_command_build (struct endat_priv *priv, int32_t cmd, struct cmd_supplement *cmd_supplement) |
setup the EnDat command in the PRU interface buffer More... | |
void | endat_command_send (struct endat_priv *priv) |
trigger sending the EnDat command in PRU More... | |
void | endat_command_wait (struct endat_priv *priv) |
wait till PRU finishes EnDat transaction More... | |
uint32_t | endat_get_recovery_time (struct endat_priv *priv) |
read RT from DMEM More... | |
int32_t | endat_get_encoder_info (struct endat_priv *priv) |
update priv with position resolution, id, serial number, encoder type and supported command set More... | |
uint32_t | endat_get_prop_delay (struct endat_priv *priv) |
get propagation delay automatically estimated by the firmware More... | |
void | endat_addinfo_track (struct endat_priv *priv, int32_t cmd, struct cmd_supplement *cmd_supplement) |
track presence of additional information in priv More... | |
void | endat_config_clock (struct endat_priv *priv, struct endat_clk_cfg *clk_cfg) |
configure EnDat clock More... | |
void | endat_config_tst_delay (struct endat_priv *priv, uint16_t delay) |
configure tST delay More... | |
void | endat_config_rx_arm_cnt (struct endat_priv *priv, uint16_t val) |
configure rx arm counter More... | |
void | endat_config_wire_delay (struct endat_priv *priv, uint16_t val) |
configure wire delay for the selected channel More... | |
void | endat_config_rx_clock_disable (struct endat_priv *priv, uint16_t val) |
configure clocks to be disabled at the end of rx to account for tD More... | |
int32_t | endat_start_continuous_mode (struct endat_priv *priv) |
start continuous mode More... | |
void | endat_stop_continuous_mode (struct endat_priv *priv) |
stop continuous mode More... | |
void | endat_config_host_trigger (struct endat_priv *priv) |
configure EnDat master for host trigger mode More... | |
void | endat_config_periodic_trigger (struct endat_priv *priv) |
configure EnDat master in periodic trigger mode More... | |
void | endat_config_syn_bits (struct endat_priv *priv, uint8_t mask) |
void | endat_config_primary_core_mask (struct endat_priv *priv, uint8_t mask) |
set a core as primay core for global configuration, clk configuration and TX_GLOBAL_INIT More... | |
void | endat_enable_load_share_mode (struct endat_priv *priv) |
enable load share mode if encoders has diffent make More... | |
void | endat_config_channel (struct endat_priv *priv, int32_t ch) |
select channel to be used by EnDat master More... | |
void | endat_config_multi_channel_mask (struct endat_priv *priv, uint8_t mask, uint8_t loadshare) |
select mask of channels to be used in multi channel configuration by EnDat master More... | |
uint8_t | endat_multi_channel_detected (struct endat_priv *priv) |
select channels detected in multi channel configuration by EnDat master. required to be invoked only if firmware indicates initialization failure to know the channels that has been detected. Initialization success implies that all channels indicated has been detected. More... | |
void | endat_multi_channel_set_cur (struct endat_priv *priv, int32_t ch) |
In multi channel configuration, select channel before receive processing in multi channel configuration. After receive is complete, select each channel and invoke rx API's to parse data recieved in each channel. More... | |
int32_t | endat_wait_initialization (struct endat_priv *priv, uint32_t timeout, uint8_t mask) |
wait for EnDat master firmware to initialize More... | |
struct endat_priv * | endat_init (struct endat_pruss_xchg *pruss_xchg, void *pruss_cfg, void *pruss_iep, int32_t slice) |
Initialize EnDat firmware interface address and get the pointer to struct endat_priv instance. More... | |
int32_t | endat_get_2_2_angle (struct endat_priv *priv) |
Read EnDat 2.2 angular position in steps for rotary encoders (prior to invoking this, 2.2 position command has to be completed) This checks the CRC status (updated on-the-fly by firmware), checks the group alarm errors (F1/F2 bits) and the angle value recieved in reverse are reversed in a highly optimized way using inline assembly. Assumptions (that holds good for quite a few encoders): More... | |