AM243x Motor Control SDK  09.00.00
cmd_supplement Struct Reference

Data Fields

uint32_t address
 
uint32_t data
 
uint32_t block
 
uint8_t has_block_address
 
uint32_t frequency
 
uint64_t cmp3
 
uint64_t cmp5
 
uint64_t cmp6
 

Field Documentation

◆ address

uint32_t cmd_supplement::address

◆ data

uint32_t cmd_supplement::data

◆ block

uint32_t cmd_supplement::block

◆ has_block_address

uint8_t cmd_supplement::has_block_address

◆ frequency

uint32_t cmd_supplement::frequency

◆ cmp3

uint64_t cmd_supplement::cmp3

◆ cmp5

uint64_t cmd_supplement::cmp5

◆ cmp6

uint64_t cmd_supplement::cmp6