AM263Px INDUSTRIAL COMMUNICATIONS SDK  2026.00.00
EtherCAT SubDevice FWHAL

Introduction

This software is designed for the TI SoCs with PRU-ICSS IP to enable customers add EtherCAT SubDevice protocol support to their system. It implements EtherCAT SubDevice Controller(ESC) Layer 2 functionality with two MII ports (one IN and one OUT port per PRU-ICSS) in accordance with ETG.1000.4 Data Link Layer protocol specification. This provides EtherCAT ASIC like functionality integrated into TI SoCs.

Software Architecture

EtherCAT firmware for PRU-ICSS is a black box product maintained by TI. EtherCAT SubDevice FWHAL(Firmware and Hardware Abstraction Layer) allows loading and running the EtherCAT firmware and acts as an interface with ESC firmware. FWHAL implements the key interface between EtherCAT SubDevice Controller Emulation firmware and EtherCAT stack.

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

SysConfig can be used to configure things mentioned below:

  • Selecting the PRU-ICSS instance
  • Configuring PINMUX needed for MII mode
  • Configuring ETHPHY for the two PHY ports of PRU-ICSS
  • Configuring Enhanced Link Detection

PRU-ICSS EtherCAT SubDevice Firmware

Features Supported

  • All EtherCAT Commands (NOP, APRD, APWR, APRW, FPRD, FPWR, FPRW, BRD, BWR, BRW, LRD, LWR, LRW, ARMW and FRMW)
  • 8 FMMU support
  • 8 SM support
  • 28KB of Process Data RAM
  • Distributed clocks
    • 64-bit DC
    • SYNC0 out generation single shot and cyclic mode support
    • SYNC1 out generation
      • SYNC1 cycle time multiple of SYNC0 cycle time
      • SYNC1 shift with respect to SYNC0
    • Latch0 and Latch1 inputs
    • System Time PDI control
  • DL Loop Control
    • Using MII_RX_LINK (fast - depending on PHY link loss detection latency) - mandatory for cable redundancy support
    • Using PRU-ICSS MDIO state machine - not recommended for cable redundancy support
  • Interrupts - AL/ECAT events
    • SYNC0, SYNC1 and PDI interrupt events on external SOC pins
  • Watchdog - PDI and SM
  • Error Counters
    • RX Invalid Frame Counter Port 0/1
    • RX ERR Counter Port 0/1
    • Forwarded Error Counter Port 0/1
    • ECAT Processing Unit Error Counter
  • LED - Run, Error and Port0/1 activity
  • EEPROM Emulation for ESI EEPROM support
  • Management Interface for PHY over EtherCAT
  • PHY address configuration and host side API for PHY programming
  • Cable redundancy support
  • Firmware supports the following clock configuration:
    • PRU-ICSS Core Clock Frequency: 200 MHz
    • IEP Clock Frequency: 200 MHz

Key Performance Parameters

Sync Jitter measurement done using TwinCAT 3.1 along with C6015-0020 (Beckhoff PLC) for PRU core running at 200MHz.

Feature Detail Value
Distributed Clock Sync Jitter 15.5ns (at 50μs cycle time running for 12 hours)
Latency Process Path Average = 426ns, Max = 440ns
Auto Forward Path (Reverse Path) Average = 326ns, Max = 340ns

Release Notes

Industrial Communications SDK Version 2026.00.00

  • Firmware Version : x.5.79
  • Fix for PINDSW-8517: When SYNC1 shift is configured, the SubDevice generates first SYNC1 pulse after 1 cycle of SYNC0 signal has elapsed.
  • PINDSW-9805: Optimize Time required to update ICSSG1 IEP0 CMP1 in DC synchronous mode

Industrial Communications SDK Version 2025.00.01

  • Firmware Version : x.5.72
  • Fix for PINDSW-9560 : TX_START_DELAY reset to default value when link broken and re-connected to the network during OP
  • Fix for PINDSW-9756 : CRC/Alignment Error observed when one SubDevice set to INIT after link re-connection
  • Fix for PINDSW-9787 : CRC Error for 8SM application individual SubDevice state transition to INIT
  • Fix for PINDSW-9821 : Malformed packet formation for 1 byte mailbox data communication due to cycle budget
  • Fix for PINDSW-9883 : PDO misalignment due to start offset in FMMU merge logic for LRD/LWR

Industrial Communications SDK Version 2025.00

  • Firmware Version : x.5.66
  • Fix for PINDSW-8527 : Sync Jitter mismatch when Continuous Sync Monitoring enabled in Acontis based MainDevices
  • Fix for PINDSW-9148 : Optimize MBX Write (FPWR) Path
  • Fix for PINDSW-9284 : Malformed packets observed in CTT (Conformance Test Tool) when using more than 4 SyncManagers
  • Fix for PINDSW-9412 : Sync0 drift happening after a month of continuous run
  • Fix for PINDSW-9565 : Incorrect length computation for SM Write

Industrial Communications SDK Version 10.02

  • Firmware Version : x.5.55
  • Fix for PINDSW-9140 : Use MDIO link interrupt along with MII Link interrupt for link detection
  • Fix for PINDSW-8428 : Configure SYNC1 Shift with respect to SYNC0 signal
  • Fix for PINDSW-8429 : Optimizing Host Handshake During Redundant State Change, that is, if the Main Device sets the Subdevice to its current state (no actual state change), the host handshake is skipped to optimize communication.

Industrial Communications SDK Version 10.00

  • Firmware Version : x.5.50
  • Fix for PINDSW-47 : Single datagram accessing multiple FMMU mapped areas using LRD/LWR commands from a single SubDevice.
    • Do note that if this feature is enabled, then the Process Path latency will be dynamically increased to take care of the timing constraints. Please refer to Register 0xED0 of Vendor Specific Register in TI EtherCAT SubDevice Controller Register List
  • Fix for PINDSW-141 : LRW access to non-interleaved input and output process data of multiple SubDevices does not work.
    • This will make EtherCAT SubDevice compatible with default mode of few open source EtherCAT MainDevice like SOEM and IgH.
    • Do note that if this feature is enabled, then the Process Path latency will be dynamically increased to take care of the timing constraints. Please refer to Register 0xED0 of Vendor Specific Register in TI EtherCAT SubDevice Controller Register List
  • Bug-fix for PINDSW-8246 : Triple buffer issue - Not getting the latest data from buffer during free-run mode.
  • Bug-fix for PINDSW-8115 : Watchdog error while using LRD and LWR with same logical address.

Features Not Supported

  • EtherCAT SubDevice Controller
    • ECAT side register protection when using LRD command
    • APRW/FPRW/BRW for SM mapped area
  • EtherCAT G
  • Reset Isolation

Known Issues

Record ID Details Workaround
PINDSW-72 PDI/PD watchdog counter incremented by 1 whenever PDI/PD watchdog is disabled None
PINDSW-74 LRD access on unused registers increment WKC - no register protection while using LRD None
PINDSW-2204 Frames with no SFD not counted as errors if received on reverse path None
PINDSW-2360 System time of next Sync0 pulse register (0x990:0x993) is not instantaneous, resulting in read of incorrect value if read immediately after sync pulse None
PINDSW-5135 Read permissions and byte level write permissions for RW type commands are not checked None
PINDSW-5145 RX_ER counter does not count errors outside frame in MII RX_CLK units precisely Added PHY RX Error Counter Register (0x0E28) for improving RX Error Counter accuracy. Configuring this register will track RX_ERs within a frame precisely using PHY registers. Refer Register Exceptions for more details.
PINDSW-5414 Link Lost Counter is incorrectly incremented once for ports with polarity of RXLINK input as “Active Low” during initialization Use Active High Polarity for LED_LINK/SPEED connected to MII0/MII1 Receive Link (RXLINK) pin of PRU-ICSS

For more details, please see the EtherCAT SubDevice Errata document.

How MDIO Works for Link Detection

In EtherCAT networks, fast detection of link status changes is crucial to maintain real-time communication and network integrity. MDIO enables the processor to read status registers from connected PHYs, allowing the system to:

  • Detect link up/down events.
  • Monitor PHY status.
  • Configure PHY settings as needed. This information is vital for the EtherCAT SubDevice Controller (ESC) to manage port states and ensure timely data transmission. The MDIO interface communicates with external PHYs using the standard IEEE 802.3 Clause 22 protocol. Each PHY on the board is connected to the MDIO bus and is accessible via a unique PHY address The MDIO module allows communication with a wide range of PHYs with some of the following features:
  • PHY Addressing: Each PHY is assigned a unique address (0–31) on the MDIO bus.
  • Clock Configuration: The MDIO clock (MDC) must be configured to operate within the PHY’s specified frequency range.
  • Register Access: The MDIO Module reads and writes to the PHY Register for EtherCAT specific requirements to determine link status and enable other functionalities. In scenarios where a port was never connected, the ESC may keep it in an “ALWAYS CLOSED” state until a valid link is detected via MDIO. This behavior ensures that the ESC only activates ports with confirmed physical connections, preventing potential communication issues. The MDIO Alive Register (MDIO_ALIVE_REG) indicates the status of the PHY along with the corresponding MDIO PHY Address. The MDIO Link Register indicates whether a valid link is detected on the corresponding PHY Address.

Please refer to Section 6.4.12 and Section 6.4.14.10 of the AM64x/AM243x Technical Reference Manual

Fast Link Detection Mechanism

To meet the stringent timing requirements of EtherCAT networks, the AM64x/AM243x platforms implement a fast link detection mechanism using the MDIO MLINK signal. This approach bypasses the standard state machine, allowing for quicker detection of link changes (10µs), which is essential for maintaining low-latency communication and effective cable redundancy. Refer to Enhanced Link for more details.

EtherCAT Firmware Migration guide

If your project is based on an older SDK and if you want to upgrade to the latest EtherCAT PRU firmware, follow the steps outlined below to ensure a smooth transition with minimal disruption to your existing codebase and system behavior:

  • The latest EtherCAT firmware can be taken from latest SDK released.
  • Copy the ecat_frame_handler_bin.h and ecat_host_interface_bin.h from {SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice/icss_fwhal/firmware/m_v2.3/ and replace the same in the SDK you are using.
  • Once the new firmware headers are in place, rebuild the libraries by running the FWHAL makefile, for example, gmake -s -f makefile.am243x.r5f.ti-arm-clang (for RELEASE build) and gmake -s -f makefile.am243x.r5f.ti-arm-clang PROFILE=debug (for DEBUG build) at {SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice/icss_fwhal/ for your corresponding device. Post this, you can rebuild the application to apply the latest FW changes.

Important Files and Directory Structure

Folder/Files Description
${SDK_INSTALL_PATH}/examples/industrial_comms
ethercat_subdevice_beckhoff_ssc_demo EtherCAT SubDevice Example based on Beckhoff SSC
${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice
icss_fwhal/firmware/m_v2.3 Firmware for the PRU cores in PRU-ICSS. Firmware Version : 5.5.79
icss_fwhal/lib/ FWHAL library for EtherCAT SubDevice
icss_fwhal/tiescbsp.h FWHAL interface file
beckhoff_stack/esi ESI XML file for Beckhoff SubDevice Stack Code(SSC) based example
beckhoff_stack/patch Patch file for Beckhoff SubDevice Stack Code(SSC) sources
beckhoff_stack/stack_hal Stack adaptation APIs for Beckhoff SubDevice Stack Code(SSC)
beckhoff_stack/stack_sources Folder where Beckhoff SubDevice Stack Code(SSC) sources should be copied. Stack sources are not packaged in the SDK

API Documentation

Please see APIs for Ethercat SubDevice FWHAL for API documentation.

It is recommended to use these FWHAL APIs in the stack adaptation files. For example, see ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice/beckhoff_stack/stack_hal, which contains the stack adaptation APIs for Beckhoff SubDevice Stack Code(SSC).

Procedure to kick-off the EtherCAT SubDevice Controller(ESC)

  • Initialize memories (register protection, register reset values, EEPROM cache) and PRU-ICSS INTC module. This is done by FWHAL(Firmware and Hardware Abstraction Layer).
  • Load firmware into PRUs of PRU-ICSS. This is done by FWHAL.
  • Enable the PRU cores. This is done by FWHAL.
  • Initialize the EtherCAT SubDevice stack.
  • Wait for AL Event Request and SYNC (in DC synchronous mode) interrupts from PRU and run EtherCAT stack main loop for handling mailbox and ESC state machine.
  • Handle the events as needed. Note that this is handled by the stack.

Hardware Requirements

  • Sitara Processor with PRU-ICSS IP and EtherCAT support
  • Current implementation uses only Spinlock 0. Spinlocks 1 to 7 are free for use.
  • HW signals required to implement EtherCAT subdevice functionality is shown below, this info needs to be used in conjunction with SYSCONFIG:
Note
Important - PRU MII TX Pin Mapping: The PRU-ICSS MII TX pins in AM65x and subsequent SoC families (AM64x, AM243x, AM263x, etc.) were physically swapped during SoC integration compared to the original PRU hardware definition shown in some TRM diagrams. This was done intentionally to simplify PCB routing. The SDK firmware is designed to work with this swapped pin configuration. You must use the SYSCONFIG-generated PRU pin mapping to ensure compatibility with the SDK firmware. Using pin mappings directly from TRM block diagrams without accounting for this swap will result in non-functional Ethernet communication.
Signal Name Requirement

Description

PRU-ICSS MDIO
PR0_MDIO0_MDC Mandatory MDIO clock
PR0_MDIO0_MDIO Mandatory MDIO Data
PRU-ICSS Distributed Clocks (Network Clock synchronization)
PR0_IEP0_EDC_SYNC_OUT0 Recommmended (for DC capable SubDevices) SYNC0 out - Time synchronized OUT0
PR0_IEP0_EDC_SYNC_OUT1 Optional (depends on customer application)) SYNC1 out - Time synchronized OUT1 (depends on SYNC0)
PRU-ICSS MII PDI Interrupt
PR0_IEP0_EDIO_DATA_IN_OUT30 Optional PDI ISR output to external SOC pin (via one of the 2 PRU-ICSS digio outputs).
PDI ISR pin can be selected via vendor specific register at offset 0xE0A.

PR0_IEP0_EDIO_DATA_IN_OUT31

PRU-ICSS MII Port0 (IN Port) & PRU-ICSS MII Port1 (OUT Port)
MII0_RXD0 Mandatory MII0 and MII1 Receive Data0
MII1_RXD0
MII0_RXD1 Mandatory MII0 and MII1 Receive Data1
MII1_RXD1
MII0_RXD2 Mandatory MII0 and MII1 Receive Data2
MII1_RXD2
MII0_RXD3 Mandatory MII0 and MII1 Receive Data3
MII1_RXD3
MII0_RXDV Mandatory MII0 and MII1 RX Data Valid
MII1_RXDV
MII0_RXER Optional if PHY supports Enhanced Link detection MII0 and MII1 RXERR
MII1_RXER
MII0_TXD0 Mandatory MII0 and MII1 Transmit Data0
MII1_TXD0
MII0_TXD1 Mandatory MII0 and MII1 Transmit Data1
MII1_TXD1
MII0_TXD2 Mandatory MII0 and MII1 Transmit Data2
MII1_TXD2
MII0_TXD3 Mandatory MII0 and MII1 Transmit Data3
MII1_TXD3
MII0_TXEN Mandatory MII0 and MII1 TX enable
MII1_TXEN
MII0_RXCLK Mandatory MII0 and MII1 Receive clock
MII1_RXCLK
MII0_TXCLK Mandatory MII0 and MII1 Transmit clock
MII1_TXCLK
MII0_RXLINK Mandatory for cable redundancy support Enhanced link detection. Redundancy support: connect LED_LINK/LED_SPEED from PHY here

MII1_RXLINK

Interrupts

EtherCAT SubDevice Controller firmware generates the following interrupts.

8 Host Interrupts (Host Interrupts 2 through 9) are exported from the PRU_ICSSG internal INTC for signaling the device level interrupt controllers. PRU_EVTOUT0 to PRU_EVTOUT7 correspond to these eight interrupts in the following table. Please check PRUICSS Interrupt Controller section for more details.

Name Host Interrupt Description
DC SYNC0 OUT PRU_EVTOUT1 Used in DC mode for syncing the application
DC SYNC1 OUT PRU_EVTOUT2 Used in DC mode for syncing the application
PDI Interrupt PRU_EVTOUT3 AL event/PDI interrupt to host stack
ESC Command Acknowledgement PRU_EVTOUT4 ESC firmware command completion acknowledgement to Host

PRU-ICSS Resource Usage

This section describes the PRU-ICSS hardware resources used by the EtherCAT SubDevice firmware.

PRU Firmware Memory Map

The EtherCAT SubDevice firmware runs on two PRU cores within the PRU-ICSS subsystem:

  • PRU0 (Frame Handler): Handles EtherCAT frame processing at wire speed.
  • PRU1 (Host Interface): Handles ESC register access, host commands, and event signaling.

PRU Instruction RAM (IRAM):

Resource Total Size Used (AM64x / AM243x) Used (AM263x / AM263Px / AM261x) Contents
PRU0 IRAM 12 kB (0x3000) 9320 bytes 9276 bytes Frame Handler firmware (ecat_frame_handler_bin.h)
PRU1 IRAM 12 kB (0x3000) 10708 bytes 9876 bytes Host Interface firmware (ecat_host_interface_bin.h)

PRU Data RAM (DMEM):

Resource Size PRU-local Base Contents
PRU0 DMEM (DMEM0) 8 kB 0x00000000 Host–PRU command interface, system time mirrors, SM state flags
PRU1 DMEM (DMEM1) 8 kB 0x00002000 (from PRU0 view) ESC register write shadow (1 kB) and register permission/protection table (4 kB)

Key layout within PRU0 DMEM:

Offset Size Description
0x0000 – 0x008F 144 B System state (reserved)
0x0090 – 0x0093 4 B System Time Low mirror
0x0094 – 0x0097 4 B System Time High mirror
0x00A0 – 0x00A1 2 B Command register (cmdlow)
0x00A2 – 0x00A3 2 B Command ACK register
0x00A4 – 0x00A5 2 B Command Parameter 1
0x00A6 – 0x00A7 2 B Command Parameter 2
0x00A8 – 0x00A9 2 B Command Response 1
0x00AA – 0x00AB 2 B Command Response 2
0x00EC – 0x00F7 12 B SM process data array (6 × 4 B)
0x0500 – 0x0529 42 B Sync Permission Update registers

Shared RAM:

Resource Size PRU-local Base Contents
Shared RAM 32 kB 0x00010000 EtherCAT process data RAM, ESC emulation registers, FMMU/SM working area

INTC (Interrupt Controller)

The PRU-ICSS INTC is mapped at PRU-local address 0x00020000. The EtherCAT firmware configures the following system events:

System Events:

Event Direction Description
IEP Timer/Capture/Compare IEP → PRU1 IEP timer event (DC synchronization, SYNC pulse timing)
PD Watchdog Expiry ESC → PRU1 Process data watchdog expired
PDI Watchdog Expiry ESC → PRU1 PDI watchdog expired
Latch0 Input External → PRU1 Latch0 timestamp capture trigger
Latch1 Input External → PRU1 Latch1 timestamp capture trigger
SYNC0 Output PRU → ARM DC SYNC0 pulse (exported as PRU_EVTOUT1)
SYNC1 Output PRU → ARM DC SYNC1 pulse (exported as PRU_EVTOUT2)
SYS_EVT_HOST_CMD ARM → PRU1 Host-to-firmware command trigger
SYS_EVT_HOST_CMD_LOW ARM → PRU1 Host-to-firmware low-priority command
SYS_EVT_AL_EVENT_REQUEST PRU → ARM AL event / PDI ISR (exported as PRU_EVTOUT3)
SYS_EVT_HOST_CMD_LOW_ACK PRU → ARM Firmware command completion ACK (exported as PRU_EVTOUT4)
PRU0/PRU1 RX Error / Overflow MII → PRU MII receive error and overflow events
MII Link0 / Link1 Event MDIO → PRU Port link state change events

INTC Channel Mapping:

Channel Host Interrupt Description
0 PRU0 internal PRU0 self-interrupt
1 PRU1 internal PRU1 self-interrupt (IEP, watchdog, link, latch events)
2 PRU_EVTOUT0 Unused
3 PRU_EVTOUT1 DC SYNC0 OUT to ARM host
4 PRU_EVTOUT2 DC SYNC1 OUT to ARM host
5 PRU_EVTOUT3 AL Event / PDI ISR to ARM host
6 PRU_EVTOUT4 ESC Command ACK to ARM host
7–9 PRU_EVTOUT5–7 Unused

IEP (Industrial Ethernet Peripheral)

The IEP is the primary timing engine for the EtherCAT Distributed Clocks (DC) implementation. It is mapped at PRU-local address 0x0002E000.

IEP features used by EtherCAT firmware:

Feature IEP Register(s) Description
64-bit system time counter COUNT_REG (offset 0x10–0x17) DC time base; all EtherCAT timestamps are derived from this counter
Compare registers (CMP0–CMP7) CMP_CFG_REG (0x70), CMP0–CMP7 (0x78–0xB0) SYNC0 and SYNC1 pulse generation based on programmed start time and cycle time
Capture registers (CAPR0–CAPR7) CAP_CFG_REG (0x18), CAPR0–CAPR7 (0x20–0x68) Latch0 and Latch1 input event timestamping (rising/falling edge selectable)
DIGIO outputs IEP EDIO registers PDI ISR output to external SoC pin (selectable via vendor register 0xE0A)
Note
64-bit IEP counter support (SUPPORT_64BIT_IEP) is available on ICSS_G v1.0 and v1.3, providing sub-nanosecond DC sync jitter performance.

IEP clock frequency:

Configuration PRU Core Clock IEP Clock
Single configuration 200 MHz 200 MHz

The active IEP clock frequency is reported in vendor-specific ESC register 0xED1.

eCAP (Enhanced Capture Module)

The eCAP module is available within the PRU-ICSS subsystem at PRU-local address 0x00030000. It is defined in the PRU linker configuration but is not actively used by the EtherCAT SubDevice firmware. All latch timestamping and DC timing functionality is handled through the IEP capture and compare registers.

SoC Hardware Spinlock

The EtherCAT SubDevice FWHAL uses the SoC hardware spinlock module to protect shared memory regions accessed concurrently by the ARM host processor and the PRU firmware.

Spinlock Instance Used By Protected Region
Spinlock 0 EtherCAT FWHAL Latch0/Latch1 timestamp reads and other concurrent host/PRU shared memory accesses
Spinlocks 1–7 Available Free for custom application use

The spinlock base address is configured via bsp_params.spinlock_base_address during bsp_init(). Spinlock acquire/release is handled through bsp_hwspinlock_lock(0) and bsp_hwspinlock_unlock(0).

MII Real-Time (MII-RT)

The MII-RT configuration module is mapped at PRU-local address 0x00032000 and controls frame-level Ethernet timing parameters.

Parameter Register Description
TX_START_DELAY (Port 0) TXCFG0 Process path transmit start delay (default 0x48/360 ns at 200 MHz; 0x50/400 ns at 333 MHz)
TX_START_DELAY (Port 1) TXCFG1 Autoforward path transmit start delay (default 0x38/280 ns at 200 MHz; 0x30/240 ns at 333 MHz)
Note
When only one port is connected to an active network, TXCFG1 carries the process path delay and TXCFG0 carries the autoforward delay. The assignment of TXCFG0 and TXCFG1 can therefore be swapped depending on which port is physically connected.

Accessing PDI ISR and Sync0/Sync1 Timestamp

PDI ISR Timestamp

There is a vendor specific register which has the PDI ISR Timestamp:

Register Offset Bits Access Default Description
PDI ISR Time Register 0x0E2C 0-63 RW 0 Register captures the System time when PDI ISR is triggered.

Configuring PDI ISR Output to External Pin

You can map PDI ISR output to external SOC pin (via one of the PRU-ICSS digio outputs):

Pin

Register Value (0x0E0A)

<tr>
    <td>PR0_IEP0_EDIO_DATA_IN_OUT31</td>
    <td>0x80</td>
</tr>
<tr>
    <td>PR0_IEP0_EDIO_DATA_IN_OUT30</td>
    <td>0x40</td>
</tr>

  • Map the corresponding EDIO pin to an available external GPIO pin in SysConfig EtherCAT module.

SYNC0 and Sync1 Timestamps

For SYNC0 and SYNC1 timestamps, refer to the following registers:

  • System time of next SYNC0 pulse: Register 0x0990-0x0997
  • System time of next SYNC1 pulse: Register 0x0998-0x099F

These registers can be read to determine the exact timestamp when SYNC pulses occur, allowing for precise timing synchronization in your application.

Enhanced Link

  • This feature ensures that the link signal is checked every approximately 10 µs.
  • Enhanced MII link detection will additionally disconnect a link if at least 32 RX errors (RX_ER) occur in a fixed interval of ~10 μs. Refer to Section 5.6.2 of Hardware Data Sheet Section I for more details.
  • For this feature to work, enhancedlink_enable of bsp_params should be set to TIESC_MDIO_RX_LINK_ENABLE while initializing the EtherCAT SubDevice FWHAL. This configuration is done in tiesc_socParamsInit() in tiescsoc.c file. In the current implementation, this feature is enabled by default and configurable through the EtherCAT module in SysConfig for ease of use:

Syscfg EnhancedLink Configuration

Enhanced Link Detection Procedure

  • Firstly, make sure the PHY supports Enhanced Link capability.
  • Make sure RXLINK pin is connected properly.
  • For this feature to work, LED pin is to be configured correctly within the application. Refer to ETHPHY_DP83826E_LED0 configuration in tiesc_ethphyInit() in tiescsoc.c file.
  • Check PRU MDIO registers for the PHY alive and link status. Refer to Section 4.2.2.360.1 (MDIO_ALIVE_REG Register) and Section 4.2.2.361.1 (MDIO_LINK_REG Register) of AM26x Register Addendum.
  • MDIO_ALIVE_REG: Each of the 32 bits of this register is set if the most recent access to the PHY with address corresponding to the register bit number was acknowledged by the PHY, the bit is reset if the PHY fails to acknowledge the access. Both the user and polling accesses to a PHY will cause the corresponding alive bit to be updated. The alive bits are only meant to be used to give an indication of the presence or not of a PHY with the corresponding address. Check to see if the expected bits are set.
  • MDIO_LINK_REG: This register is updated after a read of the Generic Status Register of a PHY. The bit is set/reset if the PHY with the corresponding address has link and the PHY acknowledges the read transaction. Check to see if the expected bits are set.
    • Do note that this register is dependent on the link polarity if the EnhancedLink feature is enabled. If the bits in this register are getting reset while connecting to an active network, it implies the polarity is active low. If the bits in this register are getting set while connecting to an active network, it implies the polarity is active high. This needs to be configured for TIESC_LINK0_POL and TIESC_LINK1_POL in tiescsoc.c file. Vendor specific ESC Register ESC_ADDR_TI_PHY_LINK_POLARITY can also be used to identify the polarity.
  • Make sure that the set bit address is configured as MDIO Phy Address in Syscfg -> ETHPHY for the corresponding PHY instances. The configured PHY address can be seen in Vendor Specific ESC Register ESC_ADDR_TI_PORT0_PHYADDR and ESC_ADDR_TI_PORT1_PHYADDR.
    Syscfg PHY Configuration
  • Check the PHY status: The MDIO module includes a user access register (MDIO_USER_ACCESS_REG_j) to directly access a specified Phy. This is described in MDIO Register offset 0x80 of the TRM for Reading and Writing Data from/to a PHY Register
  • Check frame couter and error counter vendor specific registers: ESC Register 0x0300 (RX Error Counter) is to be monitored for RX errors and Vendor specific ESC Register ESC_ADDR_TI_PORT0_ACTIVITY and ESC_ADDR_TI_PORT1_ACTIVITY should be monitored for number of valid frames at Port0 and Port1 respectively.
  • Once successful, build and load the application and try scanning with TwinCAT or any other EtherCAT MainDevices.
  • Refer to Testing Cable Redundancy for testing this feature using TwinCAT.

TX_START_DELAY Behavior and Configuration

The TX_START_DELAY parameter is a critical timing configuration for EtherCAT SubDevices that affects network stability and performance. This section explains its purpose, behavior, and configuration options.

Purpose of TX_START_DELAY

TX_START_DELAY defines the time interval between receiving a frame (RXDV active) and when the SubDevice begins transmitting the processed frame to the MII interface. Refer to MII_RT_TXCFG0 Register (for AM243x/AM64x) or ICSSM_PR1_MII_RT_PR1_MII_RT_CFG_TXCFG0 (for AM263x/AM263Px/AM261x) in the corresponding TRM for more details. This delay is measured in MII_RT clock cycles and serves several important purposes:

  1. Providing sufficient time for processing EtherCAT commands within the frame
  2. Preventing timing issues that could result in malformed frames or communication errors
  3. Ensuring stable operation across different network topologies and cable lengths

TX_START_DELAY Configuration Registers

The TX_START_DELAY is configured through the following registers:

Register Offset Bits Access Default Value Description
Port0 TX Start Delay 0x0E10 0-15 RW 0x48/0x50 TX_START_DELAY for port 0. Modification from default values is not recommended.

NOTE: Each increment of 1 corresponds to 5ns. Default values are:
  • 0x48 (360ns) for PRU Clock at 200MHz
  • 0x50 (400ns) for PRU Clock at 333MHz
Port1 TX Start Delay 0x0E12 0-15 RW 0x38/0x30 TX_START_DELAY for port 1. Modification from default values is not recommended.

NOTE: Each increment of 1 corresponds to 5ns. Default values are:
  • 0x38 (280ns) for PRU Clock at 200MHz
  • 0x30 (240ns) for PRU Clock at 333MHz

The EtherCAT firmware automatically adjusts these TX_START_DELAY values based on the FMMU configuration received from the EtherCAT MainDevice.

Increased TX Start Delay Register

For complex FMMU configurations that require additional processing time, an increased TX_START_DELAY can be configured using:

Register Offset Bits Access Default Value Description
Increased TX Start Delay 0x0ED0 0-7 RW 0x98/0xA0 Configures the increased TX_START_DELAY for complex FMMU scenarios:
  • Single datagram accessing multiple FMMU mapped areas using LRD/LWR commands
  • LRW access to non-interleaved input and output process data
NOTE: Each increment of 1 corresponds to 5ns. Default values are:
  • 0x98 (760ns) for PRU Clock at 200MHz
  • 0xA0 (800ns) for PRU Clock at 333MHz

Scenarios Requiring Increased TX_START_DELAY

The firmware automatically detects the following scenarios and applies the increased TX_START_DELAY:

  1. Multiple FMMU Access (PINDSW-47): When a single LRD/LWR command accesses multiple FMMU-mapped memory regions, the processing time increases by approximately 400ns.
  2. Non-interleaved I/O Access (PINDSW-141): When LRW commands access non-interleaved input and output process data, the processing time increases by approximately 400ns. This configuration is required for compatibility with open source EtherCAT MainDevices like SOEM and IgH.

Dynamic TX_START_DELAY Adjustment

The EtherCAT firmware continuously monitors the FMMU configuration from the MainDevice and automatically adjusts the TX_START_DELAY as needed:

  • For standard FMMU configurations, the default TX_START_DELAY values (0x0E10, 0x0E12) are used
  • For complex FMMU configurations, the increased TX_START_DELAY value (0x0ED0) is applied

The value in register 0x0ED0 should be configured before the PRU cores start running. The default value of 0x98 (760ns) is suitable for most applications, but users can optimize this value for their specific network requirements.

Troubleshooting TX_START_DELAY Issues

If you observe malformed packets for LRD, LWR, or LRW datagrams in MainDevice logs or Wireshark captures, follow these steps:

  1. Check if the TX_START_DELAY is being properly increased by examining the MII_RT_TXCFG0 register:
Register Offset Bits Access Description
ICSSM_PR1_MII_RT_PR1_MII_RT_CFG_TXCFG0 0x48032010 for ICSSM0
0x48632010 for ICSSM1
16-25 RW TX_START_DELAY for port 0. Bits 16-25 show the current active delay value.
  • Note: TXCFG0 and TXCFG1 can be changed based on the number of ports connected to active network. If both the ports of the SubDevice is connected, TXCFG0 would have the process path (forward path) delay and TXCFG1 would have the autoforward delay (reverse path), and if only one port is connected, TXCFG1 would have the process path delay.
  1. If the register still shows the default value (0x48/360ns) but you're experiencing issues, you can force the increased TX_START_DELAY by:

EtherCAT SubDevice Controller(ESC) Register List

TI EtherCAT SubDevice Controller Register List contains descriptions of the registers in TI's EtherCAT SubDevice Controller implementation.

EtherCAT SubDevice Controller(ESC) Exceptions

TI EtherCAT SubDevice Controller Exceptions lists the exceptions TI's EtherCAT SubDevice Controller implementation when compared with ET1100 ASIC. Please note that TI ESC is a 2 port EtherCAT SubDevice and it does not support E-bus interface and all the corresponding register fields are not implemented.

Debug Guide

EtherCAT Debug Guide covers the most obvious use cases and debug scenarios encountered while using EtherCAT SubDevice.

Additional References

Please refer to below documents to understand more about EtherCAT SubDevice on TI platforms and EtherCAT SubDevice protocol specifications.

Document Description
EtherCAT on Sitara Processors Application note by TI on the EtherCAT SubDevice implementation on TI's Sitara Processors.
PRU-ICSS EtherCAT SubDevice Troubleshooting Guide This troubleshooting guide is intended to provide guidance on how to set up and debug the EtherCAT SubDevice implemented on TI's Sitara processors.
EtherCAT ESC Datasheet Section 1 - Technology Section 1 of Beckhoff's EtherCAT SubDevice Controller (ESC) documentation which describes basic EtherCAT technology.
EtherCAT ESC Datasheet Section 2 - Register Description Section 2 of Beckhoff's EtherCAT SubDevice Controller (ESC) documentation which contains ESC register descriptions.
Application Note ET9300 (EtherCAT SubDevice Stack Code) This contains details on how to start EtherCAT SubDevice development with SubDevice Stack Code.
EtherCAT SubDevice Implementation Guide from EtherCAT Technology Group This contains information on how to develop an EtherCAT SubDevice implementation.
EtherCAT SubDevice Design Quick Guide from Beckhoff This contains information on modifying PDO when using Beckhoff SSC Tool for code generation.

See also