It is highly recommended to go through EtherCAT SubDevice FWHAL page before proceeding with this page.
This page is meant to help the developer in
You can refer to Ethernet PHY Configuration Using MDIO for Industrial Applications for details on the required PHY configuration to the MDIO module.
Refer to Hardware Requirements for the hardware requirements required to run EtherCAT.
See CCS Launch, Load and Run page for details on how to load and run binaries on EVM or LP using CCS.
Most common issue observed is in cases where different PHYs (compared to those on EVM/LP) and the PHY status registers may be read incorrectly and that might lead to some issues.
The presence and responsiveness of the connected PHY on the MDIO bus is indicated by the MDIO_ALIVE_REG (offset 0x2408). The link detection is observed in MDIO_LINK_REG (at offset 0x240C). On the connection of an active network to the EtherCAT SubDevice using an ethernet cable, the bits corresponding to the PHY Address will be set/cleared based on the PHY link polarity. The polarity is to be followed when EnhancedLink feature is enabled.
Make sure that PHY Address is configured in such a way where if you see the bit getting set/reset when you connect the in/out port to an active network using Ethernet cable, then you should configure that particular bit address as the PHY Address of the corresponding port. This is important to configure the correct PHY Address for the IN port or the OUT port.
Do note that the PHY Address Configuration should be as per the corresponding board schematics, where the strap pin configuration can be referred to. The MDIOALIVE Register probes for a valid PHY.
Once this is disabled, the MDIO Registers should show the details and configurations for the connected PHY at the MDIO Register space (From 0x48032400 for ICSSM0 instance and 0x48632400 for ICSSM1 instance).
Following are some of the issues that were supported in order to bring-up the EtherCAT SubDevice on a custom HW or a different PHY:
| Issue | Probable Cause | Probable Fix (Couple of things to look on) |
|---|---|---|
| PHY is not able to detect the EtherCAT link. | MDIO is not able to access the PHY Registers. | Make sure the HW connections are correct and intact. |
| MII0_RXLINK and MII1_RXLINK signals are not connected properly. | Disable EnhancedLink and make sure MDIO Manual Mode Link Status Update is configured to PHY Polling Based. | |
| LED is not configured correctly to detect a stable LINK. | LED configuration has to be a stable LINK (LED_SPEED or LED_LINK (without activity blink)) | |
| Polarity of Link is not configured properly via the API. | Refer to Enhanced Link Detection Procedure on the procedure to configure the link polarity. Make sure IN and OUT ports are configured correctly based on the PHY Link status. | |
| PHY may not be getting the link status update. | Make sure the PHY is detecting by reading the BMSR Register of the PHY. | |
| MDIO Manual Mode is enabled and Enhanced Link detection is disabled but still MLINK mode is configured. | Make sure "MDIO Manual Mode Link Status Update" field is set to PHY Polling Based in SysConfig. The current SDK will pick the correct option based on the EnhancedLink status, but in previous SDK versions, this needs to be done manually. | |
| External PHYs sometimes aren't correctly reset or initialized, leading to link problems. | Make sure PHY reset sequence is implemented correctly for the external PHY. Additionally, refer to tiesc_ethphyInit API for the EtherCAT specific configurations to be done for the PHY. | |
| The ESC Reg 0x110 DL Status shows the out port is still connected even if the cable is disconnected, which would cause the SubDevice to no longer return the frames sent by the MainDevice. | MDIO_USER_PHY_SEL_REG (offset 0x2484) register is not configured correctly. | MDIO_USER_PHY_SEL_REG (offset 0x2484) needs to be configured to enable the link change interrupt (bit6). Additionally, the corresponding link status determination (bit7) is to be programmed for MLINK/MDIO based determination (MLINK for EnhancedLink and MDIO for otherwise). For the Beckhoff Demo, this configuration is done within tiesc_ethphyInit() API. |
| Link and the auto-negotiation is complete from PHY Register Status but not able to scan using MainDevice. No link detection on ESC DL Status Register. | TI ESC is not receiving the EtherCAT frames. | Make sure RX Frame counter (ESC Register 0x0E00 and 0x0E04) is getting incremented to make sure frames are being received by the TI ESC (Firmware) |
| Incorrect MDIO API (MDIO_phyRegWrite) used to write to the extended PHY Registers. | This function is intended to be used with the IEEE standard PHY registers only. Use the MDIO_phyExtRegWrite API to write into registers above the standard PHY registers (above offset 32h) | |
| The EtherCAT Error counters (ESC Register 0x0300 to 0x0303) are incrementing from time to time. | EtherCAT MainDevice may be sending out Error frames. | Monitor the wireshark logs for any error frames from the EtherCAT MainDevice. Additionally, try with another MainDevice and observe the behavior. |
| MainDevice PC NIC may be sending out error frames and the ESC may be processing it | Make sure DL Control (ESC Register 0x0100) is configured correctly. If Bit0 is set then non-EtherCAT frames will be destroyed. Otherwise the frames are forwarded without processing. | |
| EtherCAT SubDevice configured correctly but TwinCAT not able to scan for the Device. | TwinCAT is not configured correctly to detect for the TI EtherCAT SubDevice. | Follow Creating TwinCAT Project to add the ESI file and install the EtherCAT driver for the TwinCAT port. |
| TwinCAT reports "received invalid DC timings!" warning for a SubDevice when operating in DC mode | Incorrect cable connection between SubDevices — the OUT port of one device is connected to the OUT port of the next device instead of its IN port |
|
A common issue when implementing EtherCAT on custom hardware is the inability to get proper identification from the Ethernet PHY. This section provides guidance on troubleshooting PHY identification problems.
If you're having trouble accessing the PHY registers or getting incorrect values:
| Issue | Probable Cause | Troubleshooting Steps |
|---|---|---|
| Cannot read PHY ID registers (0x02, 0x03) | Incorrect PHY address configuration |
|
| Reading all zeros or 0xFFFF from PHY registers | MDIO hardware connection issues |
|
| Inconsistent PHY register readings | Signal integrity or timing issues |
|
| PHY ID doesn't match expected value | PHY model mismatch or incorrect initialization |
|
| Link Up not coming up | PHY is not configured in MII mode |
|
When integrating a custom PHY (different from the DP83869/DP83826 used in TI EVMs/LPs), the following configurations must be implemented to ensure proper EtherCAT operation. These requirements are derived from the tiesc_ethphyInit() API implementation.
| Configuration | Purpose | Implementation Details | Priority |
|---|---|---|---|
| MII Mode Selection | EtherCAT requires MII interface mode for proper frame handling |
| Critical |
| Auto-MDIX Enable | Allows automatic detection and configuration of straight-through or crossover cables |
| Recommended |
| Extended Full-Duplex Ability | Enables full-duplex operation required for EtherCAT communication |
| Critical |
| Odd Nibble Detection | EtherCAT uses odd nibble (alignment error) frames as markers to detect error sources in the network topology |
| Critical |
| Enhanced IPG Detection | Detects RXERR during inter-packet gap (IDLE state) |
| Recommended |
| Fast Link Down Detection | Rapidly detects link loss for quick EtherCAT topology changes |
| Critical |
| Disable 1000M Advertisement | EtherCAT SubDevice operates at 100Mbps only |
| Critical |
| MDIO Link Interrupt Enable | Enables link status change interrupts for the ESC |
| Critical |
| PHY Soft Reset | Applies all configuration changes after setup |
| Critical |
When Enhanced Link Detection is enabled (using MII_RXLINK signals), proper LED configuration is essential:
| LED Pin | Configuration | Purpose | Required for Enhanced Link |
|---|---|---|---|
| LED_0 | Link OK (without activity blink) |
| Yes (Critical) |
| LED_1 | RX_ER (Receive Error) |
| Recommended |
| LED_2 | Link OK with RX/TX Activity Blink |
| Optional |
| LED_3 | 10/100M Link Established |
| Optional |
When porting to a custom PHY, use this checklist to ensure all required configurations are implemented:
| Module | Location | TRM Reference/Register Description | Description |
| ICSS0 Instance | |||
| ICSSM0_PR1_CFG_SLV | 0x48026000 to 0x48026198 | Main configuration interface for the subsystem | |
| ICSSM_PR1_IEP0_SLV | 0x4802E000 to 0x4802E318 | Section 7.3.12 | Handles precise timing needed for industrial protocols |
| ICSSM0_PR1_MII_RT_PR1_MII_RT_CFG | 0x48032000 to 0x4803206C | Section 7.3.10 | Manages the actual Ethernet frame handling |
| ICSSM0_PR1_MDIO_V1P7_MDIO | 0x48032400 to 0x4803248C | Section 7.3.11 | Deals with PHY layer configuration |
| EtherCAT ESC Register Space | 0x48010000 to 0x48010ED1 | TI EtherCAT SubDevice Controller Register List | EtherCAT ESC Register Space contains all EtherCAT-specific functionality |
Refer to EtherCAT related E2E posts for previously answered queries on EtherCAT.