|
int32_t | PN_cfgRtcMem (PN_Handle pnHandle, uint8_t ar, uint16_t size) |
| Configures the driver memory. More...
|
|
int32_t | PN_deCfgRtcMem (PN_Handle pnHandle) |
| De-configures the driver memory. More...
|
|
int32_t | PN_initPacket (t_rtcPacket *pPkt, uint8_t type) |
| Initialize packet according to type Utility API for stack. Doesn't update anything in driver. More...
|
|
int32_t | PN_allocPkt (PN_Handle pnHandle, t_rtcPacket **pPkt, uint8_t type) |
| Allocate a packet object from internal array Initializes pPkt with PN_initPacket Find the next freeslot in t_ppmBlock t_cpmBlock, update the pBuffer address. More...
|
|
int32_t | PN_freePkt (t_rtcPacket *pPkt) |
| Free a packet object for re-use Utility API for stack. Doesn't update anything in driver. More...
|
|
int32_t | PN_insPpmList (PN_Handle pnHandle, t_rtcPacket *ppmPkt, uint8_t legMode) |
| Inserts PPM descriptor data into the lists. More...
|
|
int32_t | PN_delPmList (PN_Handle pnHandle, t_rtcPacket *pmPkt) |
| Deletes a descriptor from PPM or CPM list. More...
|
|
int32_t | PN_insCpmList (PN_Handle pnHandle, t_rtcPacket *cpmPkt) |
| Insert a packet into descriptor list and lock this buffer, indicating that ARM is consuming this buffer
. More...
|
|
int32_t | PN_setCpmState (PN_Handle pnHandle, t_rtcPacket *pPkt, uint8_t val) |
|
int32_t | PN_setPpmState (PRUICSS_HwAttrs const *pruicssHwAttrs, t_rtcPacket *pPkt) |
|
int32_t | PN_chgPpmBuffer (PN_Handle pnHandle, t_rtcPacket *ppmPkt) |
| Update PPM descriptor to new buffer address (based on ARM buffer address) More...
|
|
t_cfgPN * | PN_getConfig (void) |
|
int32_t | PN_initRtcDrv (PN_Handle pnHandle) |
| Initializes RTC driver. More...
|
|
int32_t | PN_getList (t_descList **pList, uint8_t dir) |
|
int32_t | PN_clearList (PN_Handle pnHandle, uint8_t list) |
|
int32_t | PN_resetARlink (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t ARgroup, uint8_t pmNum, uint8_t dir) |
|
int32_t | PN_cpmBuffLock (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t pos, buffLocks buff) |
| Locks CPM Buffer indicating that ARM is consuming the particular buffer. PRU cannot write to this buffer. More...
|
|
void | PN_registerPpmCall (PN_Handle pnHandle, pnCallBack_t callBack) |
| Registers callback function required for PPM processing. More...
|
|
void | PN_registerCpmCall (PN_Handle pnHandle, pnCallBack_t callBack) |
| Registers callback function required for CPM processing. More...
|
|
void | PN_registerStatCall (PN_Handle pnHandle, pnCallBack_t callBack) |
| Registers callback function required for Stat processing. More...
|
|
void | PN_registerSetState (PN_Handle pnHandle, pnLegCallBack_t callBack) |
| Registers callback function for legacy state This callback is used to change the Legacy state machine. More...
|
|
void | PN_registerSetPkt (PN_Handle pnHandle, pnLegCallBack_t callBack) |
| Registers callback function for packet pointer This callback is used to configure the packet send by the IRT state machine. More...
|
|
void | PN_clearPruIRQ (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t irq_num) |
|
int32_t | PN_setBaseClock (PN_Handle pnHandle, uint16_t factor) |
| Sets Profinet base clock in multiples of 31.25us. More...
|
|
void | PN_setFSODeviationComp (PRUICSS_HwAttrs const *pruicssHwAttrs, uint16_t fso_comp_val) |
| Sets FSO deviation compensation value for propogation delays inside ICSS. More...
|
|