4.2. PRU ICSS EthernetIP Release Notes¶
4.2.1. Overview¶
The PRU-ICSS Ethernet/IP package provides the foundation that facilitate application software development for Ethernet/IP Adapter on TI Sitara Embedded Processors with PRU-ICSS HW IP.
4.2.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory. The directory structure is shown in the user guide here
4.2.3. Standard Compliance¶
Compliant to ODVA EtherNet IP Comformance Tests 19.1
4.2.4. Documentation¶
- EtherNet IP Datasheet: Data sheet contains information about the capabilities of the solution, certification information (if applicable), memory and pin mux information. It can be found in the ‘docs’ folder in the installation directory. The directory structure is shown in the user guide here
- Software Manifest: Provides license information on software included in the package. The manifest can be found on the SDK download page or in the installed directory. The directory structure is shown in the user guide here
- EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
4.2.4.1. Release 01.00.04¶
Released November 2023
PRU-ICSS Ethernet/IP package download link : https://www.ti.com/tool/PRU-ICSS-INDUSTRIAL-SW
4.2.4.1.1. What’s New¶
- Compliance to Conformance Test Suite v19.1
- LLDP support in the firmware
- TMG stack update to version 3.7.0.0
- Removed support for K2G
- Bug Fixes
4.2.4.1.2. Features supported¶
- Ethernet/IP Capabilities
- Explicit Messaging and Implicit Messaging
- UCMM
- Class 1 and Class 3 Connection
- Object classes supported
- Identity Object
- Message Router Object
- Assembly Object
- Connection Manager Object
- Ethernet Link Object
- TCP/IP Interface Object
- QOS Object
- Device Level Ring Object
- Supported Connections
- Exclusive Owner Connection
- Input Only Connection
- Listen Only Connection
- Total CIP connections : 9
- IO Messaging : 6
- Explicit Messaging : 3
- PHY Configuration
- Duplex : Half/Full/Auto
- Speed : 10/100/Auto
- Device Configuration : EDS File
- QoS scheme : 3-bit VLAN PCP
- No of levels supported : 8
- Number of queues : 4. 2 QoS levels per queue
- Statistics
- Media counters supported per port
- Interface counters supported per port
- Conformance : CT 19.1 compliant
- Min RPI supported : 1ms
- Device Level Ring
- Beacon Based
- Min. beacon interval : 200 us
- Min. beacon timeout : 400 us
- Self configuring
- PTP/1588
- Supports Drives Profile : E2E clock.
- PTP over UDP
- Transparent Clock supported
- Ordinary Clock supported
- Single and Two step clock supported
- Learning/FDB : Yes
- 1024 entries per port
- Learning table on DDR
- Storm Prevention : Yes. Configurable per port
- Support for Multicast Filtering
- Supported on all SoCs
- Hash Table for faster lookup
- O(1) complexity
4.2.4.1.4. PRU-ICSS Firmware Revision¶
| Platform | Build | Firmware Header Location |
|---|---|---|
| AM3/AM4/AMIC110 | 5.4.2 | protocols\ethernetip_adapter\firmware\v1.0 |
| AM57x | 5.4.2 | protocols\ethernetip_adapter\firmware\v2.1 |
4.2.4.1.5. Fixed Issues¶
| Record ID | Platform | Details |
|---|---|---|
| PINDSW-3359 | AM335x, AM437x AM571x, AM572x | DUT reports incorrect topology in case of DLR state change |
| PINDSW-3360 | AM335x, AM437x AM571x, AM572x | DUT forward DLR Frames only if a IP address is configured |
| PINDSW-4635 | AM335x, AM437x AM571x, AM572x | Invalid receive packet length information in Buffer descriptor when high netwrok load is applied |
| PINDSW-4651 | AM335x, AM437x AM571x, AM572x | DLR: Sign On frames are not forwarded when Supervisor switch happens |
| PINDSW-4966 | AM335x, AM437x AM571x, AM572x | Switching supervisors on the fly still does not reliably work |
| PINDSW-5014 | AM335x, AM437x AM571x, AM572x | TimeSync_drvDisable API does not work everytime |
| PINDSW-5198 | AM335x, AM437x AM571x, AM572x | EtherNet/IP Firmware does not process PTP frames if “V1 Compatibility” is set in PTP header |
| PINDSW-5382 | AM335x, AM437x AM571x, AM572x | EIP_DLR_processDLRFrame API fails on large DLR Sign-On Frames |
| PINDSW-6941 | AM335x, AM437x AM571x, AM572x | Active Supervisor MAC and IP address is not being cleared after the supervisor is disabled. |
| PINDSW-7027 | AMIC110 | Ethernet Link Object Test failures in CT19.1 - PHY does not get configured properly in Half Duplex Mode |
4.2.4.1.6. Known Issues¶
This section contains the list of known Issues at the time of making the release.
| Record ID | Platform | Details | Workaround |
|---|---|---|---|
| PINDSW-3082 | AM571x | Ping fails on AM571x board ICSS1 Port1 | |
| PINDSW-7013 | AM572x | Flash Read not working as expected when loading EthernetIP application from SD card | |
| PINDSW-7077 | AM335x, AM437x AM571x, AM572x | Automated ACD Behavior Test V2.4.13 in ODVA Interactive Test Sequencer fails sporadically. | |
| PINDSW-7014 | AM335x, AM43x, AM571x, AM572x | New stack supports minimum RPI of 2 ms |
4.2.4.2. Additional Notes¶
Details of key interface changes in the package from the previous release
Note
Ethernet/IP application on AM64x and AM65x is not supported in this release.
Note
QuickConnect (QC) has been added as an experimental feature in the TMG stack and has not been validated through testing.
| NEW | OLD | Notes/Impact | ||||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
The Ethernet/IP application uses the TimeSync library from the PROCESSOR-SDK-RTOS package.
Therefore, any changes required in the TimeSync driver need to be done in the PDK package inside the
PROCESSOR-SDK-RTOS : [PDK_INSTALL_DIR]/pakages/ti/transport/timeSync/include.
The [INSTALL-DIR]/protocols/timeSync folder only contains the files required for building the PTPD stack. |
The Ethernet/IP application used the TimeSync library from the PRU-ICSS-EthernetIP_Adapter package.
The [INSTALL-DIR]/protocols/timeSync folder contained the TimeSync driver source and include files
for building the TimeSync library. |
|||||||||||||||||||||||||||||||||||||||||||||||||
The stc folder provided with the application has been renamed to soc. All the soc files required for
the ODVA CT19.1 tests are located at [INSTALL-DIR]/examples/ethernetip_adapter/soc |
The stc files for ODVA Conformance tests were provided with the application in the stc folder. | |||||||||||||||||||||||||||||||||||||||||||||||||
The changes for the Target Configuration parameters for this release are as follows. Target Info:
Connection Information:
|
The old target configuration parameters were as follows. Target Info:
Connection Information:
|