AM263x MCU+ SDK  09.01.00

Introduction

This file contains the prototype of LIN driver APIs.

Go to the source code of this file.

Macros

#define LIN_IO_DFT_KEY   (0xAU)
 LIN IO DFT Key which when written in IODFTENA enables the User and Previledge mode Writes. More...
 
#define LIN_WAKEUP_KEY   (0xF0U)
 LIN/SCI Wakeup signal is sent by sending an byte with value 0xF0. More...
 
Lin Parity ID Masks

Note: Parity ID Masks for LIN

#define LIN_ID0   (0x1U)
 
#define LIN_ID1   (0x2U)
 
#define LIN_ID2   (0x4U)
 
#define LIN_ID3   (0x8U)
 
#define LIN_ID4   (0x10U)
 
#define LIN_ID5   (0x20U)
 
Lin Interrupt Flag Parameters
#define LIN_INT_WAKEUP   (0x00000002U) /* Wakeup */
 
#define LIN_INT_TO   (0x00000010U) /* Time out */
 
#define LIN_INT_TOAWUS   (0x00000040U) /* Time out after wakeup signal */
 
#define LIN_INT_TOA3WUS   (0x00000080U) /* Time out after 3 wakeup signals */
 
#define LIN_INT_TX   (0x00000100U) /* Transmit buffer ready */
 
#define LIN_INT_RX   (0x00000200U) /* Receive buffer ready */
 
#define LIN_INT_ID   (0x00002000U) /* Received matching identifier */
 
#define LIN_INT_PE   (0x01000000U) /* Parity error */
 
#define LIN_INT_OE   (0x02000000U) /* Overrun error */
 
#define LIN_INT_FE   (0x04000000U) /* Framing error */
 
#define LIN_INT_NRE   (0x08000000U) /* No response error */
 
#define LIN_INT_ISFE   (0x10000000U) /* Inconsistent sync field error */
 
#define LIN_INT_CE   (0x20000000U) /* Checksum error */
 
#define LIN_INT_PBE   (0x40000000U) /* Physical bus error */
 
#define LIN_INT_BE   (0x80000000U) /* Bit error */
 
#define LIN_INT_ALL   (0xFF0023D2U) /* All interrupts */
 
Lin Get Interrupt Flag

Note: Definitions for the return value of LIN_getInterruptStatus().

#define LIN_FLAG_BREAK   (CSL_LIN_SCIFLR_BRKDT_MASK)
 
#define LIN_FLAG_WAKEUP   (CSL_LIN_SCIFLR_WAKEUP_MASK)
 
#define LIN_FLAG_IDLE   (CSL_LIN_SCIFLR_IDLE_MASK)
 
#define LIN_FLAG_BUSY   (CSL_LIN_SCIFLR_BUSY_MASK)
 
#define LIN_FLAG_TO   (CSL_LIN_SCIFLR_TIMEOUT_MASK)
 
#define LIN_FLAG_TOAWUS   (CSL_LIN_SCIFLR_TOAWUS_MASK)
 
#define LIN_FLAG_TOA3WUS   (CSL_LIN_SCIFLR_TOA3WUS_MASK)
 
#define LIN_FLAG_TXRDY   (CSL_LIN_SCIFLR_TXRDY_MASK)
 
#define LIN_FLAG_RXRDY   (CSL_LIN_SCIFLR_RXRDY_MASK)
 
#define LIN_FLAG_TXWAKE   (CSL_LIN_SCIFLR_TXWAKE_MASK)
 
#define LIN_FLAG_TXEMPTY   (CSL_LIN_SCIFLR_TXEMPTY_MASK)
 
#define LIN_FLAG_RXWAKE   (CSL_LIN_SCIFLR_RXWAKE_MASK)
 
#define LIN_FLAG_TXID   (CSL_LIN_SCIFLR_IDTXFLAG_MASK)
 
#define LIN_FLAG_RXID   (CSL_LIN_SCIFLR_IDRXFLAG_MASK)
 
#define LIN_FLAG_PE   (CSL_LIN_SCIFLR_PE_MASK)
 
#define LIN_FLAG_OE   (CSL_LIN_SCIFLR_OE_MASK)
 
#define LIN_FLAG_FE   (CSL_LIN_SCIFLR_FE_MASK)
 
#define LIN_FLAG_NRE   (CSL_LIN_SCIFLR_NRE_MASK)
 
#define LIN_FLAG_ISFE   (CSL_LIN_SCIFLR_ISFE_MASK)
 
#define LIN_FLAG_CE   (CSL_LIN_SCIFLR_CE_MASK)
 
#define LIN_FLAG_PBE   (CSL_LIN_SCIFLR_PBE_MASK)
 
#define LIN_FLAG_BE   (CSL_LIN_SCIFLR_BE_MASK)
 
Lin Interrupt Offset

Note: Definitions for the return value of LIN_getInterruptLine0Offset() and LIN_getInterruptLine1Offset().

#define LIN_VECT_NONE   (0x00)
 
#define LIN_VECT_WAKEUP   (0x01)
 
#define LIN_VECT_ISFE   (0x02)
 
#define LIN_VECT_PE   (0x03)
 
#define LIN_VECT_ID   (0x04)
 
#define LIN_VECT_PBE   (0x05)
 
#define LIN_VECT_FE   (0x06)
 
#define LIN_VECT_BREAK   (0x07)
 
#define LIN_VECT_CE   (0x08)
 
#define LIN_VECT_OE   (0x09)
 
#define LIN_VECT_BE   (0x0A)
 
#define LIN_VECT_RX   (0x0B)
 
#define LIN_VECT_TX   (0x0C)
 
#define LIN_VECT_NRE   (0x0D)
 
#define LIN_VECT_TOAWUS   (0x0E)
 
#define LIN_VECT_TOA3WUS   (0x0F)
 
#define LIN_VECT_TO   (0x10)
 
Lin Error Defination

Note: Definitions for the LIN errors parameter of LIN_enableModuleErrors() and LIN_disableModuleErrors().

#define LIN_ALL_ERRORS   (0xF0000000U)
 
#define LIN_BIT_ERROR   (0x80000000U)
 
#define LIN_BUS_ERROR   (0x40000000U)
 
#define LIN_CHECKSUM_ERROR   (0x20000000U)
 
#define LIN_ISF_ERROR   (0x10000000U)
 
Lin Serial Communication Interface Error Defination
#define LIN_SCI_ALL_ERRORS   (0x7000000U)
 
#define LIN_SCI_FRAME_ERROR   (0x4000000U)
 
#define LIN_SCI_PARITY_ERROR   (0x2000000U)
 
#define LIN_SCI_BREAK_ERROR   (0x1000000U)
 
#define LIN_SCI_INT_BREAK   (0x1U)
 
#define LIN_SCI_INT_WAKEUP   (0x2U)
 
#define LIN_SCI_INT_TX   (0x100U)
 
#define LIN_SCI_INT_RX   (0x200U)
 
#define LIN_SCI_INT_TX_DMA   (0x10000U)
 
#define LIN_SCI_INT_RX_DMA   (0x20000U)
 
#define LIN_SCI_INT_PARITY   (0x1000000U)
 
#define LIN_SCI_INT_OVERRUN   (0x2000000U)
 
#define LIN_SCI_INT_FRAME   (0x4000000U)
 
#define LIN_SCI_INT_ALL   (0x7000303U)
 

Enumerations

enum  LIN_LoopbackType { LIN_LOOPBACK_DIGITAL = 0U, LIN_LOOPBACK_ANALOG = 1U }
 The following are defines for the type parameter of the LIN_enableExtLoopback() function. More...
 
enum  LIN_AnalogLoopback { LIN_ANALOG_LOOP_NONE = 0U, LIN_ANALOG_LOOP_TX = 0U, LIN_ANALOG_LOOP_RX = 1U }
 The following are defines for the path parameter of the LIN_enableExtLoopback() function. More...
 
enum  LIN_CommMode { LIN_COMM_LIN_USELENGTHVAL = 0x0000U, LIN_COMM_LIN_ID4ID5LENCTL = 0x0001U }
 The following are defines for the mode parameter of the LIN_setCommMode() function. More...
 
enum  LIN_SCICommMode { LIN_COMM_SCI_IDLELINE = 0x0000U, LIN_COMM_SCI_ADDRBIT = 0x0001U }
 The following are defines for the mode parameter of the LIN_setSCICommMode() function. More...
 
enum  LIN_LINMode { LIN_MODE_LIN_RESPONDER = 0x0U, LIN_MODE_LIN_COMMANDER = 0x1U }
 The following are defines for the mode parameter of the LIN_setLINMode() function. More...
 
enum  LIN_InterruptLine { LIN_INTERRUPT_LINE0 = 0x0U, LIN_INTERRUPT_LINE1 = 0x1U }
 The following are defines for the line parameter of the LIN_enableGlobalInterrupt(), LIN_disableGlobalInterrupt(), LIN_clearGlobalInterruptStatus(), and LIN_getGlobalInterruptStatus() functions. More...
 
enum  LIN_MessageFilter { LIN_MSG_FILTER_IDBYTE = 0x0U, LIN_MSG_FILTER_IDRESPONDER = 0x1U }
 The following are defines for the type parameter of the LIN_setMessageFiltering() function. More...
 
enum  LIN_ChecksumType { LIN_CHECKSUM_CLASSIC = 0x0U, LIN_CHECKSUM_ENHANCED = 0x1U }
 The following are defines for the type parameter of the LIN_setChecksumType() function. More...
 
enum  LIN_DebugMode { LIN_DEBUG_FROZEN = 0x0U, LIN_DEBUG_COMPLETE = 0x1U }
 The following are defines for the mode parameter of the LIN_setDebugSuspendMode() function. More...
 
enum  LIN_PinSampleMask { LIN_PINMASK_NONE = 0x0U, LIN_PINMASK_CENTER = 0x1U, LIN_PINMASK_CENTER_SCLK = 0x2U, LIN_PINMASK_CENTER_2SCLK = 0x3U }
 The following are defines for the mask parameter of the LIN_setPinSampleMask() function. More...
 
enum  LIN_SCIParityType { LIN_SCI_PAR_ODD = 0x0U, LIN_SCI_PAR_EVEN = 0x1U }
 The following are defines for the parity parameter of the LIN_enableSCIParity() function. More...
 
enum  LIN_SCIStopBits { LIN_SCI_STOP_ONE = 0x0U, LIN_SCI_STOP_TWO = 0x1U }
 The following are defines for the number parameter of the LIN_setSCIStopBits() function. More...
 
enum  LIN_PinType { LIN_PINTYPE_TX = 0x4U, LIN_PINTYPE_RX = 0x2U }
 The following are defines for the pin parameter of the LIN_getPinStatus() function. More...
 

Functions

void LIN_initModule (uint32_t base)
 This function initializes the LIN module. More...
 
void LIN_getData (uint32_t base, uint16_t *const data)
 This function reads the received data. More...
 
void LIN_sendData (uint32_t base, uint16_t *data)
 This function sends the data. More...
 
static Bool LIN_isBaseValid (uint32_t base)
 Checks a LIN base address. More...
 
static void LIN_setLINMode (uint32_t base, LIN_LINMode mode)
 Sets the LIN mode. More...
 
static void LIN_setMaximumBaudRate (uint32_t base, uint32_t clock)
 Set Maximum Baud Rate Prescaler. More...
 
static void LIN_setMessageFiltering (uint32_t base, LIN_MessageFilter type)
 Set Message filtering Type. More...
 
static void LIN_enableParity (uint32_t base)
 Enable Parity mode. More...
 
static void LIN_disableParity (uint32_t base)
 Disable Parity mode. More...
 
static uint16_t LIN_generateParityID (uint16_t identifier)
 Generate Parity Identifier. More...
 
static void LIN_setIDByte (uint32_t base, uint16_t identifier)
 Set ID Byte. More...
 
static void LIN_setIDResponderTask (uint32_t base, uint16_t identifier)
 Set ID-ResponderTask. More...
 
static void LIN_sendWakeupSignal (uint32_t base)
 Send LIN wakeup signal. More...
 
static void LIN_enterSleep (uint32_t base)
 Entering LIN sleep signal. More...
 
static void LIN_sendChecksum (uint32_t base)
 Send Checksum Byte. More...
 
static void LIN_triggerChecksumCompare (uint32_t base)
 Trigger Checksum Compare. More...
 
static Bool LIN_isTxReady (uint32_t base)
 Check Tx buffer ready flag. More...
 
static void LIN_setFrameLength (uint32_t base, uint16_t length)
 Set LIN Frame Length. More...
 
static void LIN_setCommMode (uint32_t base, LIN_CommMode mode)
 Set LIN communication mode. More...
 
static void LIN_setTxMask (uint32_t base, uint16_t mask)
 Sets the transmit ID mask. More...
 
static void LIN_setRxMask (uint32_t base, uint16_t mask)
 Sets the receive ID mask. More...
 
static uint16_t LIN_getTxMask (uint32_t base)
 Gets the transmit ID mask. More...
 
static uint16_t LIN_getRxMask (uint32_t base)
 Gets the receive ID mask. More...
 
static Bool LIN_isRxReady (uint32_t base)
 Gets the receive ID mask. More...
 
static uint16_t LIN_getRxIdentifier (uint32_t base)
 Get last received identifier. More...
 
static Bool LIN_isTxMatch (uint32_t base)
 Checks for Tx ID Match Received. More...
 
static Bool LIN_isRxMatch (uint32_t base)
 Checks for Rx ID Match Received. More...
 
static void LIN_enableInterrupt (uint32_t base, uint32_t intFlags)
 Enable interrupts. More...
 
static void LIN_disableInterrupt (uint32_t base, uint32_t intFlags)
 Disable interrupts. More...
 
static void LIN_clearInterruptStatus (uint32_t base, uint32_t intFlags)
 Clear interrupt status. More...
 
static void LIN_setInterruptLevel0 (uint32_t base, uint32_t intFlags)
 Set interrupt level to 0. More...
 
static void LIN_setInterruptLevel1 (uint32_t base, uint32_t intFlags)
 Set interrupt level to 1. More...
 
static void LIN_enableModuleErrors (uint32_t base, uint32_t errors)
 Enable Module Errors for Testing. More...
 
static void LIN_disableModuleErrors (uint32_t base, uint32_t errors)
 Disable Module Errors for Testing. More...
 
static void LIN_enableAutomaticBaudrate (uint32_t base)
 Enable Automatic Baudrate Adjustment. More...
 
static void LIN_disableAutomaticBaudrate (uint32_t base)
 Disable Automatic Baudrate Adjustment. More...
 
static void LIN_stopExtendedFrame (uint32_t base)
 Stops LIN Extended Frame Communication. More...
 
static void LIN_setChecksumType (uint32_t base, LIN_ChecksumType type)
 Set Checksum Type. More...
 
static void LIN_setSyncFields (uint32_t base, uint16_t syncBreak, uint16_t delimiter)
 Set Sync Break Extend and Delimiter. More...
 
static void LIN_enableSCIMode (uint32_t base)
 Enable SCI Mode. More...
 
static void LIN_disableSCIMode (uint32_t base)
 Disable SCI Mode. More...
 
static void LIN_setSCICommMode (uint32_t base, LIN_SCICommMode mode)
 Set SCI communication mode. More...
 
static void LIN_enableSCIParity (uint32_t base, LIN_SCIParityType parity)
 Enable SCI Parity mode. More...
 
static void LIN_disableSCIParity (uint32_t base)
 Disable SCI Parity mode. More...
 
static void LIN_setSCIStopBits (uint32_t base, LIN_SCIStopBits number)
 Set the number of stop bits for SCI. More...
 
static void LIN_enableSCISleepMode (uint32_t base)
 Enable SCI Sleep mode. More...
 
static void LIN_disableSCISleepMode (uint32_t base)
 Disable SCI Sleep mode. More...
 
static void LIN_enterSCILowPower (uint32_t base)
 Enter SCI Local Low-Power Mode. More...
 
static void LIN_exitSCILowPower (uint32_t base)
 Exit SCI Local Low-Power Mode. More...
 
static void LIN_setSCICharLength (uint32_t base, uint16_t numBits)
 Set SCI character length. More...
 
static void LIN_setSCIFrameLength (uint32_t base, uint16_t length)
 Set SCI Frame Length. More...
 
static Bool LIN_isSCIDataAvailable (uint32_t base)
 Check if new SCI data is ready to be read. More...
 
static Bool LIN_isSCISpaceAvailable (uint32_t base)
 Check if Space is available in SCI Transmit Buffer. More...
 
static uint16_t LIN_readSCICharNonBlocking (uint32_t base, Bool emulation)
 Reads a SCI character without Blocking. More...
 
static uint16_t LIN_readSCICharBlocking (uint32_t base, Bool emulation)
 Reads a SCI character with Blocking. More...
 
static void LIN_writeSCICharNonBlocking (uint32_t base, uint16_t data)
 Sends a SCI character without Blocking. More...
 
static void LIN_writeSCICharBlocking (uint32_t base, uint16_t data)
 Sends a SCI character with blocking. More...
 
static void LIN_enableSCIModuleErrors (uint32_t base, uint32_t errors)
 Enable SCI Module Errors for Testing. More...
 
static void LIN_disableSCIModuleErrors (uint32_t base, uint32_t errors)
 Disable SCI Module Errors for Testing. More...
 
static void LIN_enableSCIInterrupt (uint32_t base, uint32_t intFlags)
 Enable SCI interrupts. More...
 
static void LIN_disableSCIInterrupt (uint32_t base, uint32_t intFlags)
 Disable SCI interrupts. More...
 
static void LIN_clearSCIInterruptStatus (uint32_t base, uint32_t intFlags)
 Clear SCI interrupt status. More...
 
static void LIN_setSCIInterruptLevel0 (uint32_t base, uint32_t intFlags)
 Set interrupt level to 0. More...
 
static void LIN_setSCIInterruptLevel1 (uint32_t base, uint32_t intFlags)
 Set interrupt level to 1. More...
 
static Bool LIN_isSCIReceiverIdle (uint32_t base)
 Check if SCI Receiver is Idle. More...
 
static Bool LIN_getSCITxFrameType (uint32_t base)
 Gets the SCI Transmit Frame Type. More...
 
static Bool LIN_getSCIRxFrameType (uint32_t base)
 Gets the SCI Receiver Frame Type. More...
 
static Bool LIN_isSCIBreakDetected (uint32_t base)
 Check if SCI Detected a Break Condition. More...
 
static void LIN_enableModule (uint32_t base)
 Enables the LIN module. More...
 
static void LIN_disableModule (uint32_t base)
 Disable the LIN module. More...
 
static void LIN_setBaudRatePrescaler (uint32_t base, uint32_t prescaler, uint32_t divider)
 Set Baud Rate Prescaler. More...
 
static void LIN_enableDataTransmitter (uint32_t base)
 Enable Transmit Data Transfer. More...
 
static void LIN_disableDataTransmitter (uint32_t base)
 Disable Transmit Data Transfer. More...
 
static void LIN_enableDataReceiver (uint32_t base)
 Enable Receive Data Transfer. More...
 
static void LIN_disableDataReceiver (uint32_t base)
 Disable Receive Data Transfer. More...
 
static void LIN_performSoftwareReset (uint32_t base)
 Perform software reset. More...
 
static void LIN_enterSoftwareReset (uint32_t base)
 Put LIN into its reset state. More...
 
static void LIN_exitSoftwareReset (uint32_t base)
 Put LIN into its ready state. More...
 
static Bool LIN_isBusBusy (uint32_t base)
 Check if Bus is Busy. More...
 
static Bool LIN_isTxBufferEmpty (uint32_t base)
 Check if the Transmit Buffer is Empty. More...
 
static void LIN_enableExtLoopback (uint32_t base, LIN_LoopbackType loopbackType, LIN_AnalogLoopback path)
 Enable External Loopback mode for self test. More...
 
static void LIN_disableExtLoopback (uint32_t base)
 Disable External Loopback mode for self test. More...
 
static void LIN_enableIntLoopback (uint32_t base)
 Enable Internal Loopback mode for self test. More...
 
static void LIN_disableIntLoopback (uint32_t base)
 Disable Internal Loopback mode for self test. More...
 
static uint32_t LIN_getInterruptStatus (uint32_t base)
 Get Interrupt Flags Status. More...
 
static uint32_t LIN_getInterruptLevel (uint32_t base)
 Get the Interrupt Level. More...
 
static uint16_t LIN_getInterruptLine0Offset (uint32_t base)
 Gets the Interrupt Vector Offset for Line 0. More...
 
static uint16_t LIN_getInterruptLine1Offset (uint32_t base)
 Gets the Interrupt Vector Offset for Line 1. More...
 
static void LIN_enableMultibufferMode (uint32_t base)
 Enable Multi-buffer Mode. More...
 
static void LIN_disableMultibufferMode (uint32_t base)
 Disable Multi-buffer Mode. More...
 
static void LIN_setTransmitDelay (uint32_t base, uint16_t delay)
 Set Transmit Pin Delay. More...
 
static void LIN_setPinSampleMask (uint32_t base, LIN_PinSampleMask mask)
 Set Pin Sample Mask. More...
 
static void LIN_setDebugSuspendMode (uint32_t base, LIN_DebugMode mode)
 Set the Debug Suspended Mode. More...
 
static void LIN_enableGlobalInterrupt (uint32_t base, LIN_InterruptLine line)
 Enables a LIN global interrupt. More...
 
static void LIN_disableGlobalInterrupt (uint32_t base, LIN_InterruptLine line)
 Disables a LIN global interrupt. More...
 
static void LIN_clearGlobalInterruptStatus (uint32_t base, LIN_InterruptLine line)
 Clears a LIN global interrupt flag. More...
 
static Bool LIN_getGlobalInterruptStatus (uint32_t base, LIN_InterruptLine line)
 Returns a LIN global interrupt flag status. More...
 
static Bool LIN_getPinStatus (uint32_t base, LIN_PinType pin)
 Get the Status of LIN TX/RX Pin status. More...