Go to the source code of this file.
Data Structures | |
struct | SPLL_1PH_SOGI_FLL_OSG_COEFF |
Defines the SPLL_1PH_SOGI_FLL_OSG_COEFF structure. More... | |
struct | SPLL_1PH_SOGI_FLL_LPF_COEFF |
Defines the SPLL_1PH_SOGI_FLL_LPF_COEFF structure. More... | |
struct | SPLL_1PH_SOGI_FLL |
Defines the Orthogonal Signal Generator SPLL_1PH_SOGI_FLL structure. More... | |
Macros | |
#define | IEEE754_TYPES |
Typedefs | |
typedef float | float32_t |
typedef double | float64_t |
Functions | |
static void | SPLL_1PH_SOGI_FLL_reset (SPLL_1PH_SOGI_FLL *spll_obj) |
Resets internal data to zero,. More... | |
static void | SPLL_1PH_SOGI_FLL_coeff_calc (SPLL_1PH_SOGI_FLL *spll_obj) |
Calculates the SPLL_1PH_SOGI_FLL coefficients. More... | |
static void | SPLL_1PH_SOGI_FLL_config (SPLL_1PH_SOGI_FLL *spll_obj, float32_t acFreq, float32_t isrFrequency, float32_t lpf_b0, float32_t lpf_b1, float32_t k, float32_t gamma) |
Configures the SPLL_1PH_SOGI_FLL coefficients. More... | |
static void | SPLL_1PH_SOGI_FLL_run (SPLL_1PH_SOGI_FLL *spll_obj, float32_t acValue) |
Runs SPLL_1PH_SOGI_FLL module. More... | |