![Logo](ti_logo.svg) |
AM263x Digital Power SDK
09.01.00
|
|
Go to the documentation of this file.
41 #ifndef SPLL_1PH_SOGI_FLL_H
42 #define SPLL_1PH_SOGI_FLL_H
76 #endif // IEEE754_TYPES
85 typedef volatile struct{
215 spll_obj->
w_dash = 2*3.14159265f*acFreq;
216 spll_obj->
wc = 2*3.14159265f*acFreq;
217 spll_obj->
delta_t=((1.0f)/isrFrequency);
219 spll_obj->
gamma=gamma;
239 spll_obj->
u[0]=acValue;
245 (spll_obj->
u[0]-spll_obj->
u[2])) +
261 spll_obj->
u[2]=spll_obj->
u[1];
262 spll_obj->
u[1]=spll_obj->
u[0];
275 spll_obj->
ylf[0]=spll_obj->
ylf[1] +
278 spll_obj->
ylf[1]=spll_obj->
ylf[0];
283 spll_obj->
u_Q[1]=spll_obj->
u_Q[0];
288 spll_obj->
fo=spll_obj->
fn+spll_obj->
ylf[0];
304 spll_obj->
ef2 = ((spll_obj->
u[0] - spll_obj->
osg_u[0])*spll_obj->
osg_qu[0])
307 spll_obj->
x3[0]=spll_obj->
x3[1] + spll_obj->
ef2;
312 spll_obj->
x3[1]=spll_obj->
x3[0];
314 spll_obj->
w_dash = spll_obj->
wc + spll_obj->
x3[0];
316 spll_obj->
fn = spll_obj->
w_dash / (2.0*3.1415926f);
340 #endif // end of _SPLL_1PH_SOGI_H_ definition
static void SPLL_1PH_SOGI_FLL_coeff_calc(SPLL_1PH_SOGI_FLL *spll_obj)
Calculates the SPLL_1PH_SOGI_FLL coefficients.
Definition: spll_1ph_sogi_fll.h:176
SPLL_1PH_SOGI_FLL_OSG_COEFF osg_coeff
Orthogonal signal generator coefficient.
Definition: spll_1ph_sogi_fll.h:130
float float32_t
Definition: spll_1ph_sogi_fll.h:74
Defines the SPLL_1PH_SOGI_FLL_LPF_COEFF structure.
Definition: spll_1ph_sogi_fll.h:97
float32_t osg_qb1
Definition: spll_1ph_sogi_fll.h:91
float32_t osg_a2
Definition: spll_1ph_sogi_fll.h:89
float32_t fo
Output frequency of PLL(Hz)
Definition: spll_1ph_sogi_fll.h:118
static void SPLL_1PH_SOGI_FLL_reset(SPLL_1PH_SOGI_FLL *spll_obj)
Resets internal data to zero,.
Definition: spll_1ph_sogi_fll.h:137
float32_t k
K parameter for FLL.
Definition: spll_1ph_sogi_fll.h:129
float32_t ef2
FLL parameter.
Definition: spll_1ph_sogi_fll.h:125
float32_t osg_b0
Definition: spll_1ph_sogi_fll.h:86
float32_t fn
Nominal frequency (Hz)
Definition: spll_1ph_sogi_fll.h:119
float32_t u_D[2]
D-axis component.
Definition: spll_1ph_sogi_fll.h:116
float32_t gamma
Gamma parameter for FLL.
Definition: spll_1ph_sogi_fll.h:128
float32_t delta_t
Inverse of the ISR rate at which module is called.
Definition: spll_1ph_sogi_fll.h:124
float32_t ylf[2]
Loop filter data storage.
Definition: spll_1ph_sogi_fll.h:117
float32_t u_Q[2]
Q-axis component.
Definition: spll_1ph_sogi_fll.h:115
float32_t sine
Sine value of the PLL angle.
Definition: spll_1ph_sogi_fll.h:123
float32_t osg_b2
Definition: spll_1ph_sogi_fll.h:87
Defines the SPLL_1PH_SOGI_FLL_OSG_COEFF structure.
Definition: spll_1ph_sogi_fll.h:85
float32_t osg_qb0
Definition: spll_1ph_sogi_fll.h:90
static void SPLL_1PH_SOGI_FLL_run(SPLL_1PH_SOGI_FLL *spll_obj, float32_t acValue)
Runs SPLL_1PH_SOGI_FLL module.
Definition: spll_1ph_sogi_fll.h:231
float32_t x3[2]
FLL data storage.
Definition: spll_1ph_sogi_fll.h:126
float32_t osg_qb2
Definition: spll_1ph_sogi_fll.h:92
float32_t w_dash
Output frequency of PLL(radians)
Definition: spll_1ph_sogi_fll.h:127
float32_t cosine
Cosine value of the PLL angle.
Definition: spll_1ph_sogi_fll.h:122
float32_t wc
Center (Nominal) frequency in radians.
Definition: spll_1ph_sogi_fll.h:120
float32_t osg_qu[3]
Orthogonal signal generator quadrature data buffer.
Definition: spll_1ph_sogi_fll.h:114
SPLL_1PH_SOGI_FLL_LPF_COEFF lpf_coeff
Loop filter coeffcient structure.
Definition: spll_1ph_sogi_fll.h:131
float32_t u[3]
AC input data buffer.
Definition: spll_1ph_sogi_fll.h:112
float32_t osg_u[3]
Orthogonal signal generator data buffer.
Definition: spll_1ph_sogi_fll.h:113
static void SPLL_1PH_SOGI_FLL_config(SPLL_1PH_SOGI_FLL *spll_obj, float32_t acFreq, float32_t isrFrequency, float32_t lpf_b0, float32_t lpf_b1, float32_t k, float32_t gamma)
Configures the SPLL_1PH_SOGI_FLL coefficients.
Definition: spll_1ph_sogi_fll.h:206
double float64_t
Definition: spll_1ph_sogi_fll.h:75
float32_t b0
Definition: spll_1ph_sogi_fll.h:99
float float32_t
Defines single,double precision data type. Note: Assumes ABI to be TI_EABI, does not support legacy T...
Definition: dcl_common.h:54
float32_t theta
Angle output (0-2*pi)
Definition: spll_1ph_sogi_fll.h:121
float32_t osg_a1
Definition: spll_1ph_sogi_fll.h:88
float32_t b1
Definition: spll_1ph_sogi_fll.h:98
Defines the Orthogonal Signal Generator SPLL_1PH_SOGI_FLL structure.
Definition: spll_1ph_sogi_fll.h:111