Go to the source code of this file.
Data Structures | |
struct | RAMPGEN |
Defines the Ramp Signal Generator (RAMPGEN) structure. More... | |
Macros | |
#define | IEEE754_TYPES |
Typedefs | |
typedef float | float32_t |
typedef double | float64_t |
Functions | |
static void | RAMPGEN_reset (RAMPGEN *v) |
resets RAMPGEN internal storage data and outputs More... | |
static void | RAMPGEN_config (RAMPGEN *v, float32_t isrFrequency, float32_t rampFrequency) |
configures RAMPGEN module More... | |
static void | RAMPGEN_run (RAMPGEN *v) |
Run RAMPGEN module. More... | |