Here is the list of APIs used for Digital Control Library
◆ IEEE754_TYPES
◆ float32_t
◆ float64_t
◆ RAMPGEN_reset()
static void RAMPGEN_reset |
( |
RAMPGEN * |
v | ) |
|
|
inlinestatic |
resets RAMPGEN internal storage data and outputs
- Parameters
-
◆ RAMPGEN_config()
configures RAMPGEN module
- Parameters
-
v | a pointer to a RAMPGEN structure |
isrFrequency | Frequency at which the RAMGEN is called in ISR |
rampFrequency | Frequency of the RAMP generated by RAMPGEN module |
◆ RAMPGEN_run()
static void RAMPGEN_run |
( |
RAMPGEN * |
v | ) |
|
|
inlinestatic |