MSP430 DriverLib for MSP430FR5xx_6xx Devices  2.21.00.08
 All Data Structures Functions Variables Modules Pages
Timer_B_outputPWMParam Struct Reference

Used in the Timer_B_outputPWM() function as the param parameter. More...

#include <timer_b.h>

Data Fields

uint16_t clockSource
 
uint16_t clockSourceDivider
 
uint16_t timerPeriod
 Selects the desired Timer_B period.
 
uint16_t compareRegister
 
uint16_t compareOutputMode
 
uint16_t dutyCycle
 Specifies the dutycycle for the generated waveform.
 

Detailed Description

Used in the Timer_B_outputPWM() function as the param parameter.

Field Documentation

uint16_t Timer_B_outputPWMParam::clockSource

Selects the clock source
Valid values are:

  • TIMER_B_CLOCKSOURCE_EXTERNAL_TXCLK [Default]
  • TIMER_B_CLOCKSOURCE_ACLK
  • TIMER_B_CLOCKSOURCE_SMCLK
  • TIMER_B_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK

Referenced by Timer_B_outputPWM().

uint16_t Timer_B_outputPWMParam::clockSourceDivider

Is the divider for Clock source.
Valid values are:

  • TIMER_B_CLOCKSOURCE_DIVIDER_1 [Default]
  • TIMER_B_CLOCKSOURCE_DIVIDER_2
  • TIMER_B_CLOCKSOURCE_DIVIDER_3
  • TIMER_B_CLOCKSOURCE_DIVIDER_4
  • TIMER_B_CLOCKSOURCE_DIVIDER_5
  • TIMER_B_CLOCKSOURCE_DIVIDER_6
  • TIMER_B_CLOCKSOURCE_DIVIDER_7
  • TIMER_B_CLOCKSOURCE_DIVIDER_8
  • TIMER_B_CLOCKSOURCE_DIVIDER_10
  • TIMER_B_CLOCKSOURCE_DIVIDER_12
  • TIMER_B_CLOCKSOURCE_DIVIDER_14
  • TIMER_B_CLOCKSOURCE_DIVIDER_16
  • TIMER_B_CLOCKSOURCE_DIVIDER_20
  • TIMER_B_CLOCKSOURCE_DIVIDER_24
  • TIMER_B_CLOCKSOURCE_DIVIDER_28
  • TIMER_B_CLOCKSOURCE_DIVIDER_32
  • TIMER_B_CLOCKSOURCE_DIVIDER_40
  • TIMER_B_CLOCKSOURCE_DIVIDER_48
  • TIMER_B_CLOCKSOURCE_DIVIDER_56
  • TIMER_B_CLOCKSOURCE_DIVIDER_64

Referenced by Timer_B_outputPWM().

uint16_t Timer_B_outputPWMParam::compareOutputMode

Specifies the output mode.
Valid values are:

  • TIMER_B_OUTPUTMODE_OUTBITVALUE [Default]
  • TIMER_B_OUTPUTMODE_SET
  • TIMER_B_OUTPUTMODE_TOGGLE_RESET
  • TIMER_B_OUTPUTMODE_SET_RESET
  • TIMER_B_OUTPUTMODE_TOGGLE
  • TIMER_B_OUTPUTMODE_RESET
  • TIMER_B_OUTPUTMODE_TOGGLE_SET
  • TIMER_B_OUTPUTMODE_RESET_SET

Referenced by Timer_B_outputPWM().

uint16_t Timer_B_outputPWMParam::compareRegister

Selects the compare register being used. Refer to datasheet to ensure the device has the compare register being used.
Valid values are:

  • TIMER_B_CAPTURECOMPARE_REGISTER_0
  • TIMER_B_CAPTURECOMPARE_REGISTER_1
  • TIMER_B_CAPTURECOMPARE_REGISTER_2
  • TIMER_B_CAPTURECOMPARE_REGISTER_3
  • TIMER_B_CAPTURECOMPARE_REGISTER_4
  • TIMER_B_CAPTURECOMPARE_REGISTER_5
  • TIMER_B_CAPTURECOMPARE_REGISTER_6

Referenced by Timer_B_outputPWM().


The documentation for this struct was generated from the following file:

Copyright 2015, Texas Instruments Incorporated