MSP430 DriverLib for MSP430FR5xx_6xx Devices  2.21.00.08
 All Data Structures Functions Variables Modules Pages
Timer_B_initCompareModeParam Struct Reference

Used in the Timer_B_initCompareMode() function as the param parameter. More...

#include <timer_b.h>

Data Fields

uint16_t compareRegister
 
uint16_t compareInterruptEnable
 
uint16_t compareOutputMode
 
uint16_t compareValue
 Is the count to be compared with in compare mode.
 

Detailed Description

Used in the Timer_B_initCompareMode() function as the param parameter.

Field Documentation

uint16_t Timer_B_initCompareModeParam::compareInterruptEnable

Is to enable or disable Timer_B capture compare interrupt.
Valid values are:

  • TIMER_B_CAPTURECOMPARE_INTERRUPT_DISABLE [Default]
  • TIMER_B_CAPTURECOMPARE_INTERRUPT_ENABLE

Referenced by Timer_B_initCompareMode().

uint16_t Timer_B_initCompareModeParam::compareOutputMode

Specifies the output mode.
Valid values are:

  • TIMER_B_OUTPUTMODE_OUTBITVALUE [Default]
  • TIMER_B_OUTPUTMODE_SET
  • TIMER_B_OUTPUTMODE_TOGGLE_RESET
  • TIMER_B_OUTPUTMODE_SET_RESET
  • TIMER_B_OUTPUTMODE_TOGGLE
  • TIMER_B_OUTPUTMODE_RESET
  • TIMER_B_OUTPUTMODE_TOGGLE_SET
  • TIMER_B_OUTPUTMODE_RESET_SET

Referenced by Timer_B_initCompareMode().

uint16_t Timer_B_initCompareModeParam::compareRegister

Selects the compare register being used. Refer to datasheet to ensure the device has the compare register being used.
Valid values are:

  • TIMER_B_CAPTURECOMPARE_REGISTER_0
  • TIMER_B_CAPTURECOMPARE_REGISTER_1
  • TIMER_B_CAPTURECOMPARE_REGISTER_2
  • TIMER_B_CAPTURECOMPARE_REGISTER_3
  • TIMER_B_CAPTURECOMPARE_REGISTER_4
  • TIMER_B_CAPTURECOMPARE_REGISTER_5
  • TIMER_B_CAPTURECOMPARE_REGISTER_6

Referenced by Timer_B_initCompareMode().


The documentation for this struct was generated from the following file:

Copyright 2015, Texas Instruments Incorporated