Used in the ADC12_B_init() function as the param parameter. More...
#include <adc12_b.h>
Data Fields | |
uint16_t | sampleHoldSignalSourceSelect |
uint8_t | clockSourceSelect |
uint16_t | clockSourceDivider |
uint16_t | clockSourcePredivider |
uint16_t | internalChannelMap |
Used in the ADC12_B_init() function as the param parameter.
uint16_t ADC12_B_initParam::clockSourceDivider |
Selects the amount that the clock will be divided.
Valid values are:
Referenced by ADC12_B_init().
uint16_t ADC12_B_initParam::clockSourcePredivider |
Selects the amount that the clock will be predivided.
Valid values are:
Referenced by ADC12_B_init().
uint8_t ADC12_B_initParam::clockSourceSelect |
Selects the clock that will be used by the ADC12B core, and the sampling timer if a sampling pulse mode is enabled.
Valid values are:
Referenced by ADC12_B_init().
uint16_t ADC12_B_initParam::internalChannelMap |
Selects what internal channel to map for ADC input channels
Valid values are:
Referenced by ADC12_B_init().
uint16_t ADC12_B_initParam::sampleHoldSignalSourceSelect |
Is the signal that will trigger a sample-and-hold for an input signal to be converted.
Valid values are:
Referenced by ADC12_B_init().