Functions | |
void | Graphics_drawPixelOnDisplay (const Graphics_Display *display, uint16_t x, uint16_t y, uint16_t value) |
void | Graphics_drawMultiplePixelsOnDisplay (const Graphics_Display *display, uint16_t x, uint16_t y, uint16_t x0, uint16_t count, uint16_t bPP, const uint8_t *data, const uint32_t *palette) |
void | Graphics_drawHorizontalLineOnDisplay (const Graphics_Display *display, uint16_t x1, uint16_t x2, uint16_t y, uint32_t value) |
void | Graphics_drawVerticalLineOnDisplay (const Graphics_Display *display, uint16_t x, uint16_t y1, uint16_t y2, uint16_t value) |
void | Graphics_fillRectangleOnDisplay (const Graphics_Display *display, const Graphics_Rectangle *rect, uint16_t value) |
uint32_t | Graphics_translateColorOnDisplay (const Graphics_Display *display, uint32_t value) |
void | Graphics_flushOnDisplay (const Graphics_Display *display) |
void | Graphics_clearDisplayOnDisplay (const Graphics_Display *display, uint16_t value) |
void Graphics_drawPixelOnDisplay | ( | const Graphics_Display * | display, |
uint16_t | x, | ||
uint16_t | y, | ||
uint16_t | value | ||
) |
Draws a pixel on a display.
display | is the pointer to the display driver structure for the display to operate upon. |
x | is the X coordinate of the pixel. |
y | is the Y coordinate of the pixel. |
value | is the color to draw the pixel. |
This function draws a pixel on a display. This assumes that clipping has already been performed.
References Graphics_Display::callPixelDraw, and Graphics_Display::displayData.
Referenced by Graphics_drawImage(), Graphics_drawLine(), Graphics_drawPixel(), and Graphics_drawString().
void Graphics_drawMultiplePixelsOnDisplay | ( | const Graphics_Display * | display, |
uint16_t | x, | ||
uint16_t | y, | ||
uint16_t | x0, | ||
uint16_t | count, | ||
uint16_t | bPP, | ||
const uint8_t * | data, | ||
const uint32_t * | palette | ||
) |
Draws a horizontal sequence of pixels on a display.
display | is the pointer to the display driver structure for the display to operate upon. |
x | is the X coordinate of the first pixel. |
y | is the Y coordinate of the first pixel. |
x0 | is sub-pixel offset within the pixel data, which is valid for 1 or 4 bit per pixel formats. |
count | is the number of pixels to draw. |
bPP | is the number of bits per pixel; must be 1, 4, or 8. |
data | is a pointer to the pixel data. For 1 and 4 bit per pixel formats, the most significant bit(s) represent the left-most pixel. |
palette | is a pointer to the palette used to draw the pixels. |
This function draws a horizontal sequence of pixels on a display, using the supplied palette. For 1 bit per pixel format, the palette contains pre-translated colors; for 4 and 8 bit per pixel formats, the palette contains 24-bit RGB values that must be translated before being written to the display.
References Graphics_Display::callPixelDrawMultiple, and Graphics_Display::displayData.
Referenced by Graphics_drawImage().
void Graphics_drawHorizontalLineOnDisplay | ( | const Graphics_Display * | display, |
uint16_t | x1, | ||
uint16_t | x2, | ||
uint16_t | y, | ||
uint32_t | value | ||
) |
Draws a horizontal line on a display.
display | is the pointer to the display driver structure for the display to operate upon. |
x1 | is the starting X coordinate of the line. |
x2 | is the ending X coordinate of the line. |
y | is the Y coordinate of the line. |
value | is the color to draw the line. |
This function draws a horizontal line on a display. This assumes that clipping has already been performed, and that both end points of the line are within the extents of the display.
References Graphics_Display::callLineDrawH, and Graphics_Display::displayData.
Referenced by Graphics_drawLineH().
void Graphics_drawVerticalLineOnDisplay | ( | const Graphics_Display * | display, |
uint16_t | x, | ||
uint16_t | y1, | ||
uint16_t | y2, | ||
uint16_t | value | ||
) |
Draws a vertical line on a display.
display | is the pointer to the display driver structure for the display to operate upon. |
x | is the X coordinate of the line. |
y1 | is the starting Y coordinate of the line. |
y2 | is the ending Y coordinate of the line. |
value | is the color to draw the line. |
This function draws a vertical line on a display. This assumes that clipping has already been performed, and that both end points of the line are within the extents of the display.
References Graphics_Display::callLineDrawV, and Graphics_Display::displayData.
Referenced by Graphics_drawLineV().
void Graphics_fillRectangleOnDisplay | ( | const Graphics_Display * | display, |
const Graphics_Rectangle * | rect, | ||
uint16_t | value | ||
) |
Fills a rectangle on a display.
display | is the pointer to the display driver structure for the display to operate upon. |
rect | is a pointer to the structure describing the rectangle to fill. |
value | is the color to fill the rectangle. |
This function fills a rectangle on the display. This assumes that clipping has already been performed, and that all sides of the rectangle are within the extents of the display.
References Graphics_Display::callRectFill, and Graphics_Display::displayData.
Referenced by Graphics_fillRectangle().
uint32_t Graphics_translateColorOnDisplay | ( | const Graphics_Display * | display, |
uint32_t | value | ||
) |
Translates a 24-bit RGB color to a display driver-specific color.
display | is the pointer to the display driver structure for the display to operate upon. |
value | is the 24-bit RGB color. The least-significant byte is the blue channel, the next byte is the green channel, and the third byte is the red channel. |
This function translates a 24-bit RGB color into a value that can be written into the display's frame buffer in order to reproduce that color, or the closest possible approximation of that color.
References Graphics_Display::callColorTranslate.
Referenced by Graphics_setBackgroundColor(), and Graphics_setForegroundColor().
void Graphics_flushOnDisplay | ( | const Graphics_Display * | display) |
Flushes cached drawing operations.
display | is the pointer to the display driver structure for the display to operate upon. |
This function flushes any cached drawing operations on a display.
References Graphics_Display::callFlush, and Graphics_Display::displayData.
Referenced by Graphics_flushBuffer().
void Graphics_clearDisplayOnDisplay | ( | const Graphics_Display * | display, |
uint16_t | value | ||
) |
Forces a clear Display.
display | is the pointer to the display driver structure for the display to operate upon. |
value | is the current background color to fill the screen with. |
This function clears the Display
References Graphics_Display::callClearDisplay, and Graphics_Display::displayData.
Referenced by Graphics_clearDisplay().