Data Fields
Graphics_Display Struct Reference

This structure defines the characteristics of a display driver. More...

#include <grlib.h>

Data Fields

int32_t size
 The size of this structure. More...
 
void * displayData
 A pointer to display driver-specific data. More...
 
uint16_t width
 The width of this display. More...
 
uint16_t heigth
 The height of this display. More...
 
void(* callPixelDraw )(void *displayData, int16_t x, int16_t y, uint16_t value)
 A pointer to the function to draw a pixel on this display. More...
 
void(* callPixelDrawMultiple )(void *displayData, int16_t x, int16_t y, int16_t x0, int16_t count, int16_t bPP, const uint8_t *data, const uint32_t *pucPalette)
 A pointer to the function to draw multiple pixels on this display. More...
 
void(* callLineDrawH )(void *displayData, int16_t x1, int16_t x2, int16_t y, uint16_t value)
 A pointer to the function to draw a horizontal line on this display. More...
 
void(* callLineDrawV )(void *displayData, int16_t x, int16_t y1, int16_t y2, uint16_t value)
 A pointer to the function to draw a vertical line on this display. More...
 
void(* callRectFill )(void *displayData, const Graphics_Rectangle *rect, uint16_t value)
 A pointer to the function to draw a filled rectangle on this display. More...
 
uint32_t(* callColorTranslate )(void *displayData, uint32_t value)
 A pointer to the function to translate 24-bit RGB colors to display-specific colors. More...
 
void(* callFlush )(void *displayData)
 A pointer to the function to flush any cached drawing operations on this display. More...
 
void(* callClearDisplay )(void *displayData, uint16_t value)
 A pointer to the function to clears Display. Contents of display buffer unmodified. More...
 

Detailed Description

This structure defines the characteristics of a display driver.

Field Documentation

int32_t Graphics_Display::size

The size of this structure.

void* Graphics_Display::displayData
uint16_t Graphics_Display::width

The width of this display.

Referenced by Graphics_getDisplayWidth(), Graphics_getWidthOfDisplay(), and Graphics_initContext().

uint16_t Graphics_Display::heigth

The height of this display.

Referenced by Graphics_getDisplayHeight(), Graphics_getHeightOfDisplay(), and Graphics_initContext().

void(* Graphics_Display::callPixelDraw)(void *displayData, int16_t x, int16_t y, uint16_t value)

A pointer to the function to draw a pixel on this display.

Referenced by Graphics_drawPixelOnDisplay().

void(* Graphics_Display::callPixelDrawMultiple)(void *displayData, int16_t x, int16_t y, int16_t x0, int16_t count, int16_t bPP, const uint8_t *data, const uint32_t *pucPalette)

A pointer to the function to draw multiple pixels on this display.

Referenced by Graphics_drawMultiplePixelsOnDisplay().

void(* Graphics_Display::callLineDrawH)(void *displayData, int16_t x1, int16_t x2, int16_t y, uint16_t value)

A pointer to the function to draw a horizontal line on this display.

Referenced by Graphics_drawHorizontalLineOnDisplay().

void(* Graphics_Display::callLineDrawV)(void *displayData, int16_t x, int16_t y1, int16_t y2, uint16_t value)

A pointer to the function to draw a vertical line on this display.

Referenced by Graphics_drawVerticalLineOnDisplay().

void(* Graphics_Display::callRectFill)(void *displayData, const Graphics_Rectangle *rect, uint16_t value)

A pointer to the function to draw a filled rectangle on this display.

Referenced by Graphics_fillRectangleOnDisplay().

uint32_t(* Graphics_Display::callColorTranslate)(void *displayData, uint32_t value)

A pointer to the function to translate 24-bit RGB colors to display-specific colors.

Referenced by Graphics_translateColorOnDisplay().

void(* Graphics_Display::callFlush)(void *displayData)

A pointer to the function to flush any cached drawing operations on this display.

Referenced by Graphics_flushOnDisplay().

void(* Graphics_Display::callClearDisplay)(void *displayData, uint16_t value)

A pointer to the function to clears Display. Contents of display buffer unmodified.

Referenced by Graphics_clearDisplayOnDisplay().


The documentation for this struct was generated from the following file:

Copyright 2015, Texas Instruments Incorporated