#include "inc/hw_types.h"
#include "driverlib/5xx_6xx/debug.h"
#include "driverlib/5xx_6xx/timerd.h"
#include "driverlib/5xx_6xx/tlv.h"
#include "deprecated/CCS/msp430xgeneric.h"
Functions | |
void | privateTimerDProcessClockSourceDivider (unsigned int baseAddress, unsigned int clockSourceDivider) |
void | TimerD_startCounter (unsigned int baseAddress, unsigned int timerMode) |
void | TimerD_configureContinuousMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int clockingMode, unsigned int timerInterruptEnable_TDIE, unsigned int timerClear) |
void | TimerD_configureUpMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int clockingMode, unsigned int timerPeriod, unsigned int timerInterruptEnable_TDIE, unsigned int captureCompareInterruptEnable_CCR0_CCIE, unsigned int timerClear) |
void | TimerD_configureUpDownMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int clockingMode, unsigned int timerPeriod, unsigned int timerInterruptEnable_TDIE, unsigned int captureCompareInterruptEnable_CCR0_CCIE, unsigned int timerClear) |
void | TimerD_initCapture (unsigned int baseAddress, unsigned int captureRegister, unsigned int captureMode, unsigned int captureInputSelect, unsigned short synchronizeCaptureSource, unsigned short captureInterruptEnable, unsigned int captureOutputMode, unsigned char channelCaptureMode) |
void | TimerD_initCompare (unsigned int baseAddress, unsigned int compareRegister, unsigned short compareInterruptEnable, unsigned int compareOutputMode, unsigned int compareValue) |
void | TimerD_enableTimerInterrupt (unsigned int baseAddress) |
void | TimerD_enableHighResInterrupt (unsigned int baseAddress, unsigned int mask) |
void | TimerD_disableTimerInterrupt (unsigned int baseAddress) |
void | TimerD_disableHighResInterrupt (unsigned int baseAddress, unsigned int mask) |
unsigned long | TimerD_getTimerInterruptStatus (unsigned int baseAddress) |
void | TimerD_enableCaptureCompareInterrupt (unsigned int baseAddress, unsigned int captureCompareRegister) |
void | TimerD_disableCaptureCompareInterrupt (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned long | TimerD_getCaptureCompareInterruptStatus (unsigned int baseAddress, unsigned int captureCompareRegister, unsigned int mask) |
unsigned int | TimerD_getHighResInterruptStatus (unsigned int baseAddress, unsigned int mask) |
void | TimerD_clear (unsigned int baseAddress) |
void | TimerD_clearHighResInterruptStatus (unsigned int baseAddress, unsigned int mask) |
unsigned short | TimerD_getSynchronizedCaptureCompareInput (unsigned int baseAddress, unsigned int captureCompareRegister, unsigned short synchronized) |
unsigned char | TimerD_getOutputForOutputModeOutBitValue (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned int | TimerD_getCaptureCompareCount (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned int | TimerD_getCaptureCompareLatchCount (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned char | TimerD_getCaptureCompareInputSignal (unsigned int baseAddress, unsigned int captureCompareRegister) |
void | TimerD_setOutputForOutputModeOutBitValue (unsigned int baseAddress, unsigned int captureCompareRegister, unsigned char outputModeOutBitValue) |
void | TimerD_generatePWM (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int clockingMode, unsigned int timerPeriod, unsigned int compareRegister, unsigned int compareOutputMode, unsigned int dutyCycle) |
void | TimerD_stop (unsigned int baseAddress) |
void | TimerD_setCompareValue (unsigned int baseAddress, unsigned int compareRegister, unsigned int compareValue) |
void | TimerD_clearTimerInterruptFlag (unsigned int baseAddress) |
void | TimerD_clearCaptureCompareInterruptFlag (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned char | TimerD_configureHighResGeneratorInFreeRunningMode (unsigned int baseAddress, unsigned char desiredHighResFrequency) |
void | TimerD_configureHighResGeneratorInRegulatedMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int clockingMode, unsigned char highResClockMultiplyFactor, unsigned char highResClockDivider) |
void | TimerD_combineTDCCRToGeneratePWM (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int clockingMode, unsigned int timerPeriod, unsigned int combineCCRRegistersCombination, unsigned int compareOutputMode, unsigned int dutyCycle1, unsigned int dutyCycle2) |
void | TimerD_selectLatchingGroup (unsigned int baseAddress, unsigned int groupLatch) |
void | TimerD_selectCounterLength (unsigned int baseAddress, unsigned int counterLength) |
void | TimerD_initCompareLatchLoadEvent (unsigned int baseAddress, unsigned int compareRegister, unsigned int compareLatchLoadEvent) |
void | TimerD_disableHighResFastWakeup (unsigned int baseAddress) |
void | TimerD_enableHighResFastWakeup (unsigned int baseAddress) |
void | TimerD_disableHighResClockEnhancedAccuracy (unsigned int baseAddress) |
void | TimerD_enableHighResClockEnhancedAccuracy (unsigned int baseAddress) |
void | TimerD_DisableHighResGeneratorForceON (unsigned int baseAddress) |
void | TimerD_EnableHighResGeneratorForceON (unsigned int baseAddress) |
void | TimerD_selectHighResCoarseClockRange (unsigned int baseAddress, unsigned int highResCoarseClockRange) |
void | TimerD_selectHighResClockRange (unsigned int baseAddress, unsigned int highResClockRange) |
void privateTimerDProcessClockSourceDivider | ( | unsigned int | baseAddress, |
unsigned int | clockSourceDivider | ||
) |
Private clock source divider helper function
baseAddress | is the base address of the Timer module. |
clockSourceDivider | is the desired divider for the clock source |
Modified registers are TDxCTL1, TDxCTL0
References HWREG, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, and TIMERD_CLOCKSOURCE_DIVIDER_8.
Referenced by TimerD_combineTDCCRToGeneratePWM(), TimerD_configureContinuousMode(), TimerD_configureHighResGeneratorInRegulatedMode(), TimerD_configureUpDownMode(), TimerD_configureUpMode(), and TimerD_generatePWM().
void TimerD_startCounter | ( | unsigned int | baseAddress, |
unsigned int | timerMode | ||
) |
Starts TimerD counter
baseAddress | is the base address of the TimerA module. |
clockSource | selects Clock source. Valid values are TIMERD_CONTINUOUS_MODE [Default value] TIMERD_UPDOWN_MODE TIMERD_UP_MODE Modified register is TDxCTL0 |
NOTE: This function assumes that the timer has been previously configured using TimerD_configureContinuousMode, TimerD_configureUpMode or TimerD_configureUpDownMode.
References ASSERT, HWREG, TIMERA_CONTINUOUS_MODE, TIMERA_UP_MODE, and TIMERA_UPDOWN_MODE.
void TimerD_configureContinuousMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | clockingMode, | ||
unsigned int | timerInterruptEnable_TDIE, | ||
unsigned int | timerClear | ||
) |
Configures timer in continuous mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMERD_CLOCKSOURCE_EXTERNAL_TDCLK [Default value] TIMERD_CLOCKSOURCE_ACLK TIMERD_CLOCKSOURCE_SMCLK TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMERD_CLOCKSOURCE_DIVIDER_1 [Default value] TIMERD_CLOCKSOURCE_DIVIDER_2 TIMERD_CLOCKSOURCE_DIVIDER_4 TIMERD_CLOCKSOURCE_DIVIDER_8 TIMERD_CLOCKSOURCE_DIVIDER_3 TIMERD_CLOCKSOURCE_DIVIDER_5 TIMERD_CLOCKSOURCE_DIVIDER_6 TIMERD_CLOCKSOURCE_DIVIDER_7 TIMERD_CLOCKSOURCE_DIVIDER_10 TIMERD_CLOCKSOURCE_DIVIDER_12 TIMERD_CLOCKSOURCE_DIVIDER_14 TIMERD_CLOCKSOURCE_DIVIDER_16 TIMERD_CLOCKSOURCE_DIVIDER_20 TIMERD_CLOCKSOURCE_DIVIDER_24 TIMERD_CLOCKSOURCE_DIVIDER_28 TIMERD_CLOCKSOURCE_DIVIDER_32 TIMERD_CLOCKSOURCE_DIVIDER_40 TIMERD_CLOCKSOURCE_DIVIDER_48 TIMERD_CLOCKSOURCE_DIVIDER_56 TIMERD_CLOCKSOURCE_DIVIDER_64 |
clockingMode | is the selected clock mode register values. Valid values are TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK [Default value] TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK TIMERD_CLOCKINGMODE_AUXILIARY_CLK |
timerInterruptEnable_TDIE | is to enable or disable timer interrupt Valid values are TIMERD_TDIE_INTERRUPT_ENABLE TIMERD_TDIE_INTERRUPT_DISABLE [Default value] |
timerClear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMERD_DO_CLEAR TIMERD_SKIP_CLEAR [Default value] |
Modified registers are TDxCTL0 and TDxCTL1
This API does not start the timer. Timer needs to be started when required using the TimerD_start API.
References ASSERT, HWREG, privateTimerDProcessClockSourceDivider(), TIMERD_CLOCKINGMODE_AUXILIARY_CLK, TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK, TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK, TIMERD_CLOCKSOURCE_ACLK, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, TIMERD_CLOCKSOURCE_DIVIDER_8, TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK, TIMERD_CLOCKSOURCE_SMCLK, TIMERD_CONTINUOUS_MODE, TIMERD_DO_CLEAR, TIMERD_SKIP_CLEAR, TIMERD_STOP_MODE, TIMERD_TDIE_INTERRUPT_DISABLE, and TIMERD_TDIE_INTERRUPT_ENABLE.
void TimerD_configureUpMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | clockingMode, | ||
unsigned int | timerPeriod, | ||
unsigned int | timerInterruptEnable_TDIE, | ||
unsigned int | captureCompareInterruptEnable_CCR0_CCIE, | ||
unsigned int | timerClear | ||
) |
Configures timer in up mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMERD_CLOCKSOURCE_EXTERNAL_TDCLK [Default value] TIMERD_CLOCKSOURCE_ACLK TIMERD_CLOCKSOURCE_SMCLK TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMERD_CLOCKSOURCE_DIVIDER_1 [Default value] TIMERD_CLOCKSOURCE_DIVIDER_2 TIMERD_CLOCKSOURCE_DIVIDER_4 TIMERD_CLOCKSOURCE_DIVIDER_8 TIMERD_CLOCKSOURCE_DIVIDER_3 TIMERD_CLOCKSOURCE_DIVIDER_5 TIMERD_CLOCKSOURCE_DIVIDER_6 TIMERD_CLOCKSOURCE_DIVIDER_7 TIMERD_CLOCKSOURCE_DIVIDER_10 TIMERD_CLOCKSOURCE_DIVIDER_12 TIMERD_CLOCKSOURCE_DIVIDER_14 TIMERD_CLOCKSOURCE_DIVIDER_16 TIMERD_CLOCKSOURCE_DIVIDER_20 TIMERD_CLOCKSOURCE_DIVIDER_24 TIMERD_CLOCKSOURCE_DIVIDER_28 TIMERD_CLOCKSOURCE_DIVIDER_32 TIMERD_CLOCKSOURCE_DIVIDER_40 TIMERD_CLOCKSOURCE_DIVIDER_48 TIMERD_CLOCKSOURCE_DIVIDER_56 TIMERD_CLOCKSOURCE_DIVIDER_64 |
clockingMode | is the selected clock mode register values. Valid values are TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK [Default value] TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK TIMERD_CLOCKINGMODE_AUXILIARY_CLK |
timerPeriod | is the specified timer period. This is the value that gets written into the CCR0. Limited to 16 bits[unsigned int] |
timerInterruptEnable_TDIE | is to enable or disable timer interrupt Valid values are TIMERD_TDIE_INTERRUPT_ENABLE and TIMERD_TDIE_INTERRUPT_DISABLE [Default value] |
captureCompareInterruptEnable_CCR0_CCIE | is to enable or disable timer CCR0 captureComapre interrupt. Valid values are TIMERD_CCIE_CCR0_INTERRUPT_ENABLE and TIMERD_CCIE_CCR0_INTERRUPT_DISABLE [Default value] |
timerClear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMERD_DO_CLEAR TIMERD_SKIP_CLEAR [Default value] |
Modified registers are TDxCTL0, TDxCTL1,TDxCCR0, TDxCCTL0
This API does not start the timer. Timer needs to be started when required using the TimerD_start API.
References ASSERT, HWREG, privateTimerDProcessClockSourceDivider(), TIMERD_CCIE_CCR0_INTERRUPT_ENABLE, TIMERD_CLOCKINGMODE_AUXILIARY_CLK, TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK, TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK, TIMERD_CLOCKSOURCE_ACLK, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, TIMERD_CLOCKSOURCE_DIVIDER_8, TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK, TIMERD_CLOCKSOURCE_SMCLK, TIMERD_DO_CLEAR, TIMERD_SKIP_CLEAR, TIMERD_STOP_MODE, TIMERD_TDIE_INTERRUPT_ENABLE, and TIMERD_UPDOWN_MODE.
void TimerD_configureUpDownMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | clockingMode, | ||
unsigned int | timerPeriod, | ||
unsigned int | timerInterruptEnable_TDIE, | ||
unsigned int | captureCompareInterruptEnable_CCR0_CCIE, | ||
unsigned int | timerClear | ||
) |
Configures timer in up down mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMERD_CLOCKSOURCE_EXTERNAL_TDCLK [Default value] TIMERD_CLOCKSOURCE_ACLK TIMERD_CLOCKSOURCE_SMCLK TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMERD_CLOCKSOURCE_DIVIDER_1 [Default value] TIMERD_CLOCKSOURCE_DIVIDER_2 TIMERD_CLOCKSOURCE_DIVIDER_4 TIMERD_CLOCKSOURCE_DIVIDER_8 TIMERD_CLOCKSOURCE_DIVIDER_3 TIMERD_CLOCKSOURCE_DIVIDER_5 TIMERD_CLOCKSOURCE_DIVIDER_6 TIMERD_CLOCKSOURCE_DIVIDER_7 TIMERD_CLOCKSOURCE_DIVIDER_10 TIMERD_CLOCKSOURCE_DIVIDER_12 TIMERD_CLOCKSOURCE_DIVIDER_14 TIMERD_CLOCKSOURCE_DIVIDER_16 TIMERD_CLOCKSOURCE_DIVIDER_20 TIMERD_CLOCKSOURCE_DIVIDER_24 TIMERD_CLOCKSOURCE_DIVIDER_28 TIMERD_CLOCKSOURCE_DIVIDER_32 TIMERD_CLOCKSOURCE_DIVIDER_40 TIMERD_CLOCKSOURCE_DIVIDER_48 TIMERD_CLOCKSOURCE_DIVIDER_56 TIMERD_CLOCKSOURCE_DIVIDER_64 |
clockingMode | is the selected clock mode register values. Valid values are TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK [Default value] TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK TIMERD_CLOCKINGMODE_AUXILIARY_CLK |
timerPeriod | is the specified timer period |
timerInterruptEnable_TDIE | is to enable or disable timer interrupt Valid values are TIMERD_TDIE_INTERRUPT_ENABLE TIMERD_TDIE_INTERRUPT_DISABLE [Default value] |
captureCompareInterruptEnable_CCR0_CCIE | is to enable or disable timer CCR0 captureComapre interrupt. Valid values are TIMERD_CCIE_CCR0_INTERRUPT_ENABLE and TIMERD_CCIE_CCR0_INTERRUPT_DISABLE [Default value] |
timerClear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMERD_DO_CLEAR TIMERD_SKIP_CLEAR [Default value] |
Modified registers are TDxCTL0, TDxCTL1, TDxCCR0, TDxCCTL0
This API does not start the timer. Timer needs to be started when required using the TimerD_start API.
References ASSERT, HWREG, privateTimerDProcessClockSourceDivider(), TIMERD_CCIE_CCR0_INTERRUPT_ENABLE, TIMERD_CLOCKINGMODE_AUXILIARY_CLK, TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK, TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK, TIMERD_CLOCKSOURCE_ACLK, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, TIMERD_CLOCKSOURCE_DIVIDER_8, TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK, TIMERD_CLOCKSOURCE_SMCLK, TIMERD_DO_CLEAR, TIMERD_SKIP_CLEAR, TIMERD_STOP_MODE, TIMERD_TDIE_INTERRUPT_ENABLE, and TIMERD_UPDOWN_MODE.
void TimerD_initCapture | ( | unsigned int | baseAddress, |
unsigned int | captureRegister, | ||
unsigned int | captureMode, | ||
unsigned int | captureInputSelect, | ||
unsigned short | synchronizeCaptureSource, | ||
unsigned short | captureInterruptEnable, | ||
unsigned int | captureOutputMode, | ||
unsigned char | channelCaptureMode | ||
) |
Initializes Capture Mode
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
captureMode | is the capture mode selected. Valid values are TIMERD_CAPTUREMODE_NO_CAPTURE [Default value] TIMERD_CAPTUREMODE_RISING_EDGE TIMERD_CAPTUREMODE_FALLING_EDGE TIMERD_CAPTUREMODE_RISING_AND_FALLING_EDGE |
captureInputSelect | decides the Input Select TIMERD_CAPTURE_INPUTSELECT_CCIxA [Default value] TIMERD_CAPTURE_INPUTSELECT_CCIxB TIMERD_CAPTURE_INPUTSELECT_GND TIMERD_CAPTURE_INPUTSELECT_Vcc |
synchronizeCaptureSource | decides if capture source should be synchronized with timer clock Valid values are TIMERD_CAPTURE_ASYNCHRONOUS [Default value] TIMERD_CAPTURE_SYNCHRONOUS |
captureInterruptEnable | is to enable or disable timer captureComapre interrupt. Valid values are TIMERD_CAPTURECOMPARE_INTERRUPT_DISABLE [Default value] TIMERD_CAPTURECOMPARE_INTERRUPT_ENABLE |
captureOutputMode | specifies the output mode. Valid values are TIMERD_OUTPUTMODE_OUTBITVALUE [Default value], TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_TOGGLE_RESET, TIMERD_OUTPUTMODE_SET_RESET TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_TOGGLE_SET, TIMERD_OUTPUTMODE_RESET_SET |
channelCaptureMode | specifies single/dual capture mode. Valid values are TIMERD_SINGLE_CAPTURE_MODE [Default value], TIMERD_DUAL_CAPTURE_MODE |
Modified registers are TDxCTL2, TDxCCTLn
References ASSERT, HWREG, HWREGB, TIMERD_CAPTURE_ASYNCHRONOUS, TIMERD_CAPTURE_INPUTSELECT_CCIxA, TIMERD_CAPTURE_INPUTSELECT_CCIxB, TIMERD_CAPTURE_INPUTSELECT_GND, TIMERD_CAPTURE_INPUTSELECT_Vcc, TIMERD_CAPTURE_SYNCHRONOUS, TIMERD_CAPTURECOMPARE_INTERRUPT_DISABLE, TIMERD_CAPTURECOMPARE_INTERRUPT_ENABLE, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, TIMERD_CAPTURECOMPARE_REGISTER_6, TIMERD_CAPTUREMODE_FALLING_EDGE, TIMERD_CAPTUREMODE_NO_CAPTURE, TIMERD_CAPTUREMODE_RISING_AND_FALLING_EDGE, TIMERD_CAPTUREMODE_RISING_EDGE, TIMERD_DO_CLEAR, TIMERD_DUAL_CAPTURE_MODE, TIMERD_OUTPUTMODE_OUTBITVALUE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_RESET_SET, TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_SET_RESET, TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_TOGGLE_RESET, TIMERD_OUTPUTMODE_TOGGLE_SET, TIMERD_SINGLE_CAPTURE_MODE, and TIMERD_TDIE_INTERRUPT_ENABLE.
void TimerD_initCompare | ( | unsigned int | baseAddress, |
unsigned int | compareRegister, | ||
unsigned short | compareInterruptEnable, | ||
unsigned int | compareOutputMode, | ||
unsigned int | compareValue | ||
) |
Initializes Compare Mode
baseAddress | is the base address of the Timer module. |
compareRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
compareInterruptEnable | is to enable or disable timer captureComapre interrupt. Valid values are TIMERD_CAPTURECOMPARE_INTERRUPT_ENABLE and TIMERD_CAPTURECOMPARE_INTERRUPT_DISABLE [Default value] |
compareOutputMode | specifies the ouput mode. Valid values are TIMERD_OUTPUTMODE_OUTBITVALUE [Default value], TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_TOGGLE_RESET, TIMERD_OUTPUTMODE_SET_RESET TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_TOGGLE_SET, TIMERD_OUTPUTMODE_RESET_SET |
compareValue | is the count to be compared with in compare mode |
Modified register is TDxCCTLn and TDxCCRn
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_INTERRUPT_DISABLE, TIMERD_CAPTURECOMPARE_INTERRUPT_ENABLE, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, TIMERD_CAPTURECOMPARE_REGISTER_6, TIMERD_OUTPUTMODE_OUTBITVALUE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_RESET_SET, TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_SET_RESET, TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_TOGGLE_RESET, and TIMERD_OUTPUTMODE_TOGGLE_SET.
void TimerD_enableTimerInterrupt | ( | unsigned int | baseAddress | ) |
Enable timer interrupt
baseAddress | is the base address of the Timer module. |
Modified register is TDxCTL0
References HWREGB.
void TimerD_enableHighResInterrupt | ( | unsigned int | baseAddress, |
unsigned int | mask | ||
) |
Enable High Resolution interrupt
baseAddress | is the base address of the Timer module. |
mask | is the mask for the interrupt status Valid values is an OR of TIMERD_HIGH_RES_FREQUENCY_UNLOCK, TIMERD_HIGH_RES_FREQUENCY_LOCK TIMERD_HIGH_RES_FAIL_HIGH, TIMERD_HIGH_RES_FAIL_LOW |
Modified register is TDxHINT
References HWREG.
void TimerD_disableTimerInterrupt | ( | unsigned int | baseAddress | ) |
Disable timer interrupt
baseAddress | is the base address of the Timer module. |
Modified register is TDxCTL0
References HWREGB.
void TimerD_disableHighResInterrupt | ( | unsigned int | baseAddress, |
unsigned int | mask | ||
) |
Disable High Resolution interrupt
baseAddress | is the base address of the Timer module. |
mask | is the mask for the interrupt status Valid values is an OR of TIMERD_HIGH_RES_FREQUENCY_UNLOCK, TIMERD_HIGH_RES_FREQUENCY_LOCK TIMERD_HIGH_RES_FAIL_HIGH, TIMERD_HIGH_RES_FAIL_LOW |
Modified register is TDxHINT
References HWREG.
unsigned long TimerD_getTimerInterruptStatus | ( | unsigned int | baseAddress | ) |
Get timer interrupt status
baseAddress | is the base address of the Timer module. |
References HWREGB.
void TimerD_enableCaptureCompareInterrupt | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Enable capture compare interrupt
baseAddress | is the base address of the Timer module. |
captureCompareRegister | is the selected capture compare regsiter |
Modified register is TDxCCTLn
References ASSERT, HWREG, HWREGB, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
void TimerD_disableCaptureCompareInterrupt | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Disable capture compare interrupt
baseAddress | is the base address of the Timer module. |
captureCompareRegister | is the selected capture compare regsiter |
Modified register is TDxCCTLn
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
unsigned long TimerD_getCaptureCompareInterruptStatus | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister, | ||
unsigned int | mask | ||
) |
Return capture compare interrupt status
baseAddress | is the base address of the Timer module. |
captureCompareRegister | is the selected capture compare register |
mask | is the mask for the interrupt status Valid values is an OR of TIMERD_CAPTURE_OVERFLOW, TIMERD_CAPTURECOMPARE_INTERRUPT_FLAG |
References HWREG.
unsigned int TimerD_getHighResInterruptStatus | ( | unsigned int | baseAddress, |
unsigned int | mask | ||
) |
Returns High Resolution interrupt status
baseAddress | is the base address of the Timer module. |
mask | is the mask for the interrupt status Valid values is an OR of TIMERD_HIGH_RES_FREQUENCY_UNLOCK, TIMERD_HIGH_RES_FREQUENCY_LOCK TIMERD_HIGH_RES_FAIL_HIGH, TIMERD_HIGH_RES_FAIL_LOW |
Modified register is TDxHINT
References HWREG.
void TimerD_clear | ( | unsigned int | baseAddress | ) |
Reset/Clear the timer clock divider, count direction, count
baseAddress | is the base address of the Timer module. |
Modified register is TDxCTL0
References HWREG.
void TimerD_clearHighResInterruptStatus | ( | unsigned int | baseAddress, |
unsigned int | mask | ||
) |
Clears High Resolution interrupt status
baseAddress | is the base address of the Timer module. |
mask | is the mask for the interrupt status Valid values is an OR of TIMERD_HIGH_RES_FREQUENCY_UNLOCK, TIMERD_HIGH_RES_FREQUENCY_LOCK TIMERD_HIGH_RES_FAIL_HIGH, TIMERD_HIGH_RES_FAIL_LOW |
Modified register is TDxHINT
References HWREG.
unsigned short TimerD_getSynchronizedCaptureCompareInput | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister, | ||
unsigned short | synchronized | ||
) |
Get synchrnozied capturecompare input
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
synchronized | is to select type of capture compare input. Valid values are TIMERD_READ_CAPTURE_COMPARE_INPUT TIMERD_READ_SYNCHRONIZED_CAPTURECOMPAREINPUT |
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_INPUT_HIGH, TIMERD_CAPTURECOMPARE_INPUT_LOW, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, TIMERD_CAPTURECOMPARE_REGISTER_6, TIMERD_READ_CAPTURE_COMPARE_INPUT, and TIMERD_READ_SYNCHRONIZED_CAPTURECOMPAREINPUT.
unsigned char TimerD_getOutputForOutputModeOutBitValue | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Get ouput bit for output mode
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, TIMERD_CAPTURECOMPARE_REGISTER_6, TIMERD_OUTPUTMODE_OUTBITVALUE_HIGH, and TIMERD_OUTPUTMODE_OUTBITVALUE_LOW.
unsigned int TimerD_getCaptureCompareCount | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Get current capturecompare count
baseAddress | is the base address of the Timer module. |
captureCompareRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
unsigned int TimerD_getCaptureCompareLatchCount | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Get current capture compare latch register count
baseAddress | is the base address of the Timer module. |
captureCompareRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
unsigned char TimerD_getCaptureCompareInputSignal | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Get current capturecompare input signal
baseAddress | is the base address of the Timer module. |
captureCompareRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
References ASSERT, HWREGB, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
void TimerD_setOutputForOutputModeOutBitValue | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister, | ||
unsigned char | outputModeOutBitValue | ||
) |
Set ouput bit for output mode
baseAddress | is the base address of the Timer module. |
captureCompareRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
outputModeOutBitValueis | the value to be set for out bit Valid values are TIMERD_OUTPUTMODE_OUTBITVALUE_HIGH TIMERD_OUTPUTMODE_OUTBITVALUE_LOW |
Modified register is TDxCCTLn
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, TIMERD_CAPTURECOMPARE_REGISTER_6, TIMERD_OUTPUTMODE_OUTBITVALUE_HIGH, and TIMERD_OUTPUTMODE_OUTBITVALUE_LOW.
void TimerD_generatePWM | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | clockingMode, | ||
unsigned int | timerPeriod, | ||
unsigned int | compareRegister, | ||
unsigned int | compareOutputMode, | ||
unsigned int | dutyCycle | ||
) |
Generate a PWM with timer running in up down mode
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMERD_CLOCKSOURCE_EXTERNAL_TDCLK [Default value] TIMERD_CLOCKSOURCE_ACLK TIMERD_CLOCKSOURCE_SMCLK TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMERD_CLOCKSOURCE_DIVIDER_1 [Default value] TIMERD_CLOCKSOURCE_DIVIDER_2 TIMERD_CLOCKSOURCE_DIVIDER_4 TIMERD_CLOCKSOURCE_DIVIDER_8 TIMERD_CLOCKSOURCE_DIVIDER_3 TIMERD_CLOCKSOURCE_DIVIDER_5 TIMERD_CLOCKSOURCE_DIVIDER_6 TIMERD_CLOCKSOURCE_DIVIDER_7 TIMERD_CLOCKSOURCE_DIVIDER_10 TIMERD_CLOCKSOURCE_DIVIDER_12 TIMERD_CLOCKSOURCE_DIVIDER_14 TIMERD_CLOCKSOURCE_DIVIDER_16 TIMERD_CLOCKSOURCE_DIVIDER_20 TIMERD_CLOCKSOURCE_DIVIDER_24 TIMERD_CLOCKSOURCE_DIVIDER_28 TIMERD_CLOCKSOURCE_DIVIDER_32 TIMERD_CLOCKSOURCE_DIVIDER_40 TIMERD_CLOCKSOURCE_DIVIDER_48 TIMERD_CLOCKSOURCE_DIVIDER_56 TIMERD_CLOCKSOURCE_DIVIDER_64 |
clockingMode | is the selected clock mode register values. Valid values are TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK [Default value] TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK TIMERD_CLOCKINGMODE_AUXILIARY_CLK |
timerPeriod | selects the desired timer period |
compareRegister | selects the compare register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
compareOutputMode | specifies the ouput mode. Valid values are TIMERD_OUTPUTMODE_OUTBITVALUE, TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_TOGGLE_RESET, TIMERD_OUTPUTMODE_SET_RESET TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_TOGGLE_SET, TIMERD_OUTPUTMODE_RESET_SET |
dutyCycle | specifies the dutycycle for the generated waveform |
Modified registers are TDxCTL0, TDxCTL1, TDxCCR0, TDxCCTL0,TDxCCTLn
References ASSERT, HWREG, privateTimerDProcessClockSourceDivider(), TIMERD_CAPTURECOMPARE_INTERRUPT_ENABLE, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, TIMERD_CAPTURECOMPARE_REGISTER_6, TIMERD_CLOCKINGMODE_AUXILIARY_CLK, TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK, TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK, TIMERD_CLOCKSOURCE_ACLK, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, TIMERD_CLOCKSOURCE_DIVIDER_8, TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK, TIMERD_CLOCKSOURCE_SMCLK, TIMERD_DO_CLEAR, TIMERD_OUTPUTMODE_OUTBITVALUE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_RESET_SET, TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_SET_RESET, TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_TOGGLE_RESET, TIMERD_OUTPUTMODE_TOGGLE_SET, TIMERD_TDIE_INTERRUPT_ENABLE, TIMERD_UP_MODE, and TIMERD_UPDOWN_MODE.
void TimerD_stop | ( | unsigned int | baseAddress | ) |
Stops the timer
baseAddress | is the base address of the Timer module. |
Modified registers are TDxCTL0
References HWREG.
void TimerD_setCompareValue | ( | unsigned int | baseAddress, |
unsigned int | compareRegister, | ||
unsigned int | compareValue | ||
) |
Sets the value of the capture-compare register
baseAddress | is the base address of the Timer module. |
compareRegister | selects the Capture register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
compareValue | is the count to be compared with in compare mode |
Modified register is TDxCCRn
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
void TimerD_clearTimerInterruptFlag | ( | unsigned int | baseAddress | ) |
Clears the Timer TAIFG interrupt flag
baseAddress | is the base address of the Timer module. |
Modified bits are TAIFG og TDxCTL0 register
References HWREGB.
void TimerD_clearCaptureCompareInterruptFlag | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Clears the capture-compare interrupt flag
baseAddress | is the base address of the Timer module. |
captureCompareRegister | selects the Capture-compare register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
Modified bits are CCIFG of TDxCCTLn register
References ASSERT, HWREG, TIMERD_CAPTURECOMPARE_REGISTER_0, TIMERD_CAPTURECOMPARE_REGISTER_1, TIMERD_CAPTURECOMPARE_REGISTER_2, TIMERD_CAPTURECOMPARE_REGISTER_3, TIMERD_CAPTURECOMPARE_REGISTER_4, TIMERD_CAPTURECOMPARE_REGISTER_5, and TIMERD_CAPTURECOMPARE_REGISTER_6.
unsigned char TimerD_configureHighResGeneratorInFreeRunningMode | ( | unsigned int | baseAddress, |
unsigned char | desiredHighResFrequency | ||
) |
Configures Timer_D in free running mode
baseAddress | is the base address of the Timer module. |
desiredHighResFrequency | selects the desired High Resolution frequency used. Valid values are TIMERD_HIGHRES_64MHZ TIMERD_HIGHRES_128MHZ TIMERD_HIGHRES_200MHZ TIMERD_HIGHRES_256MHZ |
Modified registers are TDxHCTL1, TDxCTL1 and TDxHCTL0 register
References ASSERT, HWREG, STATUS_FAIL, STATUS_SUCCESS, TIMERD_HIGHRES_128MHZ, TIMERD_HIGHRES_200MHZ, TIMERD_HIGHRES_256MHZ, TIMERD_HIGHRES_64MHZ, TLV_getInfo(), and TLV_TIMER_D_CAL.
void TimerD_configureHighResGeneratorInRegulatedMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | clockingMode, | ||
unsigned char | highResClockMultiplyFactor, | ||
unsigned char | highResClockDivider | ||
) |
Configures Timer_D in Regulated mode
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMERD_CLOCKSOURCE_EXTERNAL_TDCLK [Default value] TIMERD_CLOCKSOURCE_ACLK TIMERD_CLOCKSOURCE_SMCLK TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMERD_CLOCKSOURCE_DIVIDER_1 [Default value] TIMERD_CLOCKSOURCE_DIVIDER_2 TIMERD_CLOCKSOURCE_DIVIDER_4 TIMERD_CLOCKSOURCE_DIVIDER_8 TIMERD_CLOCKSOURCE_DIVIDER_3 TIMERD_CLOCKSOURCE_DIVIDER_5 TIMERD_CLOCKSOURCE_DIVIDER_6 TIMERD_CLOCKSOURCE_DIVIDER_7 TIMERD_CLOCKSOURCE_DIVIDER_10 TIMERD_CLOCKSOURCE_DIVIDER_12 TIMERD_CLOCKSOURCE_DIVIDER_14 TIMERD_CLOCKSOURCE_DIVIDER_16 TIMERD_CLOCKSOURCE_DIVIDER_20 TIMERD_CLOCKSOURCE_DIVIDER_24 TIMERD_CLOCKSOURCE_DIVIDER_28 TIMERD_CLOCKSOURCE_DIVIDER_32 TIMERD_CLOCKSOURCE_DIVIDER_40 TIMERD_CLOCKSOURCE_DIVIDER_48 TIMERD_CLOCKSOURCE_DIVIDER_56 TIMERD_CLOCKSOURCE_DIVIDER_64 |
clockingMode | is the selected clock mode register values. Valid values are TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK [Default value] TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK TIMERD_CLOCKINGMODE_AUXILIARY_CLK |
highResClockMultiplyFactor | selects the high resolution multiply factor. TIMERD_HIGHRES_CLK_MULTIPLY_FACTOR_8x TIMERD_HIGHRES_CLK_MULTIPLY_FACTOR_16x |
highResClockDivider | selects the high resolution divider. TIMERD_HIGHRES_CLK_DIVIDER_1 [Default value] TIMERD_HIGHRES_CLK_DIVIDER_2 TIMERD_HIGHRES_CLK_DIVIDER_4 TIMERD_HIGHRES_CLK_DIVIDER_8 |
Modified registers are OFS_TDxCTL0, TDxCTL1 and TDxHCTL0 register
References ASSERT, HWREG, privateTimerDProcessClockSourceDivider(), TIMERD_CLOCKINGMODE_AUXILIARY_CLK, TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK, TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK, TIMERD_CLOCKSOURCE_ACLK, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, TIMERD_CLOCKSOURCE_DIVIDER_8, and TIMERD_CLOCKSOURCE_SMCLK.
void TimerD_combineTDCCRToGeneratePWM | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | clockingMode, | ||
unsigned int | timerPeriod, | ||
unsigned int | combineCCRRegistersCombination, | ||
unsigned int | compareOutputMode, | ||
unsigned int | dutyCycle1, | ||
unsigned int | dutyCycle2 | ||
) |
Combine TDCCRto get PWM
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMERD_CLOCKSOURCE_EXTERNAL_TDCLK [Default value] TIMERD_CLOCKSOURCE_ACLK TIMERD_CLOCKSOURCE_SMCLK TIMERD_CLOCKSOURCE_INVERTED_EXTERNAL_TDCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMERD_CLOCKSOURCE_DIVIDER_1 [Default value] TIMERD_CLOCKSOURCE_DIVIDER_2 TIMERD_CLOCKSOURCE_DIVIDER_4 TIMERD_CLOCKSOURCE_DIVIDER_8 TIMERD_CLOCKSOURCE_DIVIDER_3 TIMERD_CLOCKSOURCE_DIVIDER_5 TIMERD_CLOCKSOURCE_DIVIDER_6 TIMERD_CLOCKSOURCE_DIVIDER_7 TIMERD_CLOCKSOURCE_DIVIDER_10 TIMERD_CLOCKSOURCE_DIVIDER_12 TIMERD_CLOCKSOURCE_DIVIDER_14 TIMERD_CLOCKSOURCE_DIVIDER_16 TIMERD_CLOCKSOURCE_DIVIDER_20 TIMERD_CLOCKSOURCE_DIVIDER_24 TIMERD_CLOCKSOURCE_DIVIDER_28 TIMERD_CLOCKSOURCE_DIVIDER_32 TIMERD_CLOCKSOURCE_DIVIDER_40 TIMERD_CLOCKSOURCE_DIVIDER_48 TIMERD_CLOCKSOURCE_DIVIDER_56 TIMERD_CLOCKSOURCE_DIVIDER_64 |
clockingMode | is the selected clock mode register values. Valid values are TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK [Default value] TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK TIMERD_CLOCKINGMODE_AUXILIARY_CLK ! |
timerPeriod | selects the desired timer period |
combineCCRRegistersCombination | selects desired CCR registers to combine TIMERD_COMBINE_CCR1_CCR2 TIMERD_COMBINE_CCR3_CCR4 (available on Timer_D5, Timer_D7) TIMERD_COMBINE_CCR5_CCR6(available only on Timer_D7) |
compareOutputMode | specifies the ouput mode. Valid values are TIMERD_OUTPUTMODE_OUTBITVALUE, TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_TOGGLE_RESET, TIMERD_OUTPUTMODE_SET_RESET TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_TOGGLE_SET, TIMERD_OUTPUTMODE_RESET_SET |
dutyCycle | specifies the dutycycle for the generated waveform |
Modified registers are TDxCTL0, TDxCTL1, TDxCCR0, TDxCCTL0,TDxCCTLn
References ASSERT, HWREG, privateTimerDProcessClockSourceDivider(), TIMERD_CLOCKINGMODE_AUXILIARY_CLK, TIMERD_CLOCKINGMODE_EXTERNAL_CLOCK, TIMERD_CLOCKINGMODE_HIRES_LOCAL_CLOCK, TIMERD_CLOCKSOURCE_ACLK, TIMERD_CLOCKSOURCE_DIVIDER_1, TIMERD_CLOCKSOURCE_DIVIDER_10, TIMERD_CLOCKSOURCE_DIVIDER_12, TIMERD_CLOCKSOURCE_DIVIDER_14, TIMERD_CLOCKSOURCE_DIVIDER_16, TIMERD_CLOCKSOURCE_DIVIDER_2, TIMERD_CLOCKSOURCE_DIVIDER_20, TIMERD_CLOCKSOURCE_DIVIDER_24, TIMERD_CLOCKSOURCE_DIVIDER_28, TIMERD_CLOCKSOURCE_DIVIDER_3, TIMERD_CLOCKSOURCE_DIVIDER_32, TIMERD_CLOCKSOURCE_DIVIDER_4, TIMERD_CLOCKSOURCE_DIVIDER_40, TIMERD_CLOCKSOURCE_DIVIDER_48, TIMERD_CLOCKSOURCE_DIVIDER_5, TIMERD_CLOCKSOURCE_DIVIDER_56, TIMERD_CLOCKSOURCE_DIVIDER_6, TIMERD_CLOCKSOURCE_DIVIDER_64, TIMERD_CLOCKSOURCE_DIVIDER_7, TIMERD_CLOCKSOURCE_DIVIDER_8, TIMERD_CLOCKSOURCE_SMCLK, TIMERD_COMBINE_CCR1_CCR2, TIMERD_COMBINE_CCR3_CCR4, TIMERD_COMBINE_CCR5_CCR6, TIMERD_OUTPUTMODE_OUTBITVALUE, TIMERD_OUTPUTMODE_RESET, TIMERD_OUTPUTMODE_RESET_SET, TIMERD_OUTPUTMODE_SET, TIMERD_OUTPUTMODE_SET_RESET, TIMERD_OUTPUTMODE_TOGGLE, TIMERD_OUTPUTMODE_TOGGLE_RESET, and TIMERD_OUTPUTMODE_TOGGLE_SET.
void TimerD_selectLatchingGroup | ( | unsigned int | baseAddress, |
unsigned int | groupLatch | ||
) |
Selects TimerD Latching Group
baseAddress | is the base address of the TimerD module. |
groupLatch | selects the value of counter length. Valid values are TIMERD_GROUP_NONE [Default value] TIMERD_GROUP_CL12_CL23_CL56 TIMERD_GROUP_CL123_CL456 TIMERD_GROUP_ALL |
Modified bits are TDCLGRP of TDxCTL0 register
void TimerD_selectCounterLength | ( | unsigned int | baseAddress, |
unsigned int | counterLength | ||
) |
Selects TimerD counter length
baseAddress | is the base address of the TimerD module. |
counterLength | selects the value of counter length. Valid values are TIMERD_COUNTER_16BIT [Default value] TIMERD_COUNTER_12BIT TIMERD_COUNTER_10BIT TIMERD_COUNTER_8BIT |
Modified bits are CNTL of TDxCTL0 register
void TimerD_initCompareLatchLoadEvent | ( | unsigned int | baseAddress, |
unsigned int | compareRegister, | ||
unsigned int | compareLatchLoadEvent | ||
) |
Selects Compare Latch Load Event
baseAddress | is the base address of the TimerD module. |
captureCompareRegister | selects the Capture-compare register being used. Valid values are TIMERD_CAPTURECOMPARE_REGISTER_0 TIMERD_CAPTURECOMPARE_REGISTER_1 TIMERD_CAPTURECOMPARE_REGISTER_2 TIMERD_CAPTURECOMPARE_REGISTER_3 TIMERD_CAPTURECOMPARE_REGISTER_4 TIMERD_CAPTURECOMPARE_REGISTER_5 TIMERD_CAPTURECOMPARE_REGISTER_6 |
compareLatchLoadEvent | selects the latch load event Valid values are TIMERD_LATCH_ON_WRITE_TO_TDxCCRn_COMPARE_REGISTER [Default value] TIMERD_LATCH_WHEN_COUNTER_COUNTS_TO_0_IN_UP_OR_CONT_MODE TIMERD_LATCH_WHEN_COUNTER_COUNTS_TO_0_IN_UPDOWN_MODE TIMERD_LATCH_WHEN_COUNTER_COUNTS_TO_CURRENT_COMPARE_LATCH_VALUE |
Modified bits are CLLD of TDxCCTLn register
void TimerD_disableHighResFastWakeup | ( | unsigned int | baseAddress | ) |
Disable High Resolution fast wakeup
baseAddress | is the base address of the Timer module. |
Modified bits are TDHFW of TDxHCTL0 register.
References HWREG.
void TimerD_enableHighResFastWakeup | ( | unsigned int | baseAddress | ) |
Enable High Resolution fast wakeup
baseAddress | is the base address of the Timer module. |
Modified bits are TDHFW of TDxHCTL0 register.
References HWREG.
void TimerD_disableHighResClockEnhancedAccuracy | ( | unsigned int | baseAddress | ) |
Disable High Resolution Clock Enhanced Accuracy
baseAddress | is the base address of the Timer module. |
Modified bits are TDHEAEN of TDxHCTL0 register.
References HWREG.
void TimerD_enableHighResClockEnhancedAccuracy | ( | unsigned int | baseAddress | ) |
Enable High Resolution Clock Enhanced Accuracy
baseAddress | is the base address of the Timer module. |
Modified bits are TDHEAEN of TDxHCTL0 register.
References HWREG.
void TimerD_DisableHighResGeneratorForceON | ( | unsigned int | baseAddress | ) |
Disable High Resolution Clock Enhanced Accuracy
baseAddress | is the base address of the Timer module. |
Modified bit is TDHRON of register TDxHCTL0
High-resolution generator is on if the Timer_D counter MCx bits are 01, 10 or 11.
References HWREG.
void TimerD_EnableHighResGeneratorForceON | ( | unsigned int | baseAddress | ) |
Enable High Resolution Clock Enhanced Accuracy
baseAddress | is the base address of the Timer module. |
Modified bit is TDHRON of register TDxHCTL0
High-resolution generator is on in all Timer_D MCx modes. The PMM remains in high-current mode.
References HWREG.
void TimerD_selectHighResCoarseClockRange | ( | unsigned int | baseAddress, |
unsigned int | highResCoarseClockRange | ||
) |
Select High Resolution Coarse Clock Range
baseAddress | is the base address of the Timer module. |
highResCoarseClockRange | selects the High Resolution Coarse Clock Range Valid values are TIMERD_HIGHRES_BELOW_15MHz [Default value] TIMERD_HIGHRES_ABOVE_15MHz |
Modified bits are TDHCLKCR of registers TDxHCTL1.
References ASSERT, HWREG, TIMERD_HIGHRES_ABOVE_15MHz, and TIMERD_HIGHRES_BELOW_15MHz.
void TimerD_selectHighResClockRange | ( | unsigned int | baseAddress, |
unsigned int | highResClockRange | ||
) |
Select High Resolution Clock Range Selection
baseAddress | is the base address of the Timer module. |
highResClockRange | selects the High Resolution Clock Range Valid values are TIMERD_CLOCK_RANGE0 [Default value] TIMERD_CLOCK_RANGE1 TIMERD_CLOCK_RANGE2 Refer Datasheet for frequency details |
Modified bits are TDHCLKRx of registers TDxHCTL1 NOTE: In Regulated mode these bits are modified by hardware.
References ASSERT, HWREG, TIMERD_CLOCK_RANGE0, TIMERD_CLOCK_RANGE1, and TIMERD_CLOCK_RANGE2.