MSP DSP Library
|
Parameter structure for the Q15 vector scale function. More...
#include <DSPLib_vector.h>
Data Fields | |
uint16_t | length |
Length of source and destination data, must be a multiple of two. | |
_q15 | scale |
Q15 fractional value scale to multiply each vector element by. | |
uint8_t | shift |
Unsigned integer value to shift each vector result left by. | |
Parameter structure for the Q15 vector scale function.