MSP DSP Library
|
Parameter structure for the matrix subtract function. More...
#include <DSPLib_matrix.h>
Data Fields | |
uint16_t | rows |
Number of rows in the source matrices, must be a multiple of two. | |
uint16_t | cols |
Number of columns in the source matrices, must be a multiple of two. | |
Parameter structure for the matrix subtract function.