MSP DSP Library
|
Parameter structure for the real matrix scale function. More...
#include <DSPLib_matrix.h>
Data Fields | |
uint16_t | rows |
Number of rows in the source matrices, must be a multiple of two. | |
uint16_t | cols |
Number of columns in the source matrices, must be a multiple of two. | |
uint8_t | shift |
Integer amount to shift result matrix by, must be positive. | |
_iq31 | scale |
IQ31 constant multiplied with the source matrix. | |
Parameter structure for the real matrix scale function.