Logo
MSP DSP Library
msp_matrix_neg_iq31_params Struct Reference

Parameter structure for the real matrix negate function. More...

#include <DSPLib_matrix.h>

Data Fields

uint16_t rows
 Number of rows in the source matrices, must be a multiple of two.
 
uint16_t cols
 Number of columns in the source matrices, must be a multiple of two.
 

Detailed Description

Parameter structure for the real matrix negate function.


The documentation for this struct was generated from the following file: