MSP DSP Library
|
Parameter structure for the IQ31 complex vector scale by real function. More...
#include <DSPLib_vector.h>
Data Fields | |
uint16_t | length |
Length of source and destination data, must be a multiple of two. | |
_iq31 | scale |
q31 real fractional scale to multiply each complex vector element by. | |
uint8_t | shift |
Unsigned integer value to shift each complex vector result left by. | |
Parameter structure for the IQ31 complex vector scale by real function.