MSP DSP Library
|
Parameter structure for cascaded direct form 2 biquad filter. More...
#include <DSPLib_filter.h>
Data Fields | |
uint16_t | length |
uint16_t | stages |
const msp_biquad_df2_q15_coeffs * | coeffs |
msp_biquad_df2_q15_states * | states |
Parameter structure for cascaded direct form 2 biquad filter.
const msp_biquad_df2_q15_coeffs* msp_biquad_cascade_df2_q15_params::coeffs |
Pointer to an array of DF2 filter coefficients of length stages. This data block must be allocated in shared RAM when using LEA.
uint16_t msp_biquad_cascade_df2_q15_params::length |
Length of the source data, must be a multiple of two.
uint16_t msp_biquad_cascade_df2_q15_params::stages |
Number of cascaded biquad filters, typically the filter order divided by two.
msp_biquad_df2_q15_states* msp_biquad_cascade_df2_q15_params::states |
Pointer to an array of DF2 filter states of length stages. When continuous operation is desired the previous states must be passed to the next cascaded biquad operation. This data block must be allocated in shared RAM when using LEA.