MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Public Member Functions | Data Fields
BufferInfo Struct Reference

Buffer info structure. More...

#include <uart_comm.h>

Public Member Functions

 _Alignas (uint32_t) uint8_t buffer[MAX_BUFFER_SIZE]
 

Data Fields

uint8_t ptr
 
uint8_t len
 

Detailed Description

Buffer info structure.

Member Function Documentation

§ _Alignas()

BufferInfo::_Alignas ( uint32_t  )

Buffer array

Field Documentation

§ ptr

uint8_t BufferInfo::ptr

Pointer

Referenced by UART_getFrameLength().

§ len

uint8_t BufferInfo::len

Length

Referenced by UART_checkForCommand(), and UART_getFrameLength().


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale