MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
USER_STATUS_INTERFACE_T Struct Reference

User output structure. More...

#include <appUserOutputs.h>

Collaboration diagram for USER_STATUS_INTERFACE_T:
Collaboration graph
[legend]

Data Fields

USER_FAULT_TYPES systemFaultStatus
 
MOTOR_STATE_TYPES_T motorState
 
OUTPUT_DQ_T VdqFilt
 
OUTPUTS_CURRENT_PI_T currentPI
 
OUTPUTS_PI_T piSpeed
 
OUTPUTS_PI_T piPower
 
OUTPUTS_PI_T piId
 
OUTPUTS_PI_T piIq
 
IPD_IDENTIFIED_SECTOR_T ipdIdentifiedSector
 
int32_t estimatedSpeed
 
int32_t dcBusVoltage
 
int32_t torqueLimit
 
uint32_t gateDriverFaultStatus
 Gate driver faults status register for external reporting.
 
uint32_t controllerFaultStatus
 controller fault status register for external reporting
 
APP_VERSION_T appVersion
 

Detailed Description

User output structure.

Field Documentation

§ systemFaultStatus

USER_FAULT_TYPES USER_STATUS_INTERFACE_T::systemFaultStatus

Fault status

§ motorState

MOTOR_STATE_TYPES_T USER_STATUS_INTERFACE_T::motorState

Motor state

§ VdqFilt

OUTPUT_DQ_T USER_STATUS_INTERFACE_T::VdqFilt

Filtered dq voltage

§ currentPI

OUTPUTS_CURRENT_PI_T USER_STATUS_INTERFACE_T::currentPI

PI current outputs

§ piSpeed

OUTPUTS_PI_T USER_STATUS_INTERFACE_T::piSpeed

PI speed

§ piPower

OUTPUTS_PI_T USER_STATUS_INTERFACE_T::piPower

PI Power

§ piId

OUTPUTS_PI_T USER_STATUS_INTERFACE_T::piId

PI ID

§ piIq

OUTPUTS_PI_T USER_STATUS_INTERFACE_T::piIq

PI IQ

§ ipdIdentifiedSector

IPD_IDENTIFIED_SECTOR_T USER_STATUS_INTERFACE_T::ipdIdentifiedSector

IPD identified sector

§ estimatedSpeed

int32_t USER_STATUS_INTERFACE_T::estimatedSpeed

Estimated speed

§ dcBusVoltage

int32_t USER_STATUS_INTERFACE_T::dcBusVoltage

DC bus voltage

§ torqueLimit

int32_t USER_STATUS_INTERFACE_T::torqueLimit

Torque limit(Q axis current limit)

§ appVersion

APP_VERSION_T USER_STATUS_INTERFACE_T::appVersion

Application FW version


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale