MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
USER_CTRL_INTERFACE_T Struct Reference

DEVICE_CONFIG1 register. More...

#include <appInputCtrlInterface.h>

Collaboration diagram for USER_CTRL_INTERFACE_T:
Collaboration graph
[legend]

Data Fields

RAM_SPEED_CTRL_T speedCtrl
 
RAM_ALGO_DEBUG_1_T algoDebugCtrl1
 
RAM_ALGO_DEBUG_2_T algoDebugCtrl2
 
RAM_ALGO_DEBUG_3_T algoDebugCtrl3
 
RAM_DAC_CNTRL_T dacCtrl
 

Detailed Description

DEVICE_CONFIG1 register.

Field Documentation

§ speedCtrl

RAM_SPEED_CTRL_T USER_CTRL_INTERFACE_T::speedCtrl

Speed control

§ algoDebugCtrl1

RAM_ALGO_DEBUG_1_T USER_CTRL_INTERFACE_T::algoDebugCtrl1

Algo debug 1

§ algoDebugCtrl2

RAM_ALGO_DEBUG_2_T USER_CTRL_INTERFACE_T::algoDebugCtrl2

Algo debug 2

§ algoDebugCtrl3

RAM_ALGO_DEBUG_3_T USER_CTRL_INTERFACE_T::algoDebugCtrl3

Algo debug 3

§ dacCtrl

RAM_DAC_CNTRL_T USER_CTRL_INTERFACE_T::dacCtrl

DAC control


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale