MSPM0G3519SensoredFOCMotorControlLibrary  1.0
Data Fields
FAULT_FLAGS_T::faultFlags Struct Reference

faultFlags structure More...

#include <faults.h>

Data Fields

_Bool hardwareOverCurrentRetryEnable: 1
 
_Bool noMotorRetryEnable: 1
 
_Bool abnormalSpeedRetryEnable: 1
 
_Bool lowBemfRetryEnable: 1
 
_Bool clearFault: 1
 
_Bool retryEnable: 1
 
_Bool retryStatus: 1
 
_Bool actionTaken: 1
 

Detailed Description

faultFlags structure

Field Documentation

§ hardwareOverCurrentRetryEnable

_Bool FAULT_FLAGS_T::faultFlags::hardwareOverCurrentRetryEnable

hardwareOverCurrentRetryEnable

Referenced by faultServiceLowPriorityRun().

§ noMotorRetryEnable

_Bool FAULT_FLAGS_T::faultFlags::noMotorRetryEnable

noMotorRetryEnable

Referenced by faultServiceLowPriorityRun(), and user_config_faults().

§ abnormalSpeedRetryEnable

_Bool FAULT_FLAGS_T::faultFlags::abnormalSpeedRetryEnable

abnormalSpeedRetryEnable

Referenced by faultServiceLowPriorityRun(), and user_config_faults().

§ lowBemfRetryEnable

_Bool FAULT_FLAGS_T::faultFlags::lowBemfRetryEnable

lowBemfRetryEnable

Referenced by user_config_faults().

§ clearFault

_Bool FAULT_FLAGS_T::faultFlags::clearFault

§ retryEnable

_Bool FAULT_FLAGS_T::faultFlags::retryEnable

retryEnable

Referenced by faultServiceLowPriorityRun().

§ retryStatus

_Bool FAULT_FLAGS_T::faultFlags::retryStatus

§ actionTaken

_Bool FAULT_FLAGS_T::faultFlags::actionTaken

actionTaken

Referenced by faultServiceInit(), and faultServiceRun().


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale