![]() |
![]() |
|
MSPM0G3519SensoredFOCMotorControlLibrary
1.0
|


Go to the source code of this file.
Data Structures | |
| struct | SOURCE_CURRENT_ESTIMATOR_T |
| Source Current Working Struct. More... | |
Macros | |
| #define | SOURCE_CURRENT_FILT_CONST _IQ(0.1) |
| Source Current Filt Const. | |
Functions | |
| void | sourceCurrentEstimInit (SOURCE_CURRENT_ESTIMATOR_T *pSourceCurrentEstim) |
| source Current Estim Init More... | |
| void | sourceCurrentEstimRun (SOURCE_CURRENT_ESTIMATOR_T *pSourceCurrentEstim) |
| source Current Estim Run More... | |
| void sourceCurrentEstimInit | ( | SOURCE_CURRENT_ESTIMATOR_T * | pSourceCurrentEstim | ) |
source Current Estim Init
| [in] | *pSourceCurrentEstim | Input Pointer |
References SOURCE_CURRENT_ESTIMATOR_T::sourceCurrentFilt.
Referenced by sourceLimitsInit().
| void sourceCurrentEstimRun | ( | SOURCE_CURRENT_ESTIMATOR_T * | pSourceCurrentEstim | ) |
source Current Estim Run
| [in] | *pSourceCurrentEstim | Input Pointer |
References SOURCE_CURRENT_ESTIMATOR_T::pSourceCurrent, SOURCE_CURRENT_FILT_CONST, and SOURCE_CURRENT_ESTIMATOR_T::sourceCurrentFilt.
Referenced by sourceLimitsRun().