87 #ifndef APPLIMITS_INCLUDE_SOURCECURRENTESTIM_H_ 88 #define APPLIMITS_INCLUDE_SOURCECURRENTESTIM_H_ 95 #define SOURCE_CURRENT_FILT_CONST _IQ(0.1) void sourceCurrentEstimRun(SOURCE_CURRENT_ESTIMATOR_T *pSourceCurrentEstim)
source Current Estim Run
Definition: sourceCurrentEstim.c:90
Source Current Working Struct.
Definition: sourceCurrentEstim.h:98
Motor Control Library Module.
int32_t sourceCurrentFilt
Definition: sourceCurrentEstim.h:110
const int32_t * pSourceCurrent
Definition: sourceCurrentEstim.h:104
void sourceCurrentEstimInit(SOURCE_CURRENT_ESTIMATOR_T *pSourceCurrentEstim)
source Current Estim Init
Definition: sourceCurrentEstim.c:85