MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
userInputPeriCfg1 Struct Reference

userInputPeriCfg1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t dirChangeMode: 1
 
uint32_t dirInput: 2
 
uint32_t busCurrLimitEnable: 1
 
uint32_t busCurrLimit: 5
 
uint32_t mcuDeadTime: 6
 
uint32_t reserved: 17
 

Detailed Description

userInputPeriCfg1 structure

Field Documentation

§ dirChangeMode

uint32_t userInputPeriCfg1::dirChangeMode

Response to change of DIR pin status

§ dirInput

uint32_t userInputPeriCfg1::dirInput

DIR pin override

Referenced by update_DirectionStatus().

§ busCurrLimitEnable

uint32_t userInputPeriCfg1::busCurrLimitEnable

Bus current limit enable

§ busCurrLimit

uint32_t userInputPeriCfg1::busCurrLimit

Bus current limit

§ mcuDeadTime

uint32_t userInputPeriCfg1::mcuDeadTime

deadtime for PWM outputs

Referenced by peri1Config().

§ reserved

uint32_t userInputPeriCfg1::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale