MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
ramAlgoDebugCtrl2 Struct Reference

ramAlgoDebugCtrl2 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t reserved: 6
 
uint32_t forceVQCurrLoopDis: 10
 
uint32_t forceVDCurrLoopDis: 10
 
uint32_t currLoopDis: 1
 
uint32_t statusUpdateEn: 1
 
uint32_t updateConfigs: 1
 
uint32_t updateSysParams: 1
 
uint32_t Reserved2: 2
 

Detailed Description

ramAlgoDebugCtrl2 structure

Field Documentation

§ reserved

uint32_t ramAlgoDebugCtrl2::reserved

Reserved

§ forceVQCurrLoopDis

uint32_t ramAlgoDebugCtrl2::forceVQCurrLoopDis

Vq applied when current loop and speed loop are disabled

§ forceVDCurrLoopDis

uint32_t ramAlgoDebugCtrl2::forceVDCurrLoopDis

Vd applied when current loop and speed loop are disabled

§ currLoopDis

uint32_t ramAlgoDebugCtrl2::currLoopDis

Current loop and speed loop are disabled

§ statusUpdateEn

uint32_t ramAlgoDebugCtrl2::statusUpdateEn

statusUpdate Flag

§ updateConfigs

uint32_t ramAlgoDebugCtrl2::updateConfigs

Update configurations Flag

§ updateSysParams

uint32_t ramAlgoDebugCtrl2::updateSysParams

Update System Parameters Dynamically Flag

§ Reserved2

uint32_t ramAlgoDebugCtrl2::Reserved2

Reserved 2


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale