MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
USER_INPUT_MTR_STARTUP1_T Union Reference

START_UP1_CONFIG register. More...

#include <appInputCtrlInterface.h>

Collaboration diagram for USER_INPUT_MTR_STARTUP1_T:
Collaboration graph
[legend]

Data Fields

userInputMotorStartUp1 b
 
uint32_t w
 

Detailed Description

START_UP1_CONFIG register.

Field Documentation

§ b

userInputMotorStartUp1 USER_INPUT_MTR_STARTUP1_T::b

Bitwise access

§ w

uint32_t USER_INPUT_MTR_STARTUP1_T::w

Block access


The documentation for this union was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale