MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
userInputMotorStartUp1 Struct Reference

userInputMotorStartUp1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t iqRampEn: 1
 
uint32_t olILimitCfg: 1
 
uint32_t ipdRepeat: 2
 
uint32_t ipdAdvAngle: 2
 
uint32_t reserved: 1
 
uint32_t ipdCurrThresh: 7
 
uint32_t ipdClkFreq: 3
 
uint32_t alignOrSlowCurrLimit: 5
 
uint32_t alignTime: 4
 
uint32_t alignSlowRampRate: 4
 
uint32_t mtrStartUpOption: 2
 

Detailed Description

userInputMotorStartUp1 structure

Field Documentation

§ iqRampEn

uint32_t userInputMotorStartUp1::iqRampEn

Iq ramp down before transition to close loop

§ olILimitCfg

uint32_t userInputMotorStartUp1::olILimitCfg

Open loop current limit configuration

§ ipdRepeat

uint32_t userInputMotorStartUp1::ipdRepeat

Number of times IPD is repeatedly executed

§ ipdAdvAngle

uint32_t userInputMotorStartUp1::ipdAdvAngle

IPD advance angle

§ reserved

uint32_t userInputMotorStartUp1::reserved

Reserved

§ ipdCurrThresh

uint32_t userInputMotorStartUp1::ipdCurrThresh

IPD current threshold

§ ipdClkFreq

uint32_t userInputMotorStartUp1::ipdClkFreq

IPD clock frequency

§ alignOrSlowCurrLimit

uint32_t userInputMotorStartUp1::alignOrSlowCurrLimit

Align or slow first cycle current limit

§ alignTime

uint32_t userInputMotorStartUp1::alignTime

Align time

§ alignSlowRampRate

uint32_t userInputMotorStartUp1::alignSlowRampRate

Align, slow first cycle and open loop current ramp rate

§ mtrStartUpOption

uint32_t userInputMotorStartUp1::mtrStartUpOption

Motor start-up method


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale