MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Functions
servicesHAL.h File Reference

Detailed Description

Application services HAL Module.


Overview

Handles the HAL for services module


#include "services.h"
Include dependency graph for servicesHAL.h:

Go to the source code of this file.

Functions

void HAL_setDeadTime (uint32_t value)
 Sets deadtime. More...
 
int32_t gateDriverGetMinOTimeSineMod (void)
 Gets minimum on time for sine modulation. More...
 
int32_t gateDriverGetMinOnTimeOverMod (void)
 Gets minimum on time for over modulation. More...
 
int32_t gateDriverGetPropagationDelay (void)
 Gets the gate driver propagation delay. More...
 

Function Documentation

§ HAL_setDeadTime()

void HAL_setDeadTime ( uint32_t  value)

Sets deadtime.

Parameters
[in]valueValue for Deadtime configuration

References FOC_PWMA0_INST, gateDriverGetMinOTimeSineMod(), and gateDriverGetPropagationDelay().

Referenced by peri1Config().

§ gateDriverGetMinOTimeSineMod()

int32_t gateDriverGetMinOTimeSineMod ( void  )

Gets minimum on time for sine modulation.

Returns
Returns the minimum on time in ns

Referenced by HAL_setDeadTime().

§ gateDriverGetMinOnTimeOverMod()

int32_t gateDriverGetMinOnTimeOverMod ( void  )

Gets minimum on time for over modulation.

Returns
Returns the minimum on time in ns

§ gateDriverGetPropagationDelay()

int32_t gateDriverGetPropagationDelay ( void  )

Gets the gate driver propagation delay.

Returns
Returns the gate driver propagation delay

Referenced by HAL_setDeadTime().

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale