MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
userInputCloseLoop1 Struct Reference

userInputCloseLoop1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t reserved1: 1
 
uint32_t deadTimeCompEn: 1
 
uint32_t avsEn: 1
 
uint32_t pwmMode: 1
 
uint32_t pwmFreqOut: 4
 
uint32_t clDec: 5
 
uint32_t clDecCfg: 1
 
uint32_t clAcc: 5
 
uint32_t overModEnable: 1
 
uint32_t mtrStopOption: 2
 
uint32_t iLimit: 5
 
uint32_t highFreqFOCEn: 1
 
uint32_t controlMode: 2
 
uint32_t reserved: 2
 

Detailed Description

userInputCloseLoop1 structure

Field Documentation

§ reserved1

uint32_t userInputCloseLoop1::reserved1

Reserved

§ deadTimeCompEn

uint32_t userInputCloseLoop1::deadTimeCompEn

Deadtime compensation enable

§ avsEn

uint32_t userInputCloseLoop1::avsEn

AVS enable

§ pwmMode

uint32_t userInputCloseLoop1::pwmMode

PWM modulation

§ pwmFreqOut

uint32_t userInputCloseLoop1::pwmFreqOut

Output PWM switching frequency

§ clDec

uint32_t userInputCloseLoop1::clDec

Closed loop deceleration. This register is used only if AVS is disabled and CL_DEC_CONFIG is set to '0'

Referenced by update_CloseLoop1Config().

§ clDecCfg

uint32_t userInputCloseLoop1::clDecCfg

Closed loop deceleration configuration

Referenced by update_CloseLoop1Config().

§ clAcc

uint32_t userInputCloseLoop1::clAcc

Closed loop acceleration

Referenced by update_CloseLoop1Config().

§ overModEnable

uint32_t userInputCloseLoop1::overModEnable

Overmodulation enable

§ mtrStopOption

uint32_t userInputCloseLoop1::mtrStopOption

Motor stop options

§ iLimit

uint32_t userInputCloseLoop1::iLimit

Maximum current reference in torque PI loop

§ highFreqFOCEn

uint32_t userInputCloseLoop1::highFreqFOCEn

Reduces the ADC sampling rate to half value, so that PWM freq can be high

§ controlMode

uint32_t userInputCloseLoop1::controlMode

Control mode

§ reserved

uint32_t userInputCloseLoop1::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale