IQMathLibrary  1.0
Functions
_IQNexp.c File Reference

Detailed Description

Functions to compute the exponential of the input and return the result.



#include <stdint.h>
#include "../support/support.h"
#include "_IQNtables.h"
Include dependency graph for _IQNexp.c:

Functions

__STATIC_INLINE int_fast32_t __IQNexp (int_fast32_t iqNInput, const uint_fast32_t *iqNLookupTable, uint8_t ui8IntegerOffset, const int_fast32_t iqN_MIN, const int_fast32_t iqN_MAX, const int8_t q_value)
 Computes the exponential of an IQN input. More...
 
int32_t _IQ30exp (int32_t a)
 Computes the exponential of an IQ30 input. More...
 
int32_t _IQ29exp (int32_t a)
 Computes the exponential of an IQ29 input. More...
 
int32_t _IQ28exp (int32_t a)
 Computes the exponential of an IQ28 input. More...
 
int32_t _IQ27exp (int32_t a)
 Computes the exponential of an IQ27 input. More...
 
int32_t _IQ26exp (int32_t a)
 Computes the exponential of an IQ26 input. More...
 
int32_t _IQ25exp (int32_t a)
 Computes the exponential of an IQ25 input. More...
 
int32_t _IQ24exp (int32_t a)
 Computes the exponential of an IQ24 input. More...
 
int32_t _IQ23exp (int32_t a)
 Computes the exponential of an IQ23 input. More...
 
int32_t _IQ22exp (int32_t a)
 Computes the exponential of an IQ22 input. More...
 
int32_t _IQ21exp (int32_t a)
 Computes the exponential of an IQ21 input. More...
 
int32_t _IQ20exp (int32_t a)
 Computes the exponential of an IQ20 input. More...
 
int32_t _IQ19exp (int32_t a)
 Computes the exponential of an IQ19 input. More...
 
int32_t _IQ18exp (int32_t a)
 Computes the exponential of an IQ18 input. More...
 
int32_t _IQ17exp (int32_t a)
 Computes the exponential of an IQ17 input. More...
 
int32_t _IQ16exp (int32_t a)
 Computes the exponential of an IQ16 input. More...
 
int32_t _IQ15exp (int32_t a)
 Computes the exponential of an IQ15 input. More...
 
int32_t _IQ14exp (int32_t a)
 Computes the exponential of an IQ14 input. More...
 
int32_t _IQ13exp (int32_t a)
 Computes the exponential of an IQ13 input. More...
 
int32_t _IQ12exp (int32_t a)
 Computes the exponential of an IQ12 input. More...
 
int32_t _IQ11exp (int32_t a)
 Computes the exponential of an IQ11 input. More...
 
int32_t _IQ10exp (int32_t a)
 Computes the exponential of an IQ10 input. More...
 
int32_t _IQ9exp (int32_t a)
 Computes the exponential of an IQ9 input. More...
 
int32_t _IQ8exp (int32_t a)
 Computes the exponential of an IQ8 input. More...
 
int32_t _IQ7exp (int32_t a)
 Computes the exponential of an IQ7 input. More...
 
int32_t _IQ6exp (int32_t a)
 Computes the exponential of an IQ6 input. More...
 
int32_t _IQ5exp (int32_t a)
 Computes the exponential of an IQ5 input. More...
 
int32_t _IQ4exp (int32_t a)
 Computes the exponential of an IQ4 input. More...
 
int32_t _IQ3exp (int32_t a)
 Computes the exponential of an IQ3 input. More...
 
int32_t _IQ2exp (int32_t a)
 Computes the exponential of an IQ2 input. More...
 
int32_t _IQ1exp (int32_t a)
 Computes the exponential of an IQ1 input. More...
 

Function Documentation

§ __IQNexp()

__STATIC_INLINE int_fast32_t __IQNexp ( int_fast32_t  iqNInput,
const uint_fast32_t *  iqNLookupTable,
uint8_t  ui8IntegerOffset,
const int_fast32_t  iqN_MIN,
const int_fast32_t  iqN_MAX,
const int8_t  q_value 
)

Computes the exponential of an IQN input.

Parameters
iqNInputIQN type input.
iqNLookupTableInteger result lookup table.
ui8IntegerOffsetInteger portion offset
iqN_MINMinimum parameter value.
iqN_MAXMaximum parameter value.
q_valueIQ format.
Returns
IQN type result of exponential.

Referenced by _IQ10exp(), _IQ11exp(), _IQ12exp(), _IQ13exp(), _IQ14exp(), _IQ15exp(), _IQ16exp(), _IQ17exp(), _IQ18exp(), _IQ19exp(), _IQ1exp(), _IQ20exp(), _IQ21exp(), _IQ22exp(), _IQ23exp(), _IQ24exp(), _IQ25exp(), _IQ26exp(), _IQ27exp(), _IQ28exp(), _IQ29exp(), _IQ2exp(), _IQ30exp(), _IQ3exp(), _IQ4exp(), _IQ5exp(), _IQ6exp(), _IQ7exp(), _IQ8exp(), and _IQ9exp().

§ _IQ30exp()

int32_t _IQ30exp ( int32_t  a)

Computes the exponential of an IQ30 input.

Parameters
aIQ30 type input.
Returns
IQ30 type result of exponential.

References __IQNexp().

§ _IQ29exp()

int32_t _IQ29exp ( int32_t  a)

Computes the exponential of an IQ29 input.

Parameters
aIQ29 type input.
Returns
IQ29 type result of exponential.

References __IQNexp().

§ _IQ28exp()

int32_t _IQ28exp ( int32_t  a)

Computes the exponential of an IQ28 input.

Parameters
aIQ28 type input.
Returns
IQ28 type result of exponential.

References __IQNexp().

§ _IQ27exp()

int32_t _IQ27exp ( int32_t  a)

Computes the exponential of an IQ27 input.

Parameters
aIQ27 type input.
Returns
IQ27 type result of exponential.

References __IQNexp().

§ _IQ26exp()

int32_t _IQ26exp ( int32_t  a)

Computes the exponential of an IQ26 input.

Parameters
aIQ26 type input.
Returns
IQ26 type result of exponential.

References __IQNexp().

§ _IQ25exp()

int32_t _IQ25exp ( int32_t  a)

Computes the exponential of an IQ25 input.

Parameters
aIQ25 type input.
Returns
IQ25 type result of exponential.

References __IQNexp().

§ _IQ24exp()

int32_t _IQ24exp ( int32_t  a)

Computes the exponential of an IQ24 input.

Parameters
aIQ24 type input.
Returns
IQ24 type result of exponential.

References __IQNexp().

§ _IQ23exp()

int32_t _IQ23exp ( int32_t  a)

Computes the exponential of an IQ23 input.

Parameters
aIQ23 type input.
Returns
IQ23 type result of exponential.

References __IQNexp().

§ _IQ22exp()

int32_t _IQ22exp ( int32_t  a)

Computes the exponential of an IQ22 input.

Parameters
aIQ22 type input.
Returns
IQ22 type result of exponential.

References __IQNexp().

§ _IQ21exp()

int32_t _IQ21exp ( int32_t  a)

Computes the exponential of an IQ21 input.

Parameters
aIQ21 type input.
Returns
IQ21 type result of exponential.

References __IQNexp().

§ _IQ20exp()

int32_t _IQ20exp ( int32_t  a)

Computes the exponential of an IQ20 input.

Parameters
aIQ20 type input.
Returns
IQ20 type result of exponential.

References __IQNexp().

§ _IQ19exp()

int32_t _IQ19exp ( int32_t  a)

Computes the exponential of an IQ19 input.

Parameters
aIQ19 type input.
Returns
IQ19 type result of exponential.

References __IQNexp().

§ _IQ18exp()

int32_t _IQ18exp ( int32_t  a)

Computes the exponential of an IQ18 input.

Parameters
aIQ18 type input.
Returns
IQ18 type result of exponential.

References __IQNexp().

§ _IQ17exp()

int32_t _IQ17exp ( int32_t  a)

Computes the exponential of an IQ17 input.

Parameters
aIQ17 type input.
Returns
IQ17 type result of exponential.

References __IQNexp().

§ _IQ16exp()

int32_t _IQ16exp ( int32_t  a)

Computes the exponential of an IQ16 input.

Parameters
aIQ16 type input.
Returns
IQ16 type result of exponential.

References __IQNexp().

§ _IQ15exp()

int32_t _IQ15exp ( int32_t  a)

Computes the exponential of an IQ15 input.

Parameters
aIQ15 type input.
Returns
IQ15 type result of exponential.

References __IQNexp().

§ _IQ14exp()

int32_t _IQ14exp ( int32_t  a)

Computes the exponential of an IQ14 input.

Parameters
aIQ14 type input.
Returns
IQ14 type result of exponential.

References __IQNexp().

§ _IQ13exp()

int32_t _IQ13exp ( int32_t  a)

Computes the exponential of an IQ13 input.

Parameters
aIQ13 type input.
Returns
IQ13 type result of exponential.

References __IQNexp().

§ _IQ12exp()

int32_t _IQ12exp ( int32_t  a)

Computes the exponential of an IQ12 input.

Parameters
aIQ12 type input.
Returns
IQ12 type result of exponential.

References __IQNexp().

§ _IQ11exp()

int32_t _IQ11exp ( int32_t  a)

Computes the exponential of an IQ11 input.

Parameters
aIQ11 type input.
Returns
IQ11 type result of exponential.

References __IQNexp().

§ _IQ10exp()

int32_t _IQ10exp ( int32_t  a)

Computes the exponential of an IQ10 input.

Parameters
aIQ10 type input.
Returns
IQ10 type result of exponential.

References __IQNexp().

§ _IQ9exp()

int32_t _IQ9exp ( int32_t  a)

Computes the exponential of an IQ9 input.

Parameters
aIQ9 type input.
Returns
IQ9 type result of exponential.

References __IQNexp().

§ _IQ8exp()

int32_t _IQ8exp ( int32_t  a)

Computes the exponential of an IQ8 input.

Parameters
aIQ8 type input.
Returns
IQ8 type result of exponential.

References __IQNexp().

§ _IQ7exp()

int32_t _IQ7exp ( int32_t  a)

Computes the exponential of an IQ7 input.

Parameters
aIQ7 type input.
Returns
IQ7 type result of exponential.

References __IQNexp().

§ _IQ6exp()

int32_t _IQ6exp ( int32_t  a)

Computes the exponential of an IQ6 input.

Parameters
aIQ6 type input.
Returns
IQ6 type result of exponential.

References __IQNexp().

§ _IQ5exp()

int32_t _IQ5exp ( int32_t  a)

Computes the exponential of an IQ5 input.

Parameters
aIQ5 type input.
Returns
IQ5 type result of exponential.

References __IQNexp().

§ _IQ4exp()

int32_t _IQ4exp ( int32_t  a)

Computes the exponential of an IQ4 input.

Parameters
aIQ4 type input.
Returns
IQ4 type result of exponential.

References __IQNexp().

§ _IQ3exp()

int32_t _IQ3exp ( int32_t  a)

Computes the exponential of an IQ3 input.

Parameters
aIQ3 type input.
Returns
IQ3 type result of exponential.

References __IQNexp().

§ _IQ2exp()

int32_t _IQ2exp ( int32_t  a)

Computes the exponential of an IQ2 input.

Parameters
aIQ2 type input.
Returns
IQ2 type result of exponential.

References __IQNexp().

§ _IQ1exp()

int32_t _IQ1exp ( int32_t  a)

Computes the exponential of an IQ1 input.

Parameters
aIQ1 type input.
Returns
IQ1 type result of exponential.

References __IQNexp().

© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale