![]() |
MCUSW
|
This file contains the interface of the Virtual Mac Ethernet driver.
Go to the source code of this file.
Functions | |
| Std_ReturnType | Eth_VirtMacRpcInit (const Eth_ConfigType *CfgPtr) |
| This function initializes Eth Virtual MAC driver's Remote Procedure Call. | |
| Std_ReturnType | Eth_DispatchVirtmacInit (uint8 CtrlIdx) |
| Dispatch virtual mac initialization request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDeinit (uint8 CtrlIdx) |
| Dispatch virtual mac deinit request to ethernet firmware. | |
| Std_ReturnType | Eth_NotifyVirtmacMsgReceived (uint8 CtrlIdx) |
| Notify Ethernet driver that a RPC msg has been received from ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacSubscribeAllTraffic (uint8 CtrlIdx) |
| Dispatch virtual mac all traffic subscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacUnsubscribeAllTraffic (uint8 CtrlIdx) |
| Dispatch virtual mac all traffic unsubscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacSubscribeDstMac (uint8 CtrlIdx, uint8 *macAddress) |
| Dispatch virtual mac destination mac traffic subscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacUnsubscribeDstMac (uint8 CtrlIdx, uint8 *macAddress) |
| Dispatch virtual mac destination traffic unsubscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacAssociateIPv4Macaddr (uint8 CtrlIdx, uint8 *ipv4Address, uint8 *macAddress) |
| Dispatch virtual mac IPV4 address:destination mac association request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDisassociateIPv4Macaddr (uint8 CtrlIdx, uint8 *ipv4Address) |
| Dispatch virtual mac IPV4 address:destination mac disassociation request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacAddMcastAddr (uint8 CtrlIdx, uint8 *macAddress, uint32 vlanId) |
| Dispatch virtual mac addition of given multicast address to switch address resolution table request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDelAddr (uint8 CtrlIdx, uint8 *macAddress, uint32 vlanId) |
| Dispatch virtual mac removal of given mac address from switch address resolution table request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacAddVlan (uint8 CtrlIdx, uint32 vlanId) |
| Dispatch virtual VLAN join request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDelVlan (uint8 CtrlIdx, uint32 vlanId) |
| Dispatch virtual VLAN leave command to ethernet firmware. | |
| void | Eth_VirtMac_MainFunction (uint8 ctrlIdx) |