![]() |
MCUSW
|
The Virtual Mac Ethernet Driver provides low-level access to the five-port or night-port Gigabit Ethernet Switch hardware in the Jacinto 7 family which integrate Ethernet Firmware functionality.
The Ethernet Driver is part of the Communication Stack in the AUTOSAR Basic Software (BSW).
Functions | |
| Std_ReturnType | Eth_VirtMacRpcInit (const Eth_ConfigType *CfgPtr) |
| This function initializes Eth Virtual MAC driver's Remote Procedure Call. | |
| Std_ReturnType | Eth_DispatchVirtmacInit (uint8 CtrlIdx) |
| Dispatch virtual mac initialization request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDeinit (uint8 CtrlIdx) |
| Dispatch virtual mac deinit request to ethernet firmware. | |
| Std_ReturnType | Eth_NotifyVirtmacMsgReceived (uint8 CtrlIdx) |
| Notify Ethernet driver that a RPC msg has been received from ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacSubscribeAllTraffic (uint8 CtrlIdx) |
| Dispatch virtual mac all traffic subscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacUnsubscribeAllTraffic (uint8 CtrlIdx) |
| Dispatch virtual mac all traffic unsubscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacSubscribeDstMac (uint8 CtrlIdx, uint8 *macAddress) |
| Dispatch virtual mac destination mac traffic subscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacUnsubscribeDstMac (uint8 CtrlIdx, uint8 *macAddress) |
| Dispatch virtual mac destination traffic unsubscription request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacAssociateIPv4Macaddr (uint8 CtrlIdx, uint8 *ipv4Address, uint8 *macAddress) |
| Dispatch virtual mac IPV4 address:destination mac association request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDisassociateIPv4Macaddr (uint8 CtrlIdx, uint8 *ipv4Address) |
| Dispatch virtual mac IPV4 address:destination mac disassociation request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacAddMcastAddr (uint8 CtrlIdx, uint8 *macAddress, uint32 vlanId) |
| Dispatch virtual mac addition of given multicast address to switch address resolution table request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDelAddr (uint8 CtrlIdx, uint8 *macAddress, uint32 vlanId) |
| Dispatch virtual mac removal of given mac address from switch address resolution table request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacAddVlan (uint8 CtrlIdx, uint32 vlanId) |
| Dispatch virtual VLAN join request to ethernet firmware. | |
| Std_ReturnType | Eth_DispatchVirtmacDelVlan (uint8 CtrlIdx, uint32 vlanId) |
| Dispatch virtual VLAN leave command to ethernet firmware. | |
| void | Eth_VirtMac_MainFunction (uint8 ctrlIdx) |
| Std_ReturnType Eth_VirtMacRpcInit | ( | const Eth_ConfigType * | CfgPtr | ) |
This function initializes Eth Virtual MAC driver's Remote Procedure Call.
* Service name : Eth_VirtMacRpcInit * Syntax : Std_ReturnType Eth_VirtMacRpcInit(Eth_ConfigType *CfgPtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x2BU * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CfgPtr. Pointer to virt mac config struct. Refer to /ref Eth_ConfigType * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function initializes the RPC configuration required to invoke remote procedure * calls to ethernet firmware to enable data path setup to AUTOSAR Eth MCAL * driver. On initialization of AUTOSAR MCAL driver in virtual mac mode, the driver * announces autosar ethernet mcal driver RpMsg service to the ethernet * firmware core. The ethernet firmware server service will block waiting for * the announcment from MCAL driver and then attach to the Ethernet MCAL driver * by sending it a EthFwInfo msg * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacInit | ( | uint8 | CtrlIdx | ) |
Dispatch virtual mac initialization request to ethernet firmware.
* Service name : Eth_DispatchVirtmacInit * Syntax : Std_ReturnType Eth_DispatchVirtmacInit(CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x1CU * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx. Index of the controller within the context of the * Ethernet Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: RPC init failed * * Description : The function dispatches RPC command to ethernet * firmware core to allocate data path resources. * The allocated Tx, Rx DMA channels are then setup in the * Eth_Init() API. The function only send the * RPC msg to ethernet firmware core. Completion of RPC msg * processing is indicated by invokcation of * rpcCmdComplete part of Eth_ConfigType sturcture. * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacDeinit | ( | uint8 | CtrlIdx | ) |
Dispatch virtual mac deinit request to ethernet firmware.
* Service name : Eth_DispatchVirtmacDeinit * Syntax : Std_ReturnType Eth_DispatchVirtmacDeinit(CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x1DU * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx. Index of the controller within the context of the * Ethernet Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: virtual mac init failed * * Description : The function dispatches RPC command to ethernet * firmware core to free data path resources. * This function dispatches RPC msg to ethernet firmware core. * Completion of RPC msg processing is indicated by invokcation * of rpcCmdComplete part of Eth_ConfigType sturcture. * Once complete the data path to Ethernet virtual MAC * has been torn down and driver can no loner send or receive packets *
| Std_ReturnType Eth_NotifyVirtmacMsgReceived | ( | uint8 | CtrlIdx | ) |
Notify Ethernet driver that a RPC msg has been received from ethernet firmware.
* Service name : Eth_NotifyVirtmacMsgReceived * Syntax : Std_ReturnType Eth_NotifyVirtmacMsgReceived(CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x1EU * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx. Index of the controller within the context of the * Ethernet Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : Invocation of this function will cause the Ethernet * MCAL driver to process any queued messages received * from ethernet firmware. Depending on type of msg received * ethernet firmware will invoke rpcCmdComplete/fwRegisteredCb * application callbacks. This function is typically * called from the Cdd_IpcNewMessageNotify if the channel * id matches the Ethernet MCAL IPC channel id * (ethfwRpcComChId member of Eth_ConfigType structure) * Application can also trigger recv msg processing by * setting pollRecvMsgInEthMain in Eth_ConfigType to TRUE * Invoking Eth_MainFunction with this config set will * trigger recv msg processing. In triggering recv msg * processing from Eth_MainFunction, this API should be * disabled * *
| Std_ReturnType Eth_DispatchVirtmacSubscribeAllTraffic | ( | uint8 | CtrlIdx | ) |
Dispatch virtual mac all traffic subscription request to ethernet firmware.
* Service name : Eth_DispatchVirtmacSubscribeAllTraffic * Syntax : Std_ReturnType Eth_DispatchVirtmacSubscribeAllTraffic(CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x1FU * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx. Index of the controller within the context of the * Ethernet Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to subscribe to all default flow traffic * received on host port.The default flow contains all * traffic that is not explicitly categorized into a specific * flow using a classifier entry in the switch . * Note that only one core can subscribe to default flow * traffic in a system and this is by default the ethernet * firmware core. This API requires a compatible ethernet * firmware that _does_ _not_ subscribe to default flow * and allows Eth Driver to subscribe to default flow * The function only send the RPC msg to ethernet firmware core. * Completion of RPC msg processing is indicated by invokcation of * rpcCmdComplete part of Eth_ConfigType sturcture. * A failure status indicates ethernet firmware does not allow * AUTOSAR Eth Driver to subscribe to default flow * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeAllTraffic() * 7. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacUnsubscribeAllTraffic | ( | uint8 | CtrlIdx | ) |
Dispatch virtual mac all traffic unsubscription request to ethernet firmware.
* Service name : Eth_DispatchVirtmacUnsubscribeAllTraffic * Syntax : Std_ReturnType Eth_DispatchVirtmacUnsubscribeAllTraffic(CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x20U * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx. Index of the controller within the context of the * Ethernet Driver * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to unsubscribe to all default flow traffic * received on host port.The driver should have subscribed * to all default flow traffic previously by invoking * Eth_DispatchVirtmacSubscribeAllTraffic(). * On unsubscribing to default flow all traffic with * default flow will be dropped. * The function only send the RPC msg to ethernet firmware core. * Completion of RPC msg processing is indicated by invokcation of * rpcCmdComplete part of Eth_ConfigType sturcture. * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeAllTraffic() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_SetControllerMode(ETH_MODE_ACTIVE) * 9. Packet processing using Eth_Receive/Eth_Trasmit * 10. Eth_DispatchVirtmacUnsubscribeAllTraffic * 11. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure * *
| Std_ReturnType Eth_DispatchVirtmacSubscribeDstMac | ( | uint8 | CtrlIdx, |
| uint8 * | macAddress ) |
Dispatch virtual mac destination mac traffic subscription request to ethernet firmware.
* Service name : Eth_DispatchVirtmacSubscribeDstMac * Syntax : Std_ReturnType Eth_DispatchVirtmacSubscribeDstMac(CtrlIdx, macAddress) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x21 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * macAddress: Destination Mac address * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to subscribe to traffic with the given * destination macAddress to be routed to the rx flow * of the Ethernet MCAL driver so that driver can receive * the packets.The macAddres can be a unicast address * allocated to the EthDriver (returned by Eth_GetPhysAddr()) * or a multicast address. * The switch address resolution table should have an entry to * route the destination mac address to the host port. * For unicast address , the switch address resolution table * can be updated using Eth_DispatchVirtmacSubscribeDstMac() * For multicast address , the switch address resolution table * can be updated using Eth_DispatchVirtmacSubscribeDstMac() * Note that broadcast address is usually subscribed to by * ethernet firmware so that it can respond to ARP requests. * If ARP response handling by ethernet firmware is required, * Eth driver should not be subscribed to broadcast address. * The function only send the RPC msg to ethernet firmware core. * Completion of RPC msg processing is indicated by invokcation of * rpcCmdComplete part of Eth_ConfigType sturcture. * A failure status indicates ethernet firmware does not allow * AUTOSAR Eth Driver to subscribe to default flow * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacUnsubscribeDstMac | ( | uint8 | CtrlIdx, |
| uint8 * | macAddress ) |
Dispatch virtual mac destination traffic unsubscription request to ethernet firmware.
* Service name : Eth_DispatchVirtmacUnsubscribeDstMac * Syntax : Std_ReturnType Eth_DispatchVirtmacUnsubscribeDstMac(CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x22 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx. Index of the controller within the context of the * Ethernet Driver * macAddress: Destination Mac address * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to unsubscribe the specified destination * mac address flow traffic received on host port. * The driver should have subscribed to the destination mac * address previously by invoking * Eth_DispatchVirtmacSubscribeDstMac(). * On unsubscribing to destination mac flow , traffic with * given destination mac address flow will be directed to * default flow. * The function only send the RPC msg to ethernet firmware core. * Completion of RPC msg processing is indicated by invokcation of * rpcCmdComplete part of Eth_ConfigType sturcture. * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_SetControllerMode(ETH_MODE_ACTIVE) * 9. Packet processing using Eth_Receive/Eth_Trasmit * 10. Eth_DispatchVirtmacUnsubscribeDstMac() * 11. Wait for rpcCmdComplete() callback with status E_OK * 12. Eth_SetControllerMode(ETH_MODE_DOWN) * Note that all subscribed MAC address must be unsubscribed * before Eth_SetControllerMode(ETH_MODE_DOWN) is invoked * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacAssociateIPv4Macaddr | ( | uint8 | CtrlIdx, |
| uint8 * | ipv4Address, | ||
| uint8 * | macAddress ) |
Dispatch virtual mac IPV4 address:destination mac association request to ethernet firmware.
* Service name : Eth_DispatchVirtmacAssociateIPv4Macaddr * Syntax : Std_ReturnType Eth_DispatchVirtmacAssociateIPv4Macaddr(CtrlIdx, ipv4Address, macAddress) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x23 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * ipv4Address: IPv4 address * macAddress: Destination Mac address * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to associate the given unicast macaddress * with the given IP address. * The ethernet firmware maintains the ARP database for * the ethernet driver and ethfw will respond to any ARP request. * To correctly respond to ARP queries for IP address assigned to * the AUTOSAR network stack , the AUTOSAR stack must invoke * this API so that the ARP database maintained by ethernet * firmware is updated.The macAddres must be a unicast address * allocated to the EthDriver (returned by Eth_GetPhysAddr()) * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_SetControllerMode(ETH_MODE_ACTIVE) * 9. Send out DHCP request to acquire IP address for the * AUTOSAR network stack * 10. On getting DHCP response with IP address, invoke * Eth_DispatchVirtmacAssociateIPv4Macaddr * 11. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacDisassociateIPv4Macaddr | ( | uint8 | CtrlIdx, |
| uint8 * | ipv4Address ) |
Dispatch virtual mac IPV4 address:destination mac disassociation request to ethernet firmware.
* Service name : Eth_DispatchVirtmacDisassociateIPv4Macaddr * Syntax : Std_ReturnType Eth_DispatchVirtmacDisassociateIPv4Macaddr(CtrlIdx, ipv4Address) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x24 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * ipv4Address: IPv4 address * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to remove the given IP address from the * ARP database maintained by ethernet firmware. * On deletion the ethfw will no longer respond to any ARP * queries for the given IP address. * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_SetControllerMode(ETH_MODE_ACTIVE) * 9. Send out DHCP request to acquire IP address for the * AUTOSAR network stack * 10. On getting DHCP response with IP address, invoke * Eth_DispatchVirtmacAssociateIPv4Macaddr * 11. Wait for rpcCmdComplete() callback with status E_OK * 12. Network Packet processing * 13. Eth_DispatchVirtmacDisassociateIPv4Macaddr * 14. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacAddMcastAddr | ( | uint8 | CtrlIdx, |
| uint8 * | macAddress, | ||
| uint32 | vlanId ) |
Dispatch virtual mac addition of given multicast address to switch address resolution table request to ethernet firmware.
* Service name : Eth_DispatchVirtmacAddMcastAddr * Syntax : Std_ReturnType Eth_DispatchVirtmacAddMcastAddr(CtrlIdx, macAddress, numLsbToIgnore, vlanId, portList) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x26 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * macAddress: _Exclusive_ multicast address, or _shared_ multicast address * in devices with ALE multihost support * vlanId: Vlan Id associated with the mac Address. If vlan id is not needed, 0 should be passed * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to add the given multicast macaddress * to the switch address resolution table with the given * vlan id. * Note that this API requires that either the address is an * _exclusive_ multicast address not claimed by any other * remote client, or if the address is a _shared_ multicast * address that the device supports ALE multihost feature * (ETHFW with VEPA support). _Shared_ multicast address * support in devices withotu ALE multihost feature are * currently not supported as this requires shared memory * packet transfer, which is not supported in MCAL. * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_DispatchVirtmacAddMcastAddr() * 9. Wait for rpcCmdComplete() callback with status E_OK * 10. Eth_SetControllerMode(ETH_MODE_ACTIVE) * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacDelAddr | ( | uint8 | CtrlIdx, |
| uint8 * | macAddress, | ||
| uint32 | vlanId ) |
Dispatch virtual mac removal of given mac address from switch address resolution table request to ethernet firmware.
* Service name : Eth_DispatchVirtmacDelAddr * Syntax : Std_ReturnType Eth_DispatchVirtmacDelAddr(uint8 CtrlIdx, uint8 *macAddress, uint32 vlanId) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x27 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * macAddress: Multicast Mac address to be removed from filter * vlanId: Vlan Id associated with the mac Address. If vlan id is not needed, 0 should be passed * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to remove the given multicast macaddress * and vlan id from the switch address resolution table * On removal of entry switch would switch frames * received with the given destination macAddress: * vlan id combo by flooding to all the ports in vlan membership. * Address should have been added previously using * Eth_DispatchVirtmacAddMcastAddr(). * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_DispatchVirtmacAddMcastAddr() * 9. Wait for rpcCmdComplete() callback with status E_OK * 10. Eth_DispatchVirtmacDelAddr() * 11. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacAddVlan | ( | uint8 | CtrlIdx, |
| uint32 | vlanId ) |
Dispatch virtual VLAN join request to ethernet firmware.
* Service name : Eth_DispatchVirtmacAddVlan * Syntax : Std_ReturnType Eth_DispatchVirtmacAddVlan(CtrlIdx, vlanId) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x28 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * vlanId: Vlan Id for which port membership is to be added to switch VLAN membership table * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to join a VLAN. The VLAN creation is * owned by ethernet firmware which defines what * Ethernet ports and virtual ports are members. If * the virtual client is not a member of the VLAN, then * the request to join the VLAN will be rejected. * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_DispatchVirtmacAddVlan() * 9. Wait for rpcCmdComplete() callback with status E_OK * 10. Eth_SetControllerMode(ETH_MODE_ACTIVE) * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| Std_ReturnType Eth_DispatchVirtmacDelVlan | ( | uint8 | CtrlIdx, |
| uint32 | vlanId ) |
Dispatch virtual VLAN leave command to ethernet firmware.
* Service name : Eth_DispatchVirtmacDelVlan * Syntax : Std_ReturnType Eth_DispatchVirtmacDelVlan(uint8 CtrlIdx, uint32 vlanId) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x29 * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Driver * vlanId: Vlan Id which is to be removed from switch VLAN membership table * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: success * E_NOT_OK: otherwise * * Description : The function dispatches RPC command to ethernet * firmware core to leave a VLAN previously joined * through Eth_DispatchVirtmacAddVlan(). * If configured in virtual mac mode application should * invoke this API as follows: * 1. Eth_VirtMacRpcInit() * 2. Wait for fwRegisteredCb() callback * 3. Eth_DispatchVirtmacInit * 4. Wait for rpcCmdComplete() callback with status E_OK * 5. Eth_Init() * 6. Eth_DispatchVirtmacSubscribeDstMac() * 7. Wait for rpcCmdComplete() callback with status E_OK * 8. Eth_DispatchVirtmacAddVlan() * 9. Wait for rpcCmdComplete() callback with status E_OK * 10. Eth_DispatchVirtmacDelVlan() * 11. Wait for rpcCmdComplete() callback with status E_OK * The callbacks fwRegisteredCb() and rpcCmdComplete() are * populated by the application as part of the Eth_ConfigType * structure *
| void Eth_VirtMac_MainFunction | ( | uint8 | ctrlIdx | ) |
The function checks for state related to EthFw(attach/error, or new message from EthFw) polling state changes.
* Service name : Eth_VirtMac_MainFunction * Syntax : Std_ReturnType Eth_VirtMac_MainFunction(uint8 CtrlIdx) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : None * Sync/Async : Asynchronous * Reentrancy : Non-Reentrant * Parameters (in) : CtrlIdx: Index of the controller within the context of the * Ethernet Drivere * Parameters (inout): None * Parameters (out) : None * Return value : None * * Description : The function check the controller state(firmware attach state or * recovery state) *