![]() |
MCUSW
|
This file contains interface header for SPI MCAL driver.
Go to the source code of this file.
SPI Buffer Definition | |
| #define | SPI_IB (0U) |
| Buffer definitions IB - internal buffers. | |
| #define | SPI_EB (1U) |
| Buffer definitions EB - external buffers. Only this is supported. | |
| #define | SPI_IB_EB (2U) |
| Buffer definitions IB/EB - internal/external buffers. | |
| typedef uint8 | Spi_DataBufferType |
| Type of application data buffer elements. | |
| typedef uint16 | Spi_NumberOfDataType |
| Type for defining the number of data elements of the type Spi_DataBufferType to send and / or receive by Channel. | |
| typedef uint8 | Spi_ChannelType |
| Specifies the identification (ID) for a Channel. | |
| typedef uint16 | Spi_JobType |
| Specifies the identification (ID) for a Job. | |
| typedef uint8 | Spi_SequenceType |
| Specifies the identification (ID) for a sequence of jobs. | |
| typedef uint8 | Spi_HWUnitType |
| Specifies the identification (ID) for a SPI Hardware micro controller peripheral (unit) | |
SPI Config Ids | |
The Config Ids used for different SPI Configuration builds | |
| #define | SPI_CFG_ID_0 (0x01U) |
| Config 0 (All configurations ON), Scaleability level 2) | |
| #define | SPI_CFG_ID_1 (0x02U) |
| Config 1 (All configurations OFF). SPI_CFG_ID_1 is used only for compile check. | |
| #define | SPI_CFG_ID_2 (0x04U) |
| Config 2 (All configurations ON except DET OFF) | |
| #define | SPI_CFG_ID_3 (0x08U) |
| Config 3 (Configurator auto generated file) | |
| #define | SPI_CFG_ID_4 (0x10U) |
| Config 4 (Config is used only by Unit Test, Scaleability level 0) | |
| #define | SPI_CFG_ID_5 (0x20U) |
| Config 5 (Config is used only by Unit Test for DMA | |
| #define | SPI_CFG_ID_6 (0x40U) |
| Config 6 (Config is used only by Unit Test for DMA. | |
| #define | SPI_CFG_ID_7 (0x80U) |
| Config 7 (Performance testing only, level 2, asynch, no DMA) | |
| enum | Spi_StatusType { SPI_UNINIT = 0U , SPI_IDLE = 1U , SPI_BUSY = 2U } |
| This type defines a range of specific status for SPI Handler/Driver. More... | |
| enum | Spi_JobResultType { SPI_JOB_OK = 0U , SPI_JOB_PENDING = 1U , SPI_JOB_FAILED = 2U , SPI_JOB_QUEUED = 3U } |
| This type defines a range of specific Jobs status for SPI Handler/Driver. More... | |
| enum | Spi_SeqResultType { SPI_SEQ_OK = 0U , SPI_SEQ_PENDING = 1U , SPI_SEQ_FAILED = 2U , SPI_SEQ_CANCELLED = 3U } |
| This type defines a range of specific Sequences status for SPI Handler/Driver. More... | |
| enum | Spi_HwUnitResultType { SPI_HW_UNIT_OK = 0U , SPI_HW_UNIT_PENDING = 1U , SPI_HW_UNIT_FAILED = 2U } |
| This type defines a range of specific HW unit status for SPI Handler/Driver. More... | |
| enum | Spi_AsyncModeType { SPI_POLLING_MODE = 0U , SPI_INTERRUPT_MODE = 1U } |
| Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2. More... | |
| enum | Spi_TransferType { SPI_MSB = 0U , SPI_LSB = 1U } |
| Word transfer order - MSB first or LSB first. More... | |
| enum | Spi_LevelType { SPI_LOW = STD_LOW , SPI_HIGH } |
| Type for SPI Chip Select Polarity and Clock Idle Level. More... | |
| enum | Spi_CsPinType { SPI_CS0 = 0U , SPI_CS1 , SPI_CS2 , SPI_CS3 } |
| SPI Chip Select Pin. More... | |
| enum | Spi_ClkMode { SPI_CLK_MODE_0 = 0x00U , SPI_CLK_MODE_1 = 0x01U , SPI_CLK_MODE_2 = 0x02U , SPI_CLK_MODE_3 = 0x03U } |
| SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping. So don't change value. More... | |
| enum | Spi_TxRxMode { SPI_TX_RX_MODE_BOTH = 0x00U , SPI_TX_RX_MODE_TX_ONLY = 0x02U } |
| SPI TX/RX Mode. More... | |
| enum | Spi_JobPriorityType { SPI_JOB_PRIORITY_0 = 0U , SPI_JOB_PRIORITY_1 , SPI_JOB_PRIORITY_2 , SPI_JOB_PRIORITY_3 } |
| SPI Job Priority. More... | |
| enum | Spi_CsModeType { SPI_SINGLE = 0U , SPI_CONTINUOUS = 1U } |
| SPI Chip Select Mode. More... | |
| enum | Spi_DataDelayType { SPI_DATADELAY_0 = 0U , SPI_DATADELAY_1 = 1U , SPI_DATADELAY_2 = 2U , SPI_DATADELAY_3 = 3U } |
| Spi_DataDelayType defines the number of interface clock cycles between CS toggling and first or last edge of MCSPI clock. More... | |
| enum | Spi_DataLineReceiveType { DATA_LINE_0_RECEPTION = 0U , DATA_LINE_1_RECEPTION = 1U } |
| Spi_DataLineReceiveType defines the lines selected for reception. More... | |
| enum | Spi_DataLineTransmitType { DATA_LINE_NO_TRANSMISSION = 0x3U , DATA_LINE_0_TRANSMISSION = 0x2U , DATA_LINE_1_TRANSMISSION = 0x1U , DATA_LINE_BOTH_TRANSMISSION = 0x0U } |
| Spi_DataLineTransmitType defines the lines selected for transmission. More... | |
| enum | Mcspi_IrqStatusType { SPI_NO_EVENT = 0U , SPI_EVENT_PENDING = 1U , SPI_STATUS_READ_FAIL = 2U } |
| Irq status and std return type. More... | |
| typedef void(* | Spi_CacheWbInv) (uint8 *BufPtr, uint16 LenByte) |
| Cache write-back invalidate function. | |
| typedef void(* | Spi_CacheWb) (uint8 *BufPtr, uint16 LenByte) |
| Cache write-back function. | |
| typedef void(* | Spi_CacheInv) (uint8 *BufPtr, uint16 LenByte) |
| Cache invalidate function. | |
| void | Spi_Init (const Spi_ConfigType *CfgPtr) |
| Service for SPI initialization. | |
| Std_ReturnType | Spi_DeInit (void) |
| Service for SPI de-initialization. | |
| Spi_StatusType | Spi_GetStatus (void) |
| Service returns the SPI Handler/Driver software module status. | |
| Spi_JobResultType | Spi_GetJobResult (Spi_JobType Job) |
| This service returns the last transmission result of the specified Job. | |
| Spi_SeqResultType | Spi_GetSequenceResult (Spi_SequenceType Sequence) |
| This service returns the last transmission result of the specified Sequence. | |
| void | Spi_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. | |
| Spi_StatusType | Spi_GetHWUnitStatus (Spi_HWUnitType HWUnit) |
| This service returns the status of the specified SPI Hardware microcontroller peripheral. | |
| Std_ReturnType | Spi_WriteIB (Spi_ChannelType Channel, const Spi_DataBufferType *DataBufferPtr) |
| Service for writing one or more data to an IB SPI Handler/Driver Channel specified by parameter. | |
| Std_ReturnType | Spi_ReadIB (Spi_ChannelType Channel, Spi_DataBufferType *DataBufferPointer) |
| Service for reading synchronously one or more data from an IB SPI Handler/Driver Channel specified by parameter. | |
| Std_ReturnType | Spi_SetupEB (Spi_ChannelType Channel, const Spi_DataBufferType *SrcDataBufferPtr, Spi_DataBufferType *DesDataBufferPtr, Spi_NumberOfDataType Length) |
| Service to setup the buffers and the length of data for the EB SPI Handler/Driver Channel specified. | |
| Std_ReturnType | Spi_AsyncTransmit (Spi_SequenceType Sequence) |
| Service to transmit data on the SPI bus. | |
| void | Spi_Cancel (Spi_SequenceType Sequence) |
| Service cancels the specified on-going sequence transmission. | |
| Std_ReturnType | Spi_SyncTransmit (Spi_SequenceType Sequence) |
| Service to transmit data on the SPI bus. | |
| Std_ReturnType | Spi_SetAsyncMode (Spi_AsyncModeType Mode) |
| Service to set the asynchronous mechanism mode for SPI busses handled asynchronously. | |
| void | Spi_MainFunction_Handling (void) |
| This function polls the SPI interrupts linked to HW Units allocated to the transmission of SPI sequences to enable the evolution of transmission state machine. | |
| Std_ReturnType | Spi_RegisterReadback (Spi_HWUnitType HWUnit, Spi_RegisterReadbackType *RegRbPtr) |
| This function reads the important registers of the hardware unit and returns the value in the structure. | |
| Std_ReturnType | Spi_dataOverflowUnderflowIntrEnable (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function Enable Under/Overflow Interupts of the hardware unit and returns the status. | |
| Std_ReturnType | Spi_dataOverflowUnderflowIntrDisable (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function Disable Under/Overflow Interupts of the hardware unit and returns the status. | |
| Mcspi_IrqStatusType | Spi_dataOverflowUnderflowIntrGetStatus (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function status Under/Overflow Interupts of the hardware unit and returns the status. | |
| Std_ReturnType | Spi_dataOverflowUnderflowIntrStatusClear (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function status clear Under/Overflow Interupts of the hardware unit and returns the status. | |
Data Structures | |
| struct | Spi_ChannelConfigType |
| SPI Channel configuration structure. More... | |
| struct | Spi_McspiExternalDeviceConfigType |
| SPI Job configuration structure specific to McSPI peripheral. More... | |
| struct | Spi_ExternalDeviceConfigType |
| SPI external device specific configuration structure . More... | |
| struct | Spi_JobConfigType |
| SPI Job configuration structure. More... | |
| struct | Spi_SeqConfigType |
| SPI Sequence configuration structure. More... | |
| struct | Spi_HwUnitConfigType |
| SPI Hardware unit configuration structure. More... | |
| struct | Spi_ConfigType |
| SPI config structure. More... | |
| struct | Spi_ChannelConfigType_PC |
| SPI channel config structure parameters Pre-Compile only. More... | |
| struct | Spi_JobConfigType_PC |
| SPI job config structure parameters Pre-Compile only. More... | |
| struct | Spi_SeqConfigType_PC |
| SPI sequence config structure parameters Pre-Compile only. More... | |
| struct | Spi_RegisterReadbackType |
| SPI register readback structure. More... | |
Macros | |
SPI Driver Module SW Version Info | |
Defines for SPI Driver version used for compatibility checks | |
| #define | SPI_SW_MAJOR_VERSION (9U) |
| Driver Implementation Major Version. | |
| #define | SPI_SW_MINOR_VERSION (1U) |
| Driver Implementation Minor Version. | |
| #define | SPI_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. | |
SPI Driver Module AUTOSAR Version Info | |
Defines for SPI Driver AUTOSAR version used for compatibility checks | |
| #define | SPI_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by SPI Driver. | |
| #define | SPI_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by SPI Driver. | |
| #define | SPI_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by SPI Driver. | |
SPI Driver ID Info | |
| #define | SPI_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. | |
| #define | SPI_MODULE_ID ((uint16) 83U) |
| SPI Driver Module ID. | |
| #define | SPI_INSTANCE_ID ((uint8) 0U) |
| SPI Driver Instance ID. | |
SPI Error Codes | |
Error codes returned by SPI functions | |
| #define | SPI_E_PARAM_CHANNEL ((uint8) 0x0AU) |
| API service called with wrong parameter. | |
| #define | SPI_E_PARAM_JOB ((uint8) 0x0BU) |
| API service called with wrong parameter. | |
| #define | SPI_E_PARAM_SEQ ((uint8) 0x0CU) |
| API service called with wrong parameter. | |
| #define | SPI_E_PARAM_LENGTH ((uint8) 0x0DU) |
| API service called with wrong parameter. | |
| #define | SPI_E_PARAM_UNIT ((uint8) 0x0EU) |
| API service called with wrong parameter. | |
| #define | SPI_E_PARAM_POINTER ((uint8) 0x10U) |
| APIs called with a Null Pointer. | |
| #define | SPI_E_UNINIT ((uint8) 0x1AU) |
| API service used without module initiali-zation. | |
| #define | SPI_E_SEQ_PENDING ((uint8) 0x2AU) |
| Services called in a wrong sequence. | |
| #define | SPI_E_SEQ_IN_PROCESS ((uint8) 0x3AU) |
| Synchronous transmission service called at wrong time. | |
| #define | SPI_E_ALREADY_INITIALIZED ((uint8) 0x4AU) |
| API Spi_Init service called while the SPI driver has already been initialized. | |
| #define | SPI_E_SEQUENCE_NOT_OK ((uint8) 0x5AU) |
| Sequence did not complete successfully. | |
SPI Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | SPI_SID_INIT ((uint8) 0x00U) |
| Spi_Init() API Service ID. | |
| #define | SPI_SID_DEINIT ((uint8) 0x01U) |
| Spi_DeInit() API Service ID. | |
| #define | SPI_SID_WRITE_IB ((uint8) 0x02U) |
| Spi_WriteIB() API Service ID. | |
| #define | SPI_SID_ASYNC_TRANSMIT ((uint8) 0x03U) |
| Spi_AsyncTransmit() API Service ID. | |
| #define | SPI_SID_READ_IB ((uint8) 0x04U) |
| Spi_ReadIB() API Service ID. | |
| #define | SPI_SID_SETUP_EB ((uint8) 0x05U) |
| Spi_SetupEB() API Service ID. | |
| #define | SPI_SID_GET_STATUS ((uint8) 0x06U) |
| Spi_GetStatus() API Service ID. | |
| #define | SPI_SID_GET_JOB_RESULT ((uint8) 0x07U) |
| Spi_GetJobResult() API Service ID. | |
| #define | SPI_SID_GET_SEQ_RESULT ((uint8) 0x08U) |
| Spi_GetSequenceResult() API Service ID. | |
| #define | SPI_SID_GET_VERSION_INFO ((uint8) 0x09U) |
| Spi_GetVersionInfo() API Service ID. | |
| #define | SPI_SID_SYNC_TRANSMIT ((uint8) 0x0AU) |
| Spi_SyncTransmit() API Service ID. | |
| #define | SPI_SID_GET_HW_UNIT_STATUS ((uint8) 0x0BU) |
| Spi_GetHWUnitStatus() API Service ID. | |
| #define | SPI_SID_CANCEL ((uint8) 0x0CU) |
| Spi_Cancel() API Service ID. | |
| #define | SPI_SID_SET_ASYNC_MODE ((uint8) 0x0DU) |
| Spi_SetAsyncMode() API Service ID. | |
| #define | SPI_SID_MAINFUNCTION_HANDLING ((uint8) 0x10U) |
| Spi_MainFunction_Handling() API Service ID. | |
| #define | SPI_MCSPI_FCLK (48000000U) |
| MCSPI functional clock input in Hz. This clock is used to generate the serial clock output after the divider. | |