![]() |
MCUSW
|
Data Structures | |
| struct | Mcu_ClockConfigType |
| Structure for module clock setting. More... | |
| struct | Mcu_ConfigType |
| MCU CONFIG ROOT structure. More... | |
Variables | |
| const struct Mcu_ConfigType_s | McuModuleConfiguration_0 |
| MCU Configuration struct declaration. More... | |
Typedefs | |
| typedef uint8 | Mcu_ClockType |
| This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock() More... | |
| typedef uint32 | Mcu_RawResetType |
| This type specifies the identification (ID) for a RAW MCU reset status returned by Mcu_GetResetRawValue() More... | |
| typedef uint8 | Mcu_RamSectionType |
| This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection() More... | |
| typedef uint8 | Mcu_ModeType |
| This type specifies the identification (ID) for a MCU mode used in Mcu_SetMode() More... | |
| typedef const Mcu_ClockConfigType * | Mcu_ClockConfigPtrType |
| Pointer to Clock Config structure. More... | |
Macros | |
| #define | ARRAYSIZE(array) |
| #define | MCU_E_MODE_FAILURE 0U |
MCU Driver Module SW Version Info | |
Defines for MCU Driver version used for compatibility checks | |
| #define | MCU_SW_MAJOR_VERSION (10U) |
| Driver Implementation Major Version. More... | |
| #define | MCU_SW_MINOR_VERSION (0U) |
| Driver Implementation Minor Version. More... | |
| #define | MCU_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
MCU Driver Module AUTOSAR Version Info | |
Defines for MCU Driver AUTOSAR version used for compatibility checks | |
| #define | MCU_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by MCU Driver. More... | |
| #define | MCU_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by MCU Driver. More... | |
| #define | MCU_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by MCU Driver. More... | |
MCU Driver ID Info | |
| #define | MCU_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. More... | |
| #define | MCU_MODULE_ID ((uint16) 101U) |
| MCU Driver Module ID. More... | |
| #define | MCU_INSTANCE_ID ((uint8) 0U) |
| MCU Driver Instance ID. More... | |
MCU Error Codes | |
| #define | MCU_E_PARAM_CONFIG (0x0AU) |
| ERROR Description: API service called with wrong configuration parameter. More... | |
| #define | MCU_E_PARAM_CLOCK (0x0BU) |
| ERROR Description: API service used with wrong clock value. More... | |
| #define | MCU_E_PARAM_MODE (0x0CU) |
| ERROR Description: API service used with wrong mode. More... | |
| #define | MCU_E_PARAM_RAMSECTION (0x0DU) |
| ERROR Description: API service called with invalid/wrong RAM section. More... | |
| #define | MCU_E_PLL_NOT_LOCKED (0x0EU) |
| ERROR Description: API service is called while PLL is not locked. More... | |
| #define | MCU_E_UNINIT (0x0FU) |
| ERROR Description: Mcu Driver API service is called before initialization of MCU Driver. More... | |
| #define | MCU_E_PARAM_POINTER (0x10U) |
| ERROR Description: API service is called with NULL/Wrong pointer. More... | |
| #define | MCU_E_INIT_FAILED (0x11U) |
| ERROR Description: Initialization of the MCU Driver Failed. More... | |
MCU Driver State Values | |
| #define | MCU_STATUS_UNINIT ((uint8)(0U)) |
| MCU driver Status uninitialized. More... | |
| #define | MCU_STATUS_INIT ((uint8)(1U)) |
| MCU driver Status Initialized. More... | |
MCU Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | MCU_SID_INIT (0x00U) |
| Mcu_Init() API Service ID. More... | |
| #define | MCU_SID_INIT_RAM_SECTION (0x01U) |
| Mcu_InitRamSection() API Service ID. More... | |
| #define | MCU_SID_INIT_CLOCK (0x02U) |
| Mcu_InitClock() API Service ID. More... | |
| #define | MCU_SID_DISTRIBUTE_PLL_CLOCK (0x03U) |
| Mcu_DistributePllClock() API Service ID. More... | |
| #define | MCU_SID_GET_PLL_STATUS (0x04U) |
| Mcu_GetPllStatus() API Service ID. More... | |
| #define | MCU_SID_GET_RESET_REASON (0x05U) |
| Mcu_GetResetReason() API Service ID. More... | |
| #define | MCU_SID_GET_RESET_RAW_VALUE (0x06U) |
| Mcu_GetResetRawValue() API Service ID. More... | |
| #define | MCU_SID_PERFORM_RESET (0x07U) |
| Mcu_PerformReset() API Service ID. More... | |
| #define | MCU_SID_SETMODE (0x08U) |
| Mcu_SetMode() API Service ID. More... | |
| #define | MCU_SID_GET_VERSION_INFO (0x09U) |
| Mcu_GetVersionInfo() API Service ID. More... | |
| #define | MCU_SID_GET_RAM_STATE (0x0AU) |
| Mcu_GetRamState() API Service ID. More... | |
MCU Reset Modes | |
Reset mode enum which can be used in Mcu_PerformReset() | |
| #define | MCU_PERFORM_RESET_MODE_COLD ((uint8) 0U) |
| Initiate SW COLD RESET sequence. More... | |
| #define | MCU_PERFORM_RESET_MODE_WARM ((uint8) 1U) |
| Initiate SW WARM RESET sequence. More... | |
| #define ARRAYSIZE | ( | array | ) |
| #define MCU_SW_MAJOR_VERSION (10U) |
Driver Implementation Major Version.
| #define MCU_SW_MINOR_VERSION (0U) |
Driver Implementation Minor Version.
| #define MCU_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version.
| #define MCU_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by MCU Driver.
| #define MCU_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by MCU Driver.
| #define MCU_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by MCU Driver.
| #define MCU_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID.
| #define MCU_MODULE_ID ((uint16) 101U) |
MCU Driver Module ID.
| #define MCU_INSTANCE_ID ((uint8) 0U) |
MCU Driver Instance ID.
| #define MCU_E_PARAM_CONFIG (0x0AU) |
ERROR Description: API service called with wrong configuration parameter.
| #define MCU_E_PARAM_CLOCK (0x0BU) |
ERROR Description: API service used with wrong clock value.
| #define MCU_E_PARAM_MODE (0x0CU) |
ERROR Description: API service used with wrong mode.
| #define MCU_E_PARAM_RAMSECTION (0x0DU) |
ERROR Description: API service called with invalid/wrong RAM section.
| #define MCU_E_PLL_NOT_LOCKED (0x0EU) |
ERROR Description: API service is called while PLL is not locked.
| #define MCU_E_UNINIT (0x0FU) |
ERROR Description: Mcu Driver API service is called before initialization of MCU Driver.
| #define MCU_E_PARAM_POINTER (0x10U) |
ERROR Description: API service is called with NULL/Wrong pointer.
| #define MCU_E_INIT_FAILED (0x11U) |
ERROR Description: Initialization of the MCU Driver Failed.
| #define MCU_STATUS_UNINIT ((uint8)(0U)) |
MCU driver Status uninitialized.
| #define MCU_STATUS_INIT ((uint8)(1U)) |
MCU driver Status Initialized.
| #define MCU_SID_INIT (0x00U) |
Mcu_Init() API Service ID.
| #define MCU_SID_INIT_RAM_SECTION (0x01U) |
Mcu_InitRamSection() API Service ID.
| #define MCU_SID_INIT_CLOCK (0x02U) |
Mcu_InitClock() API Service ID.
| #define MCU_SID_DISTRIBUTE_PLL_CLOCK (0x03U) |
Mcu_DistributePllClock() API Service ID.
| #define MCU_SID_GET_PLL_STATUS (0x04U) |
Mcu_GetPllStatus() API Service ID.
| #define MCU_SID_GET_RESET_REASON (0x05U) |
Mcu_GetResetReason() API Service ID.
| #define MCU_SID_GET_RESET_RAW_VALUE (0x06U) |
Mcu_GetResetRawValue() API Service ID.
| #define MCU_SID_PERFORM_RESET (0x07U) |
Mcu_PerformReset() API Service ID.
| #define MCU_SID_SETMODE (0x08U) |
Mcu_SetMode() API Service ID.
| #define MCU_SID_GET_VERSION_INFO (0x09U) |
Mcu_GetVersionInfo() API Service ID.
| #define MCU_SID_GET_RAM_STATE (0x0AU) |
Mcu_GetRamState() API Service ID.
| #define MCU_PERFORM_RESET_MODE_COLD ((uint8) 0U) |
Initiate SW COLD RESET sequence.
| #define MCU_PERFORM_RESET_MODE_WARM ((uint8) 1U) |
Initiate SW WARM RESET sequence.
| #define MCU_E_MODE_FAILURE 0U |
| typedef uint8 Mcu_ClockType |
This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock()
| typedef uint32 Mcu_RawResetType |
This type specifies the identification (ID) for a RAW MCU reset status returned by Mcu_GetResetRawValue()
| typedef uint8 Mcu_RamSectionType |
This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection()
| typedef uint8 Mcu_ModeType |
This type specifies the identification (ID) for a MCU mode used in Mcu_SetMode()
| typedef const Mcu_ClockConfigType* Mcu_ClockConfigPtrType |
Pointer to Clock Config structure.
| const struct Mcu_ConfigType_s McuModuleConfiguration_0 |
MCU Configuration struct declaration.