![]() |
MCUSW
|
This file contains interface header for MCU MCAL driver.
Go to the source code of this file.
Data Structures | |
| struct | Mcu_ClockConfigType |
| Structure for module clock setting. More... | |
| struct | Mcu_ConfigType |
| MCU CONFIG ROOT structure. More... | |
Macros | |
| #define | ARRAYSIZE(array) |
| #define | MCU_E_MODE_FAILURE 0U |
MCU Driver Module SW Version Info | |
Defines for MCU Driver version used for compatibility checks | |
| #define | MCU_SW_MAJOR_VERSION (10U) |
| Driver Implementation Major Version. More... | |
| #define | MCU_SW_MINOR_VERSION (0U) |
| Driver Implementation Minor Version. More... | |
| #define | MCU_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
MCU Driver Module AUTOSAR Version Info | |
Defines for MCU Driver AUTOSAR version used for compatibility checks | |
| #define | MCU_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by MCU Driver. More... | |
| #define | MCU_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by MCU Driver. More... | |
| #define | MCU_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by MCU Driver. More... | |
MCU Driver ID Info | |
| #define | MCU_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. More... | |
| #define | MCU_MODULE_ID ((uint16) 101U) |
| MCU Driver Module ID. More... | |
| #define | MCU_INSTANCE_ID ((uint8) 0U) |
| MCU Driver Instance ID. More... | |
MCU Error Codes | |
Error codes returned by MCU functions | |
| #define | MCU_E_PARAM_CONFIG (0x0AU) |
| ERROR Description: API service called with wrong configuration parameter. More... | |
| #define | MCU_E_PARAM_CLOCK (0x0BU) |
| ERROR Description: API service used with wrong clock value. More... | |
| #define | MCU_E_PARAM_MODE (0x0CU) |
| ERROR Description: API service used with wrong mode. More... | |
| #define | MCU_E_PARAM_RAMSECTION (0x0DU) |
| ERROR Description: API service called with invalid/wrong RAM section. More... | |
| #define | MCU_E_PLL_NOT_LOCKED (0x0EU) |
| ERROR Description: API service is called while PLL is not locked. More... | |
| #define | MCU_E_UNINIT (0x0FU) |
| ERROR Description: Mcu Driver API service is called before initialization of MCU Driver. More... | |
| #define | MCU_E_PARAM_POINTER (0x10U) |
| ERROR Description: API service is called with NULL/Wrong pointer. More... | |
| #define | MCU_E_INIT_FAILED (0x11U) |
| ERROR Description: Initialization of the MCU Driver Failed. More... | |
MCU Driver State Values | |
The MCU Driver State Values | |
| #define | MCU_STATUS_UNINIT ((uint8)(0U)) |
| MCU driver Status uninitialized. More... | |
| #define | MCU_STATUS_INIT ((uint8)(1U)) |
| MCU driver Status Initialized. More... | |
MCU Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | MCU_SID_INIT (0x00U) |
| Mcu_Init() API Service ID. More... | |
| #define | MCU_SID_INIT_RAM_SECTION (0x01U) |
| Mcu_InitRamSection() API Service ID. More... | |
| #define | MCU_SID_INIT_CLOCK (0x02U) |
| Mcu_InitClock() API Service ID. More... | |
| #define | MCU_SID_DISTRIBUTE_PLL_CLOCK (0x03U) |
| Mcu_DistributePllClock() API Service ID. More... | |
| #define | MCU_SID_GET_PLL_STATUS (0x04U) |
| Mcu_GetPllStatus() API Service ID. More... | |
| #define | MCU_SID_GET_RESET_REASON (0x05U) |
| Mcu_GetResetReason() API Service ID. More... | |
| #define | MCU_SID_GET_RESET_RAW_VALUE (0x06U) |
| Mcu_GetResetRawValue() API Service ID. More... | |
| #define | MCU_SID_PERFORM_RESET (0x07U) |
| Mcu_PerformReset() API Service ID. More... | |
| #define | MCU_SID_SETMODE (0x08U) |
| Mcu_SetMode() API Service ID. More... | |
| #define | MCU_SID_GET_VERSION_INFO (0x09U) |
| Mcu_GetVersionInfo() API Service ID. More... | |
| #define | MCU_SID_GET_RAM_STATE (0x0AU) |
| Mcu_GetRamState() API Service ID. More... | |
MCU Reset Modes | |
Reset mode enum which can be used in Mcu_PerformReset() | |
| #define | MCU_PERFORM_RESET_MODE_COLD ((uint8) 0U) |
| Initiate SW COLD RESET sequence. More... | |
| #define | MCU_PERFORM_RESET_MODE_WARM ((uint8) 1U) |
| Initiate SW WARM RESET sequence. More... | |
Typedefs | |
| typedef uint8 | Mcu_ClockType |
| This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock() More... | |
| typedef uint32 | Mcu_RawResetType |
| This type specifies the identification (ID) for a RAW MCU reset status returned by Mcu_GetResetRawValue() More... | |
| typedef uint8 | Mcu_RamSectionType |
| This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection() More... | |
| typedef uint8 | Mcu_ModeType |
| This type specifies the identification (ID) for a MCU mode used in Mcu_SetMode() More... | |
| typedef const Mcu_ClockConfigType * | Mcu_ClockConfigPtrType |
| Pointer to Clock Config structure. More... | |
Functions | |
| void | Mcu_Init (const Mcu_ConfigType *ConfigPtr) |
| This service initializes the MCU driver. More... | |
| Std_ReturnType | Mcu_ClockSetSource (Mcu_ClkModuleIdType moduleId, Mcu_ClkSourceIdType clkSrcId, uint8 clkParentId) |
| Std_ReturnType | Mcu_InitClock (Mcu_ClockType ClockSetting) |
| This service initializes the PLL and other MCU specific clock options. More... | |
| Std_ReturnType | Mcu_DistributePllClock (void) |
| This service activates the PLL clock to the MCU clock distribution. More... | |
| void | Mcu_PerformReset (void) |
| The service performs a microcontroller reset. More... | |
| Std_ReturnType | Mcu_InitRamSection (Mcu_RamSectionType RamSection) |
| This service initializes the RAM section wise. More... | |
| Mcu_PllStatusType | Mcu_GetPllStatus (void) |
| This service provides the lock status of the PLL. More... | |
| Mcu_ResetType | Mcu_GetResetReason (void) |
| The service reads the reset type from the hardware, if supported. More... | |
| Mcu_RawResetType | Mcu_GetResetRawValue (void) |
| The service reads the reset type from the hardware register, if supported. More... | |
| void | Mcu_ClearResetReason (void) |
| Clear the Mcu Reset reason by clearing the reset reason register. More... | |
| Mcu_RamStateType | Mcu_GetRamState (void) |
| This service provides the actual status of the microcontroller Ram. (if supported) More... | |
| void | Mcu_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. More... | |
| void | Mcu_SetMode (Mcu_ModeType McuMode) |
| This service activates the MCU power modes. More... | |
Variables | |
| const struct Mcu_ConfigType_s | McuModuleConfiguration_0 |
| MCU Configuration struct declaration. More... | |
| void Mcu_Init | ( | const Mcu_ConfigType * | ConfigPtr | ) |
This service initializes the MCU driver.
* Service name : Mcu_Init * Syntax : void Mcu_Init( const Mcu_ConfigType* ConfigPtr ) * Service ID[hex] : 0x0 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : ConfigPtr - Pointer to MCU driver configuration set. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This service initializes the MCU driver *
| Std_ReturnType Mcu_ClockSetSource | ( | Mcu_ClkModuleIdType | moduleId, |
| Mcu_ClkSourceIdType | clkSrcId, | ||
| uint8 | clkParentId | ||
| ) |
| Std_ReturnType Mcu_InitClock | ( | Mcu_ClockType | ClockSetting | ) |
This service initializes the PLL and other MCU specific clock options.
* Service name : Mcu_InitClock * Syntax : Std_ReturnType Mcu_InitClock( * Mcu_ClockType ClockSetting ) * Service ID[hex] : 0x02 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : ClockSetting - Clock setting * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Command has been accepted * - E_NOT_OK: Command has not been accepted * Description : This service initializes the PLL and other MCU specific * clock options *
| Std_ReturnType Mcu_DistributePllClock | ( | void | ) |
This service activates the PLL clock to the MCU clock distribution.
* Service name : Mcu_DistributePllClock * Syntax : Std_ReturnType Mcu_DistributePllClock(void) * Service ID[hex] : 0x03 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType : E_OK: Command has been accepted * E_NOT_OK: Command has not been accepted * Description : This service activates the PLL clock to the MCU clock distribution. *
| void Mcu_PerformReset | ( | void | ) |
The service performs a microcontroller reset.
* Service name : Mcu_PerformReset * Syntax : void Mcu_PerformReset( void ) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : The service performs a microcontroller reset *
| Std_ReturnType Mcu_InitRamSection | ( | Mcu_RamSectionType | RamSection | ) |
This service initializes the RAM section wise.
* Service name : Mcu_InitRamSection * Syntax : Std_ReturnType Mcu_InitRamSection( * Mcu_RamSectionType RamSection ) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : RamSection - Selects RAM memory section provided * in configuration set * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: command has been accepted * - E_NOT_OK: command has not been accepted e.g. due to * parameter error * Description : This service initializes the RAM section wise *
| Mcu_PllStatusType Mcu_GetPllStatus | ( | void | ) |
This service provides the lock status of the PLL.
* Service name : Mcu_GetPllStatus * Syntax : Mcu_PllStatusType Mcu_GetPllStatus( void ) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : Mcu_PllStatusType - PLL Status * Description : This service provides the lock status of the PLL. *
| Mcu_ResetType Mcu_GetResetReason | ( | void | ) |
The service reads the reset type from the hardware, if supported.
* Service name : Mcu_GetResetReason * Syntax : Mcu_ResetType Mcu_GetResetReason( void ) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : Mcu_ResetType * Description : The service reads the reset type from the hardware, if * supported *
| Mcu_RawResetType Mcu_GetResetRawValue | ( | void | ) |
The service reads the reset type from the hardware register, if supported.
* Service name : Mcu_GetResetRawValue * Syntax : Mcu_RawResetType Mcu_GetResetRawValue( void ) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : nONE * Parameters (inout): None * Parameters (out) : None * Return value : Mcu_RawResetType - Reset raw value * Description : The service reads the reset type from the hardware * register, if supported *
| void Mcu_ClearResetReason | ( | void | ) |
Clear the Mcu Reset reason by clearing the reset reason register.
* Service name : Mcu_ClearResetReason * Syntax : void Mcu_ClearResetReason(void) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Clear the Mcu Reset reason by clearing the reset reason * register *
| Mcu_RamStateType Mcu_GetRamState | ( | void | ) |
This service provides the actual status of the microcontroller Ram. (if supported)
* Service name : Mcu_GetRamState * Syntax : Mcu_RamStateType Mcu_GetRamState(void) * Service ID[hex] : 0x0a * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : Mcu_RamStateType - Status of the Ram Content * Description : This service provides the actual status of the * microcontroller Ram. (if supported) *
| void Mcu_GetVersionInfo | ( | Std_VersionInfoType * | versioninfo | ) |
This service returns the version information of this module.
* Service name : Mcu_GetVersionInfo * Syntax : void Mcu_GetVersionInfo(Std_VersionInfoType* * versioninfo) * Service ID[hex] : 0x09 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : versioninfo - Pointer to where to store the * version information of this module. * Return value : None * Description : This service returns the version information of this * module *
| void Mcu_SetMode | ( | Mcu_ModeType | McuMode | ) |
This service activates the MCU power modes.
* Service name : Mcu_SetMode * Syntax : void Mcu_SetMode(Mcu_ModeType McuMode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : McuMode : Set different MCU power modes configured in the configuration set * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This service activates the MCU power modes. *