105#define CAN_VARIANT_PRE_COMPILE (STD_ON)
113#define CAN_VERSION_INFO_API (STD_ON)
116#define CAN_DEV_ERROR_DETECT (STD_ON)
119#define CAN_SAFETY_DIAGNOSTIC (STD_ON)
122#define CAN_LOOPBACK_ENABLE (STD_ON)
125#define CAN_REGISTER_READBACK_API (STD_ON)
128#define CAN_SET_BAUDRATE_API (STD_ON)
131#define CAN_WAKEUP_FUNCTIONALITY_API (STD_OFF)
134#define CAN_MULTIPLEXED_TRANSMISSION_ENABLE (STD_ON)
142#define CAN_INIT_CONFIG_PC CanConfigSet
150#define CAN_TX_POLLING (STD_OFF)
152#define CAN_RX_POLLING (STD_OFF)
154#define CAN_BUSOFF_POLLING (STD_OFF)
156#define CAN_WAKEUP_POLLING (STD_OFF)
161#define CAN_NUM_CONTROLLER (3U)
164#define CAN_NUM_MAILBOXES (9U)
167#define CAN_MAX_CONTROLLER (16U)
170#define CAN_MAX_MAILBOXES (64U)
173#define CAN_ISR_TYPE (CAN_ISR_CAT1)
176#define CLK_CAN_FD_FREQ (80U)
185#define CanConf_CanController_CanController_0 (0U)
186#define CanConf_CanController_CanController_1 (1U)
187#define CanConf_CanController_CanController_2 (2U)
193#define CAN_CONTROLLER_MCU_MCAN0
196#define CAN_CONTROLLER_MCU_MCAN1
199#define CAN_CONTROLLER_MCAN0
288#define CanConf_CanHardwareObject_CanHardwareObject_0 (0U)
289#define CAN_HTRH_0 (CanConf_CanHardwareObject_CanHardwareObject_0)
291#define CanConf_CanHardwareObject_CanHardwareObject_1 (1U)
292#define CAN_HTRH_1 (CanConf_CanHardwareObject_CanHardwareObject_1)
294#define CanConf_CanHardwareObject_CanHardwareObject_2 (2U)
295#define CAN_HTRH_2 (CanConf_CanHardwareObject_CanHardwareObject_2)
297#define CanConf_CanHardwareObject_CanHardwareObject_3 (3U)
298#define CAN_HTRH_3 (CanConf_CanHardwareObject_CanHardwareObject_3)
300#define CanConf_CanHardwareObject_CanHardwareObject_4 (4U)
301#define CAN_HTRH_4 (CanConf_CanHardwareObject_CanHardwareObject_4)
303#define CanConf_CanHardwareObject_CanHardwareObject_5 (5U)
304#define CAN_HTRH_5 (CanConf_CanHardwareObject_CanHardwareObject_5)
306#define CanConf_CanHardwareObject_CanHardwareObject_6 (6U)
307#define CAN_HTRH_6 (CanConf_CanHardwareObject_CanHardwareObject_6)
309#define CanConf_CanHardwareObject_CanHardwareObject_7 (7U)
310#define CAN_HTRH_7 (CanConf_CanHardwareObject_CanHardwareObject_7)
312#define CanConf_CanHardwareObject_CanHardwareObject_8 (8U)
313#define CAN_HTRH_8 (CanConf_CanHardwareObject_CanHardwareObject_8)
320#define CAN_OS_COUNTER_ID ((CounterType)OsCounter_0)
327#define CAN_TIMEOUT_DURATION (10000U)
335#define DemConf_DemEventParameter_CAN_DEM_NO_EVENT (0xFFFFU)
336#define CAN_DEM_NO_EVENT DemConf_DemEventParameter_CAN_DEM_NO_EVENT
338#ifndef CAN_E_HARDWARE_ERROR
340#define CAN_E_HARDWARE_ERROR (DemConf_DemEventParameter_CAN_E_HARDWARE_ERROR)
364extern const struct Can_ControllerStruct_PC
368extern const struct Can_MailboxStruct_PC
397extern CONST(uint32, CAN_CONST)
400extern CONST(uint32, CAN_CONST)
403extern CONST(uint32, CAN_CONST)
406extern CONST(uint32, CAN_CONST)
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_1
CAN Controller Configuration Pre Compile struct declaration.
const struct Can_ConfigType_s CanConfigSet
CAN Configuration struct declaration.
Can_ControllerInstance
Can Controller Instances enum.
Definition Can_Cfg.h:378
void Can_2_Int0ISR(void)
MCAN0 Controller Instance ISR.
const uint32 Can_MCANECCAggrRegBaseAddr[CAN_MAX_CONTROLLER]
const uint32 Can_MCANSSBaseAddr[CAN_MAX_CONTROLLER]
void Can_1_Int0ISR(void)
MCU_MCAN1 Controller Instance ISR.
void Can_0_Int0ISR(void)
MCU_MCAN0 Controller Instance ISR.
#define CAN_MAX_CONTROLLER
Definition Can_Cfg.h:167
const uint32 Can_MsgmemRAMBaseAddr[CAN_MAX_CONTROLLER]
Base Address of the can peripherals.
const struct Can_ControllerStruct_PC * CanConfigSet_CanController_List_PC[CAN_NUM_CONTROLLER]
CAN Controller Pre Compile Configuration List.
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_0
CAN Controller Configuration Pre Compile struct declaration.
#define CAN_NUM_CONTROLLER
Definition Can_Cfg.h:161
const struct Can_MailboxStruct_PC * CanConfigSet_CanHardwareObject_List_PC[CAN_NUM_MAILBOXES]
CAN Mailbox Pre Compile Configuration List.
const uint32 Can_MCANCoreRegBaseAddr[CAN_MAX_CONTROLLER]
#define CAN_NUM_MAILBOXES
Definition Can_Cfg.h:164
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_2
CAN Controller Configuration Pre Compile struct declaration.
@ CAN_CONTROLLER_INSTANCE_MCU_MCAN0
Definition Can_Cfg.h:379
@ CAN_CONTROLLER_INSTANCE_MCAN0
Definition Can_Cfg.h:388
@ CAN_CONTROLLER_INSTANCE_MCU_MCAN1
Definition Can_Cfg.h:383