MCUSW
Loading...
Searching...
No Matches
Can Configuration

Introduction

This files defines CAN MCAL configuration structures

Data Structures

struct  Can_MaskType
 Structure defining the filter mask to be used. More...
 
struct  Can_HwFilterType
 Structure defining the HW filter to be used. More...
 
struct  Can_FdBaudConfigType
 Structure defining the CAN FD data phase baud rate configuration. More...
 
struct  Can_BaudConfigType
 Structure defining the CAN baud rate configuration. More...
 
struct  Can_ControllerType
 Can Controller Configuration definition. More...
 
struct  Can_ControllerType_PC
 Can Controller Pre Compile Configuration definition. More...
 
struct  Can_MailboxType
 Can mailox configuration definition. More...
 
struct  Can_MailboxType_PC
 Can mailox Pre compile configuration definition. More...
 
struct  Can_DmaPrms
 Dummy structure will be used if DMA support is required. More...
 
struct  Can_ConfigType
 Can MCAL root configuration structure. More...
 
struct  Can_RegisterReadbackType
 Register Readback Structure. More...
 

Variables

uint32 Can_MaskType::MaskValue
 
Can_IdType Can_HwFilterType::IDValue
 
uint32 Can_HwFilterType::Mask
 
uint16 Can_FdBaudConfigType::Baud
 
uint8 Can_FdBaudConfigType::PropSeg
 
uint8 Can_FdBaudConfigType::Pseg1
 
uint8 Can_FdBaudConfigType::Pseg2
 
uint8 Can_FdBaudConfigType::Sjw
 
uint16 Can_FdBaudConfigType::TimingValues
 
uint16 Can_FdBaudConfigType::BrpValue
 
uint16 Can_FdBaudConfigType::TrcvCompDelay
 
boolean Can_FdBaudConfigType::BrsSwitch
 
uint16 Can_BaudConfigType::Baud
 
uint8 Can_BaudConfigType::PropSeg
 
uint8 Can_BaudConfigType::Pseg1
 
uint8 Can_BaudConfigType::Pseg2
 
uint8 Can_BaudConfigType::Sjw
 
uint16 Can_BaudConfigType::TimingValues
 
uint16 Can_BaudConfigType::BrpValue
 
Can_FdBaudConfigType Can_BaudConfigType::BaudFdRateConfig
 
Can_BaudConfigTypeCan_ControllerType::DefaultBaud
 
Can_BaudConfigType ** Can_ControllerType::BaudRateConfigList
 
uint8 Can_ControllerType_PC::ControllerId
 
boolean Can_ControllerType_PC::CntrActive
 
uint32 Can_ControllerType_PC::CntrAddr
 
Can_TxRxProcessingType Can_ControllerType_PC::RxProcessingType
 
Can_TxRxProcessingType Can_ControllerType_PC::TxProcessingType
 
boolean Can_ControllerType_PC::BusOffProcessingInterrupt
 
Can_ControllerInstance Can_ControllerType_PC::CanControllerInst
 
boolean Can_ControllerType_PC::CanFDModeEnabled
 
uint8 Can_MailboxType::CanHandleType
 
uint32 Can_MailboxType::MBIdType
 
Can_HwHandleType Can_MailboxType::HwHandle
 
uint32 Can_MailboxType::CanHwObjectCount
 
Can_MailBoxDirectionType Can_MailboxType::MBDir
 
const Can_ControllerType_PCCan_MailboxType::Controller
 
Can_HwFilterType ** Can_MailboxType::HwFilterList
 
uint32 Can_MailboxType::HwFilterCnt
 
uint8 Can_MailboxType::CanFdPaddingValue
 
boolean Can_MailboxType::CanHardwareObjectUsesPolling
 
uint16 Can_MailboxType_PC::CanObjectId
 
uint32 Can_DmaPrms::Reserved
 
Can_ControllerType ** Can_ConfigType::CanControllerList
 
uint8 Can_ConfigType::CanMaxControllerCount
 
Can_MailboxType ** Can_ConfigType::MailBoxList
 
uint32 Can_ConfigType::MaxMbCnt
 
uint32 Can_ConfigType::MaxBaudConfigID [CAN_MAX_CONTROLLER]
 
Can_DmaPrmsCan_ConfigType::DmaPrms
 
uint32 Can_RegisterReadbackType::CanReadBackRegPID
 
uint32 Can_RegisterReadbackType::CanReadBackRegSTAT
 
uint32 Can_RegisterReadbackType::CanReadBackRegCREL
 
uint32 Can_RegisterReadbackType::CanReadBackRegENDN
 
uint32 Can_RegisterReadbackType::CanReadBackRegCTRL
 
uint32 Can_RegisterReadbackType::CanReadBackRegDBTP
 
uint32 Can_RegisterReadbackType::CanReadBackRegRWD
 
uint32 Can_RegisterReadbackType::CanReadBackRegCCCR
 
uint32 Can_RegisterReadbackType::CanReadBackRegNBTP
 
uint32 Can_RegisterReadbackType::CanReadBackRegTDCR
 
uint32 Can_RegisterReadbackType::CanReadBackRegGFC
 
uint32 Can_RegisterReadbackType::CanReadBackRegSIDFC
 
uint32 Can_RegisterReadbackType::CanReadBackRegXIDFC
 
uint32 Can_RegisterReadbackType::CanReadBackRegRXF0C
 
uint32 Can_RegisterReadbackType::CanReadBackRegRXBC
 
uint32 Can_RegisterReadbackType::CanReadBackRegRXF1C
 
uint32 Can_RegisterReadbackType::CanReadBackRegTXBC
 
uint32 Can_RegisterReadbackType::CanReadBackRegTXESC
 
uint32 Can_RegisterReadbackType::CanReadBackRegTXEFC
 

Macros

#define CAN_VARIANT_PRE_COMPILE   (STD_ON)
 CAN Build Variant. Build variants.(i.e Pre Compile,Post Build)
 

Can Error Types

Error Types returned by Can functions

enum  Can_MailBoxDirectionType { CAN_MAILBOX_DIRECTION_RX = 0x0U , CAN_MAILBOX_DIRECTION_TX = 0x1U }
 Can Mailbox direction enum. More...
 
enum  Can_HandleType { CAN_FULL = 0x0U , CAN_BASIC = 0x1U }
 Can Handle Type enum. More...
 
enum  Can_TxRxProcessingType { CAN_TX_RX_PROCESSING_INTERRUPT = 0x0U , CAN_TX_RX_PROCESSING_MIXED = 0x1U , CAN_TX_RX_PROCESSING_POLLING = 0x2U }
 Can Tx/Rx processing enum. More...
 
enum  Can_IrqStatusType {
  CAN_IRQ_NO_INTR_EVENT = 0U , CAN_IRQ_INTR_STUFF_EVENT = 1U , CAN_IRQ_INTR_FORM_EVENT = 2U , CAN_IRQ_INTR_ACK_EVENT = 3U ,
  CAN_IRQ_INTR_BIT1_EVENT = 4U , CAN_IRQ_INTR_BIT0_EVENT = 5U , CAN_IRQ_INTR_CRC_EVENT = 6U , CAN_IRQ_INTR_TOO_EVENT = 7U ,
  CAN_IRQ_STATUS_READ_FAIL = 8U
}
 CAN IRQ status enum. More...
 
typedef uint8 CanControllerState_Type
 Can Controller State enum type.
 
typedef uint32 Can_InterruptMask_Type
 Can Interrupt Mask type.
 
void Can_GetVersionInfo (Std_VersionInfoType *VersionInfo)
 Function returns the version information of this module.
 
void Can_Init (const Can_ConfigType *CfgPtr)
 This function initializes the module.
 
Std_ReturnType Can_SetControllerMode (uint8 Controller, Can_ControllerStateType Transition)
 This function performs software triggered state transitions of the CAN controller State machine.
 
Std_ReturnType Can_Write (Can_HwHandleType Hth, const Can_PduType *PduInfo)
 This function is called by CanIf to pass a CAN message to CanDrv for transmission.
 
void Can_DisableControllerInterrupts (uint8 Controller)
 This function disables all interrupts for this CAN controller.
 
void Can_EnableControllerInterrupts (uint8 Controller)
 This function enables all allowed interrupts.
 
void Can_MainFunction_Write (void)
 This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.
 
void Can_MainFunction_BusOff (void)
 This function performs the polling of bus-off events that are configured statically as 'to be polled'.
 
void Can_MainFunction_Read (void)
 This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.
 
void Can_MainFunction_Wakeup (void)
 This function performs the polling of wake-up events that are configured statically as 'to be polled'.
 
void Can_MainFunction_Mode (void)
 This function performs the polling of CAN controller mode transitions.
 
Std_ReturnType Can_SetBaudrate (uint8 Controller, uint16 BaudRateConfigID)
 This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset.
 
Std_ReturnType Can_TestLoopBackModeEnable (uint8 Controller, uint8 Mode)
 This service will enable CAN loopback mode.
 
Std_ReturnType Can_TestLoopBackModeDisable (uint8 Controller, uint8 Mode)
 This service will disable CAN loopback mode.
 
Std_ReturnType Can_RegisterReadback (VAR(uint8,) Controller, Can_RegisterReadbackType *RegRbPtr)
 This service will readback CAN registers.
 
Std_ReturnType Can_EnableIntr (VAR(uint8,) Controller, VAR(uint8,) CanErrVar)
 This service will Enable the interrupts.
 
Std_ReturnType Can_DisableIntr (VAR(uint8,) Controller, VAR(uint8,) CanErrVar)
 This service will Disable the Interrupts.
 
Can_IrqStatusType Can_GetIntrStatus (VAR(uint8,) Controller)
 This service will provide the status of the interrupt.
 
Std_ReturnType Can_ClearIntrStatus (VAR(uint8,) Controller)
 This service will clear the interrupt status.
 
void Can_IntISR_Fun (Can_ControllerInstance CanInstanceID)
 This function is the ISR for CAN controller 0/INT 0.
 
void Can_IntISR_Function (Can_ControllerInstance CanInstanceID, uint32 baseAddr)
 This function is the ISR for CAN controller 0/INT 0.
 
void Can_DeInit (void)
 This function de-initializes the module.
 
Std_ReturnType Can_GetControllerMode (uint8 Controller, Can_ControllerStateType *ControllerModePtr)
 This service reports about the current status of the requested CAN controller.
 
Std_ReturnType Can_GetControllerErrorState (uint8 ControllerId, Can_ErrorStateType *ErrorStatePtr)
 This service obtains the error state of the CAN controller.
 

CAN DEM Error codes to report

Pre-compile switches for enabling/disabling DEM events

enum  Can_ControllerInstance { CAN_CONTROLLER_INSTANCE_MCU_MCAN0 = 0U , CAN_CONTROLLER_INSTANCE_MCU_MCAN1 = 1U , CAN_CONTROLLER_INSTANCE_MCAN0 = 2U }
 Can Controller Instances enum. More...
 
const struct Can_ConfigType_s CanConfigSet
 CAN Configuration struct declaration.
 
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_0
 CAN Controller Configuration Pre Compile struct declaration.
 
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_1
 CAN Controller Configuration Pre Compile struct declaration.
 
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_2
 CAN Controller Configuration Pre Compile struct declaration.
 
const struct Can_ControllerStruct_PC * CanConfigSet_CanController_List_PC [CAN_NUM_CONTROLLER]
 CAN Controller Pre Compile Configuration List.
 
const struct Can_MailboxStruct_PC * CanConfigSet_CanHardwareObject_List_PC [CAN_NUM_MAILBOXES]
 CAN Mailbox Pre Compile Configuration List.
 
const uint32 Can_MsgmemRAMBaseAddr [CAN_MAX_CONTROLLER]
 Base Address of the can peripherals.
 
const uint32 Can_MCANSSBaseAddr [CAN_MAX_CONTROLLER]
 
const uint32 Can_MCANCoreRegBaseAddr [CAN_MAX_CONTROLLER]
 
const uint32 Can_MCANECCAggrRegBaseAddr [CAN_MAX_CONTROLLER]
 
void Can_0_Int0ISR (void)
 MCU_MCAN0 Controller Instance ISR.
 
void Can_1_Int0ISR (void)
 MCU_MCAN1 Controller Instance ISR.
 
void Can_2_Int0ISR (void)
 MCAN0 Controller Instance ISR.
 
#define DemConf_DemEventParameter_CAN_DEM_NO_EVENT   (0xFFFFU)
 
#define CAN_DEM_NO_EVENT   DemConf_DemEventParameter_CAN_DEM_NO_EVENT
 
#define CAN_E_HARDWARE_ERROR   (DemConf_DemEventParameter_CAN_E_HARDWARE_ERROR)
 Hardware failed.
 

Can Driver Configuration SW Version Info

Pre-compile switches for enabling/disabling CAN MCAL APIs

#define CAN_VERSION_INFO_API   (STD_ON)
 
#define CAN_DEV_ERROR_DETECT   (STD_ON)
 
#define CAN_SAFETY_DIAGNOSTIC   (STD_ON)
 
#define CAN_LOOPBACK_ENABLE   (STD_ON)
 
#define CAN_REGISTER_READBACK_API   (STD_ON)
 
#define CAN_SET_BAUDRATE_API   (STD_ON)
 
#define CAN_WAKEUP_FUNCTIONALITY_API   (STD_OFF)
 
#define CAN_MULTIPLEXED_TRANSMISSION_ENABLE   (STD_ON)
 
#define CAN_INIT_CONFIG_PC   CanConfigSet
 Pre Compile config macro name.
 
#define CAN_TX_POLLING   (STD_OFF)
 
#define CAN_RX_POLLING   (STD_OFF)
 
#define CAN_BUSOFF_POLLING   (STD_OFF)
 
#define CAN_WAKEUP_POLLING   (STD_OFF)
 
#define CAN_NUM_CONTROLLER   (3U)
 
#define CAN_NUM_MAILBOXES   (9U)
 
#define CAN_MAX_CONTROLLER   (16U)
 
#define CAN_MAX_MAILBOXES   (64U)
 
#define CAN_ISR_TYPE   (CAN_ISR_CAT1)
 
#define CLK_CAN_FD_FREQ   (80U)
 

Can Controller Id names

Defines for symbolic names for the CanControllerIds

#define CanConf_CanController_CanController_0   (0U)
 
#define CanConf_CanController_CanController_1   (1U)
 
#define CanConf_CanController_CanController_2   (2U)
 
#define CAN_CONTROLLER_MCU_MCAN0
 
#define CAN_CONTROLLER_MCU_MCAN1
 
#define CAN_CONTROLLER_MCAN0
 

Can HW Object names

Defines for symbolic names for the CanHardwareObjectIds

#define CanConf_CanHardwareObject_CanHardwareObject_0   (0U)
 
#define CAN_HTRH_0   (CanConf_CanHardwareObject_CanHardwareObject_0)
 
#define CanConf_CanHardwareObject_CanHardwareObject_1   (1U)
 
#define CAN_HTRH_1   (CanConf_CanHardwareObject_CanHardwareObject_1)
 
#define CanConf_CanHardwareObject_CanHardwareObject_2   (2U)
 
#define CAN_HTRH_2   (CanConf_CanHardwareObject_CanHardwareObject_2)
 
#define CanConf_CanHardwareObject_CanHardwareObject_3   (3U)
 
#define CAN_HTRH_3   (CanConf_CanHardwareObject_CanHardwareObject_3)
 
#define CanConf_CanHardwareObject_CanHardwareObject_4   (4U)
 
#define CAN_HTRH_4   (CanConf_CanHardwareObject_CanHardwareObject_4)
 
#define CanConf_CanHardwareObject_CanHardwareObject_5   (5U)
 
#define CAN_HTRH_5   (CanConf_CanHardwareObject_CanHardwareObject_5)
 
#define CanConf_CanHardwareObject_CanHardwareObject_6   (6U)
 
#define CAN_HTRH_6   (CanConf_CanHardwareObject_CanHardwareObject_6)
 
#define CanConf_CanHardwareObject_CanHardwareObject_7   (7U)
 
#define CAN_HTRH_7   (CanConf_CanHardwareObject_CanHardwareObject_7)
 
#define CanConf_CanHardwareObject_CanHardwareObject_8   (8U)
 
#define CAN_HTRH_8   (CanConf_CanHardwareObject_CanHardwareObject_8)
 
#define CAN_OS_COUNTER_ID   ((CounterType)OsCounter_0)
 Counter ID for counter used to count wait ticks.
 
#define CAN_TIMEOUT_DURATION   (10000U)
 CAN timeout - used in CAN IFCMD busy wait and Start/Stop busy wait. Specifies the maximum time for blocking function until a timeout is detected. Unit is milli seconds.
 

Macro Definition Documentation

◆ CAN_VARIANT_PRE_COMPILE

#define CAN_VARIANT_PRE_COMPILE   (STD_ON)

CAN Build Variant. Build variants.(i.e Pre Compile,Post Build)

◆ CAN_VERSION_INFO_API

#define CAN_VERSION_INFO_API   (STD_ON)

Enable/Disable Can_GetVersionInfo()

◆ CAN_DEV_ERROR_DETECT

#define CAN_DEV_ERROR_DETECT   (STD_ON)

Enable/Disable DEV error detection

◆ CAN_SAFETY_DIAGNOSTIC

#define CAN_SAFETY_DIAGNOSTIC   (STD_ON)

Enable/Disable Can Safety Diagnostic

◆ CAN_LOOPBACK_ENABLE

#define CAN_LOOPBACK_ENABLE   (STD_ON)

◆ CAN_REGISTER_READBACK_API

#define CAN_REGISTER_READBACK_API   (STD_ON)

Enable/Disable Can_ConfigRegReadBack()

◆ CAN_SET_BAUDRATE_API

#define CAN_SET_BAUDRATE_API   (STD_ON)

Enable/Disable Can_SetBaudrate() API

◆ CAN_WAKEUP_FUNCTIONALITY_API

#define CAN_WAKEUP_FUNCTIONALITY_API   (STD_OFF)

Enable/Disable Can_CheckWakeup()

◆ CAN_MULTIPLEXED_TRANSMISSION_ENABLE

#define CAN_MULTIPLEXED_TRANSMISSION_ENABLE   (STD_ON)

Enable/Disable Multiplexed Transmission

◆ CAN_INIT_CONFIG_PC

#define CAN_INIT_CONFIG_PC   CanConfigSet

Pre Compile config macro name.

◆ CAN_TX_POLLING

#define CAN_TX_POLLING   (STD_OFF)

Enable/Disable Can_MainFunction_Write

◆ CAN_RX_POLLING

#define CAN_RX_POLLING   (STD_OFF)

Enable/Disable Can_MainFunction_Read

◆ CAN_BUSOFF_POLLING

#define CAN_BUSOFF_POLLING   (STD_OFF)

Enable/Disable Can_MainFunction_BusOff

◆ CAN_WAKEUP_POLLING

#define CAN_WAKEUP_POLLING   (STD_OFF)

Enable/Disable Can_MainFunction_Wakeup

◆ CAN_NUM_CONTROLLER

#define CAN_NUM_CONTROLLER   (3U)

Number of controllers defined

◆ CAN_NUM_MAILBOXES

#define CAN_NUM_MAILBOXES   (9U)

Number of mailboxes defined

◆ CAN_MAX_CONTROLLER

#define CAN_MAX_CONTROLLER   (16U)

Max number of controller instances per SOC

◆ CAN_MAX_MAILBOXES

#define CAN_MAX_MAILBOXES   (64U)

Max number of mailboxes per controller

◆ CAN_ISR_TYPE

#define CAN_ISR_TYPE   (CAN_ISR_CAT1)

OSEK Category 1 ISR Type

◆ CLK_CAN_FD_FREQ

#define CLK_CAN_FD_FREQ   (80U)

Clock source frequency CAN FD

◆ CanConf_CanController_CanController_0

#define CanConf_CanController_CanController_0   (0U)

◆ CanConf_CanController_CanController_1

#define CanConf_CanController_CanController_1   (1U)

◆ CanConf_CanController_CanController_2

#define CanConf_CanController_CanController_2   (2U)

◆ CAN_CONTROLLER_MCU_MCAN0

#define CAN_CONTROLLER_MCU_MCAN0

MCU_MCAN0 CONTROLLER INSTANCE

◆ CAN_CONTROLLER_MCU_MCAN1

#define CAN_CONTROLLER_MCU_MCAN1

MCU_MCAN1 CONTROLLER INSTANCE

◆ CAN_CONTROLLER_MCAN0

#define CAN_CONTROLLER_MCAN0

MCAN0 CONTROLLER INSTANCE

◆ CanConf_CanHardwareObject_CanHardwareObject_0

#define CanConf_CanHardwareObject_CanHardwareObject_0   (0U)

◆ CAN_HTRH_0

◆ CanConf_CanHardwareObject_CanHardwareObject_1

#define CanConf_CanHardwareObject_CanHardwareObject_1   (1U)

◆ CAN_HTRH_1

◆ CanConf_CanHardwareObject_CanHardwareObject_2

#define CanConf_CanHardwareObject_CanHardwareObject_2   (2U)

◆ CAN_HTRH_2

◆ CanConf_CanHardwareObject_CanHardwareObject_3

#define CanConf_CanHardwareObject_CanHardwareObject_3   (3U)

◆ CAN_HTRH_3

◆ CanConf_CanHardwareObject_CanHardwareObject_4

#define CanConf_CanHardwareObject_CanHardwareObject_4   (4U)

◆ CAN_HTRH_4

◆ CanConf_CanHardwareObject_CanHardwareObject_5

#define CanConf_CanHardwareObject_CanHardwareObject_5   (5U)

◆ CAN_HTRH_5

◆ CanConf_CanHardwareObject_CanHardwareObject_6

#define CanConf_CanHardwareObject_CanHardwareObject_6   (6U)

◆ CAN_HTRH_6

◆ CanConf_CanHardwareObject_CanHardwareObject_7

#define CanConf_CanHardwareObject_CanHardwareObject_7   (7U)

◆ CAN_HTRH_7

◆ CanConf_CanHardwareObject_CanHardwareObject_8

#define CanConf_CanHardwareObject_CanHardwareObject_8   (8U)

◆ CAN_HTRH_8

◆ CAN_OS_COUNTER_ID

#define CAN_OS_COUNTER_ID   ((CounterType)OsCounter_0)

Counter ID for counter used to count wait ticks.

◆ CAN_TIMEOUT_DURATION

#define CAN_TIMEOUT_DURATION   (10000U)

CAN timeout - used in CAN IFCMD busy wait and Start/Stop busy wait. Specifies the maximum time for blocking function until a timeout is detected. Unit is milli seconds.

◆ DemConf_DemEventParameter_CAN_DEM_NO_EVENT

#define DemConf_DemEventParameter_CAN_DEM_NO_EVENT   (0xFFFFU)

◆ CAN_DEM_NO_EVENT

#define CAN_DEM_NO_EVENT   DemConf_DemEventParameter_CAN_DEM_NO_EVENT

◆ CAN_E_HARDWARE_ERROR

#define CAN_E_HARDWARE_ERROR   (DemConf_DemEventParameter_CAN_E_HARDWARE_ERROR)

Hardware failed.

Typedef Documentation

◆ CanControllerState_Type

typedef uint8 CanControllerState_Type

Can Controller State enum type.

◆ Can_InterruptMask_Type

typedef uint32 Can_InterruptMask_Type

Can Interrupt Mask type.

Enumeration Type Documentation

◆ Can_MailBoxDirectionType

Can Mailbox direction enum.

Enumerator
CAN_MAILBOX_DIRECTION_RX 

Mailbox is for receive

CAN_MAILBOX_DIRECTION_TX 

Mailbox is for transmit

◆ Can_HandleType

Can Handle Type enum.

Enumerator
CAN_FULL 

For only one L-PDU (identifier) is handled by the hardware object

CAN_BASIC 

For several L-PDUs are handled by the hardware object

◆ Can_TxRxProcessingType

Can Tx/Rx processing enum.

Enumerator
CAN_TX_RX_PROCESSING_INTERRUPT 

Interrupt Mode of operation

CAN_TX_RX_PROCESSING_MIXED 

Mixed Mode of operation

CAN_TX_RX_PROCESSING_POLLING 

Polling Mode of operation

◆ Can_IrqStatusType

CAN IRQ status enum.

Enumerator
CAN_IRQ_NO_INTR_EVENT 

No Interrupt Event occured

CAN_IRQ_INTR_STUFF_EVENT 

Stuff Error Event occured

CAN_IRQ_INTR_FORM_EVENT 

Form Error Event occured

CAN_IRQ_INTR_ACK_EVENT 

Acknowldgement Error Event occured

CAN_IRQ_INTR_BIT1_EVENT 

Bit-1 Error Event occured

CAN_IRQ_INTR_BIT0_EVENT 

Bit-0 Error Event occured

CAN_IRQ_INTR_CRC_EVENT 

Cyclic Redundancy Error Event occured

CAN_IRQ_INTR_TOO_EVENT 

Time Out Error Event occured

CAN_IRQ_STATUS_READ_FAIL 

Interrupt status reading fail

◆ Can_ControllerInstance

Can Controller Instances enum.

Enumerator
CAN_CONTROLLER_INSTANCE_MCU_MCAN0 

MCU MCAN0 Controller Instance

CAN_CONTROLLER_INSTANCE_MCU_MCAN1 

MCU MCAN1 Controller Instance

CAN_CONTROLLER_INSTANCE_MCAN0 

MCAN0 Controller Instance

Function Documentation

◆ Can_GetVersionInfo()

void Can_GetVersionInfo ( Std_VersionInfoType * VersionInfo)

Function returns the version information of this module.

* Service name    : Can_GetVersionInfo
* Syntax          : void Can_GetVersionInfo(Std_VersionInfoType* versioninfo)
* Mode            : User Mode (Non-Privileged Mode)
* Service ID[hex] : 0x07
* Sync/Async      : Synchronous
* Reentrancy      : Reentrant
* Parameters (in) : None
* Parameters (inout): None
* Parameters (out)  : versioninfo
*                     Pointer to where to store the version information of this
*                     module.
* Return value      : None
* Description       : This function returns the version information of this
*                     module
* 

◆ Can_Init()

void Can_Init ( const Can_ConfigType * CfgPtr)

This function initializes the module.

* Service name      : Can_Init
* Syntax            : void Can_Init(const Can_ConfigType* CfgPtr)
* Mode              : Supervisor Mode (Privileged Mode)
* Service ID[hex]   : 0x00
* Sync/Async        : Synchronous
* Reentrancy        : Non Reentrant
* Parameters (in)   : CfgPtr
*                     Pointer to driver configuration.
* Parameters (inout): None
* Parameters (out)  : None
* Return value      : None
* Description       : This function initializes the module.
* 

◆ Can_SetControllerMode()

Std_ReturnType Can_SetControllerMode ( uint8 Controller,
Can_ControllerStateType Transition )

This function performs software triggered state transitions of the CAN controller State machine.

* Service name: Can_SetControllerMode
* Syntax: Std_ReturnType Can_SetControllerMode(uint8 Controller,
*                     Can_ControllerStateType Transition)
* Mode              : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x03
* Sync/Async: Asynchronous
* Reentrancy: Non Reentrant
* Parameters (in): Controller
*                  - CAN controller for which the status shall be changed
*                   Transition
*                  - Transition value to request new CAN controller state
* Parameters (inout): None
* Parameters (out):   None
* Return value: Std_ReturnType
*               - E_OK: request accepted
*               - E_NOT_OK: request not accepted, a development error
*                     occurred
* Description:  This function performs software triggered state transitions of
*                     the CAN controller State machine.
* 

◆ Can_Write()

Std_ReturnType Can_Write ( Can_HwHandleType Hth,
const Can_PduType * PduInfo )

This function is called by CanIf to pass a CAN message to CanDrv for transmission.

* Service name: Can_Write
* Syntax      : Std_ReturnType Can_Write(Can_HwHandleType Hth, const
*                     Can_PduType* PduInfo)
* Mode              : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x06
* Sync/Async     : Synchronous
* Reentrancy     : Reentrant (thread-safe)
* Parameters (in): Hth
*                  - Information which HW-transmit handle shall be used for
*                    transmit. Implicitly this is also the information about
*                    the controller to use because the Hth numbers are unique
*                    inside one hardware unit.
*                  PduInfo
*                  - Pointer to SDU user memory, DLC and Identifier.
* Parameters (inout): None
* Parameters (out)  : None
* Return value: Std_ReturnType
*               - E_OK: Write command has been accepted
*               - E_NOT_OK: development error occurred
*               - CAN_BUSY: No TX hardware buffer available or pre-emptive call
*                      of Can_Write that can't be implemented re-entrant
* Description: This function is called by CanIf to pass a CAN message to CanDrv
*                     for transmission.
* 

◆ Can_DisableControllerInterrupts()

void Can_DisableControllerInterrupts ( uint8 Controller)

This function disables all interrupts for this CAN controller.

* Service name      : Can_DisableControllerInterrupts
* Syntax            : void Can_DisableControllerInterrupts(uint8 Controller)
* Mode              : Supervisor Mode (Privileged Mode)
* Service ID[hex]   : 0x04
* Sync/Async        : Synchronous
* Reentrancy        : Reentrant
* Parameters (in)   : Controller
*                     - CAN controller for which interrupts shall be disabled.
* Parameters (inout): None
* Parameters (out)  : None
* Return value      : None
* Description       : This function disables all interrupts for this CAN
*                     controller
*
* 

◆ Can_EnableControllerInterrupts()

void Can_EnableControllerInterrupts ( uint8 Controller)

This function enables all allowed interrupts.

* Service name      : Can_EnableControllerInterrupts
* Syntax            : void Can_EnableControllerInterrupts(uint8 Controller)
* Mode              : Supervisor Mode (Privileged Mode)
* Service ID[hex]   : 0x05
* Sync/Async        : Synchronous
* Reentrancy        : Reentrant
* Parameters (in)   : Controller
*                     - CAN controller for which interrupts shall be re-enabled.
* Parameters (inout): None
* Parameters (out)  : None
* Return value      : None
* Description       : This function enables all allowed interrupts
*
* 

◆ Can_MainFunction_Write()

void Can_MainFunction_Write ( void )

This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

* Service name   : Can_MainFunction_Write
* Syntax         : void Can_MainFunction_Write(void)
* Mode           : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x01
* Description    : This function performs the polling of TX confirmation when
*                     CAN_TX_PROCESSING is set to POLLING.
*
* 

◆ Can_MainFunction_BusOff()

void Can_MainFunction_BusOff ( void )

This function performs the polling of bus-off events that are configured statically as 'to be polled'.

* Service name   : Can_MainFunction_BusOff
* Syntax         : void Can_MainFunction_BusOff(void)
* Mode           : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x09
* Description    : This function performs the polling of bus-off events that are
*                     configured statically as 'to be polled'.
*
* 

◆ Can_MainFunction_Read()

void Can_MainFunction_Read ( void )

This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

* Service name   : Can_MainFunction_Read
* Syntax         : void Can_MainFunction_Read(void)
* Mode           : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x08
* Description    : This function performs the polling of RX indications when
*                     CAN_RX_PROCESSING is set to POLLING.
*
* 

◆ Can_MainFunction_Wakeup()

void Can_MainFunction_Wakeup ( void )

This function performs the polling of wake-up events that are configured statically as 'to be polled'.

* Service name   : Can_MainFunction_Wakeup
* Syntax         : void Can_MainFunction_Wakeup(void)
* Mode           : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x0A
* Description    : This function performs the polling of wake-up events that are
*                     configured statically as 'to be polled'.
*
* 

◆ Can_MainFunction_Mode()

void Can_MainFunction_Mode ( void )

This function performs the polling of CAN controller mode transitions.

* Service name   : Can_MainFunction_Mode
* Syntax         : void Can_MainFunction_Mode(void)
* Mode           : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x0C
* Description    : This function performs the polling of CAN controller mode
*                     transitions.
*
* 

◆ Can_SetBaudrate()

Std_ReturnType Can_SetBaudrate ( uint8 Controller,
uint16 BaudRateConfigID )

This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset.

*
*  Function name     : Can_SetBaudrate
*  Syntax            : FUNC(Std_ReturnType, CAN_CODE) Can_SetBaudrate(uint8
*                           Controller, uint16 BaudRateConfigID)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : 0x0f
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant for different Controllers.
*                      Non reentrant for the same Controller.
*  Parameters (in)   : None
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : None
*  Description       : This service shall set the baud rate configuration
*                      of the CAN controller. Depending on necessary baud rate
*                      modifications the controller might have to reset.
*
* 

◆ Can_TestLoopBackModeEnable()

Std_ReturnType Can_TestLoopBackModeEnable ( uint8 Controller,
uint8 Mode )

This service will enable CAN loopback mode.

*
*  Service name      : Can_TestLoopBackModeEnable
*  Syntax            : Std_ReturnType Can_TestLoopBackModeEnable(uint8
*                      Controller, uint8 mode)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - CAN Controller to enable loopback mode
*                      mode
*                      - Loopback mode
*                      -# 0 - Digital Loopback
*                      -# 1 - Analog  Loopback
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : Std_ReturnType
*                      - E_OK: Baudrate supported by the CAN Controller
*                      - E_NOT_OK: Baudrate not supported / invalid CAN
*  Description       : This service will enable CAN loopback mode.
* 

◆ Can_TestLoopBackModeDisable()

Std_ReturnType Can_TestLoopBackModeDisable ( uint8 Controller,
uint8 Mode )

This service will disable CAN loopback mode.

*
*  Service name      : Can_TestLoopBackModeDisable
*  Syntax            : Std_ReturnType Can_TestLoopBackModeDisable(uint8
*                      Controller, uint8 Mode)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - CAN Controller to enable loopback mode
*                      mode
*                      Loopback mode
*                      -# 0 - Digital Loopback
*                      -# 1 - Analog  Loopback
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : Std_ReturnType
*                      - E_OK: Loopback mode enabled in the CAN Controller
*                      - E_NOT_OK: Loopback mode enable failed
*  Description       : This service will disable CAN loopback mode.
* 

◆ Can_RegisterReadback()

Std_ReturnType Can_RegisterReadback ( VAR(uint8,) Controller,
Can_RegisterReadbackType * RegRbPtr )

This service will readback CAN registers.

*
*  Service name      : Can_RegisterReadback
*  Syntax            : Std_ReturnType Can_RegisterReadback(uint8 Controller)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - CAN Controller to readback registers configuration.
*  Parameters (inout): RegRbPtr - Pointer to where to store the readback
*                      values. If this pointer is NULL_PTR, then the API
*                      will return E_NOT_OK.
*  Parameters (out)  : None
*  Return value      : Std_ReturnType
*                      - E_OK: Register readback successful.
*                      - E_NOT_OK: Register readback failed.
*  Description       : This service will readback CAN registers.
* 

◆ Can_EnableIntr()

Std_ReturnType Can_EnableIntr ( VAR(uint8,) Controller,
VAR(uint8,) CanErrVar )

This service will Enable the interrupts.

*
*  Service name      : Can_EnableIntr
*  Syntax            : Std_ReturnType Can_EnableIntr(
*                        VAR(uint8, AUTOMATIC)Controller,
*                        VAR(uint8, AUTOMATIC)CanErrVar);
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - Controller for which interrupt errors has
*                        to be enabled.
*                      - CanErrVar - CAN Error Type.
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : Std_ReturnType
*                      - E_OK: Enabling Interrupts is success.
*                      - E_NOT_OK: Enabling Interrupts failed.
*  Description       : This service will Enable the interrupts.
* 

◆ Can_DisableIntr()

Std_ReturnType Can_DisableIntr ( VAR(uint8,) Controller,
VAR(uint8,) CanErrVar )

This service will Disable the Interrupts.

*
*  Service name      : Can_DisableIntr
*  Syntax            : Std_ReturnType Can_DisableIntr(
*                        VAR(uint8, AUTOMATIC)Controller,
*                        VAR(uint8, AUTOMATIC)CanErrVar)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - Controller for which interrupt errors has to
*                        be Disabled.
*                      - CanErrVar - CAN Error Type.
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : Std_ReturnType
*                      - E_OK: Disabling Interrupts is success.
*                      - E_NOT_OK: Disabling Interrupts failed.
*  Description       : This service will Disable the Interrupts.
* 

◆ Can_GetIntrStatus()

Can_IrqStatusType Can_GetIntrStatus ( VAR(uint8,) Controller)

This service will provide the status of the interrupt.

*
*  Service name      : Can_GetIntrStatus
*  Syntax            : Can_IrqStatusType Can_GetIntrStatus(
*                        VAR(uint8, AUTOMATIC)Controller)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - Controller for which it reads the interrupt error
*                        status.
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : Can_IrqStatusType
*                      - CAN_IRQ_NO_INTR_EVENT: No Interrupt Event occured.
*                      - CAN_IRQ_INTR_STUFF_EVENT: STUFF Error Event occured.
*                      - CAN_IRQ_INTR_FORM_EVENT: FORM Error Event occured.
*                      - CAN_IRQ_INTR_ACK_EVENT: ACK Error Event occured.
*                      - CAN_IRQ_INTR_BIT1_EVENT: BIT1 Error Event occured.
*                      - CAN_IRQ_INTR_BIT0_EVENT: BIT0` Error Event occured.
*                      - CAN_IRQ_INTR_CRC_EVENT: CRC Error Event occured.
*                      - CAN_IRQ_INTR_TOO_EVENT: TOO  Error Event occured.
*                      - CAN_IRQ_STATUS_READ_FAIL: Interrupt status read fail.
*  Description       : This service will provide the status of the interrupt.
* 

◆ Can_ClearIntrStatus()

Std_ReturnType Can_ClearIntrStatus ( VAR(uint8,) Controller)

This service will clear the interrupt status.

*
*  Service name      : Can_ClearIntrStatus
*  Syntax            : Std_ReturnType Can_ClearIntrStatus(
*                        VAR(uint8, AUTOMATIC)Controller)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Reentrant
*  Parameters (in)   : Controller
*                      - Controller for which it clears the interrupt
*                        error status.
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : Std_ReturnType
*                      - E_OK: Clearing Interrupt Status is Success.
*                      - E_NOT_OK: Clearing Interrupt Status Failed.
*  Description       : This service will clear the interrupt status.
* 

◆ Can_IntISR_Fun()

void Can_IntISR_Fun ( Can_ControllerInstance CanInstanceID)

This function is the ISR for CAN controller 0/INT 0.

*
*  Function name     : Can_IntISR_Fun
*  Syntax            : void Can_IntISR_Fun(Can_ControllerInstance CanInstanceID)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Non-Reentrant
*  Parameters (in)   : None
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : None
*  Description       : This function is the ISR for CAN controller 0/INT 0 <br>
*                      This function should be invoked either by OS Interrupt
*                      frame handler <br>
*                      CAN Interrupt frame handler for Category 1 ISR
* 

◆ Can_IntISR_Function()

void Can_IntISR_Function ( Can_ControllerInstance CanInstanceID,
uint32 baseAddr )

This function is the ISR for CAN controller 0/INT 0.

*
*  Function name     : Can_IntISR_Fun
*  Syntax            : void Can_IntISR_Fun(Can_ControllerInstance CanInstanceID)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Service ID[hex]   : N/A
*  Sync/Async        : Synchronous
*  Reentrancy        : Non-Reentrant
*  Parameters (in)   : None
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : None
*  Description       : This function is the ISR for CAN controller 0/INT 0 <br>
*                      This function should be invoked either by OS Interrupt
*                      frame handler <br>
*                      CAN Interrupt frame handler for Category 1 ISR
* 

◆ Can_DeInit()

void Can_DeInit ( void )

This function de-initializes the module.

*  Service name      : Can_DeInit
*  Syntax            : void Can_DeInit(void)
*  Mode              : Supervisor Mode (Privileged Mode)
*  Sync/Async        : Synchronous
*  Reentrancy        : Non-Reentrant
*  Parameters (in)   : None
*  Parameters (inout): None
*  Parameters (out)  : None
*  Return value      : None
*  Description       : This function de-initializes the module.
*  

◆ Can_GetControllerMode()

Std_ReturnType Can_GetControllerMode ( uint8 Controller,
Can_ControllerStateType * ControllerModePtr )

This service reports about the current status of the requested CAN controller.

* Service name: Can_GetControllerMode
* Syntax: Std_ReturnType Can_GetControllerMode(uint8 Controller,
*                     Can_ControllerStateType* ControllerModePtr)
* Mode            : User Mode (Non-Privileged Mode)
* Service ID[hex]: 0x12
* Sync/Async: Synchronous
* Reentrancy: Non Reentrant
* Parameters (in): Controller
*                  - CAN controller for which the status shall be changed
* Parameters (out): ControllerModePtr
*                  - Pointer to a memory location,
*                    where the current mode of the CAN controller will be stored.
* Parameters (inout):  None
* Return value: Std_ReturnType
*               - E_OK: request accepted
*               - E_NOT_OK: request not accepted.
* Description:  This service reports about the current status of the requested
*               CAN controller.
* 

◆ Can_GetControllerErrorState()

Std_ReturnType Can_GetControllerErrorState ( uint8 ControllerId,
Can_ErrorStateType * ErrorStatePtr )

This service obtains the error state of the CAN controller.

* Service name: Can_GetControllerErrorState
* Syntax: Std_ReturnType Can_GetControllerErrorState(uint8 Controller,
*                     Can_ErrorStateType* ErrorStatePtr)
* Mode           : Supervisor Mode (Privileged Mode)
* Service ID[hex]: 0x11
* Sync/Async: Synchronous
* Reentrancy: Non Reentrant
* Parameters (in): Controller
*                  - CAN controller for which the status shall be changed
* Parameters (out): ErrorStatePtr
*                  - Pointer to a memory location,
*                    where the error state of the CAN controller will be stored.
* Parameters (inout):  None
* Return value: Std_ReturnType
*               - E_OK: request accepted
*               - E_NOT_OK: request not accepted
* Description:  This service obtains the error state of the CAN controller.
* 

◆ Can_0_Int0ISR()

void Can_0_Int0ISR ( void )

MCU_MCAN0 Controller Instance ISR.

◆ Can_1_Int0ISR()

void Can_1_Int0ISR ( void )

MCU_MCAN1 Controller Instance ISR.

◆ Can_2_Int0ISR()

void Can_2_Int0ISR ( void )

MCAN0 Controller Instance ISR.

Variable Documentation

◆ MaskValue

uint32 Can_MaskType::MaskValue

Filter mask value.

◆ IDValue

Can_IdType Can_HwFilterType::IDValue

ID value extended will have MSB set

◆ Mask

uint32 Can_HwFilterType::Mask

Mask for the RX filtering

◆ Baud [1/2]

uint16 Can_FdBaudConfigType::Baud

In Kbps

◆ PropSeg [1/2]

uint8 Can_FdBaudConfigType::PropSeg

Prop Segement value

◆ Pseg1 [1/2]

uint8 Can_FdBaudConfigType::Pseg1

Phase Segment 1

◆ Pseg2 [1/2]

uint8 Can_FdBaudConfigType::Pseg2

Phase Segment 2

◆ Sjw [1/2]

uint8 Can_FdBaudConfigType::Sjw

Sync jump width

◆ TimingValues [1/2]

uint16 Can_FdBaudConfigType::TimingValues

Sum of all timing parameters *

◆ BrpValue [1/2]

uint16 Can_FdBaudConfigType::BrpValue

Controller BRP value for Baud

◆ TrcvCompDelay

uint16 Can_FdBaudConfigType::TrcvCompDelay

Specifies the Transceiver Delay Compensation Offset in ns

◆ BrsSwitch

boolean Can_FdBaudConfigType::BrsSwitch

Specifies if the bit rate switching shall be used for transmissions.

◆ Baud [2/2]

uint16 Can_BaudConfigType::Baud

In Kbps

◆ PropSeg [2/2]

uint8 Can_BaudConfigType::PropSeg

Prop Segement value

◆ Pseg1 [2/2]

uint8 Can_BaudConfigType::Pseg1

Phase Segment 1

◆ Pseg2 [2/2]

uint8 Can_BaudConfigType::Pseg2

Phase Segment 2

◆ Sjw [2/2]

uint8 Can_BaudConfigType::Sjw

Sync jump width

◆ TimingValues [2/2]

uint16 Can_BaudConfigType::TimingValues

Sum of all timing parameters

◆ BrpValue [2/2]

uint16 Can_BaudConfigType::BrpValue

Controller BRP value for Baud

◆ BaudFdRateConfig

Can_FdBaudConfigType Can_BaudConfigType::BaudFdRateConfig

List of available Data phase Baud rates for CAN FD

◆ DefaultBaud

Can_BaudConfigType* Can_ControllerType::DefaultBaud

pointer to default Baud structure

◆ BaudRateConfigList

Can_BaudConfigType** Can_ControllerType::BaudRateConfigList

List of available Baud rates

◆ ControllerId

uint8 Can_ControllerType_PC::ControllerId

Id as provided by GUI

◆ CntrActive

boolean Can_ControllerType_PC::CntrActive

Contoller is used=1 or not_used=0

◆ CntrAddr

uint32 Can_ControllerType_PC::CntrAddr

Pointer to CanReg structure

◆ RxProcessingType

Can_TxRxProcessingType Can_ControllerType_PC::RxProcessingType

Type can be Interrupt, Polling or Mixed

◆ TxProcessingType

Can_TxRxProcessingType Can_ControllerType_PC::TxProcessingType

Type can be Interrupt, Polling or Mixed

◆ BusOffProcessingInterrupt

boolean Can_ControllerType_PC::BusOffProcessingInterrupt

TRUE = Interrupt FALSE = Polling

◆ CanControllerInst

Can_ControllerInstance Can_ControllerType_PC::CanControllerInst

Can Controller Instance

◆ CanFDModeEnabled

boolean Can_ControllerType_PC::CanFDModeEnabled

Controller is in CAN FD Mode or not

◆ CanHandleType

uint8 Can_MailboxType::CanHandleType

CanHandleType 0=Full, *1=Basic

◆ MBIdType

uint32 Can_MailboxType::MBIdType

CanIdType 0=standard 1=Extended 2= Mixed

◆ HwHandle

Can_HwHandleType Can_MailboxType::HwHandle

Mailbox - Hw object in the controller

◆ CanHwObjectCount

uint32 Can_MailboxType::CanHwObjectCount

Number of hardware objects used to implement one HOH

◆ MBDir

Can_MailBoxDirectionType Can_MailboxType::MBDir

CanObjectType - Direction of Mailbox

See also
Can_MailBoxDirectionType

◆ Controller

const Can_ControllerType_PC* Can_MailboxType::Controller

Reference to CAN Controller to which the HOH is associated to.

◆ HwFilterList

Can_HwFilterType** Can_MailboxType::HwFilterList

List of HW Filter

◆ HwFilterCnt

uint32 Can_MailboxType::HwFilterCnt

HW Filter Count

◆ CanFdPaddingValue

uint8 Can_MailboxType::CanFdPaddingValue

If PduInfo->SduLength does not match possible DLC values CanDrv will use the next higher valid DLC for transmission with initialization of unused bytes to the value of the corresponding CanFdPaddingValue.

◆ CanHardwareObjectUsesPolling

boolean Can_MailboxType::CanHardwareObjectUsesPolling

TRUE = Polling, FALSE = Interrupt

◆ CanObjectId

uint16 Can_MailboxType_PC::CanObjectId

CanObjectId - Holds handle Id

◆ Reserved

uint32 Can_DmaPrms::Reserved

Reserved for Future use, currently unused parameter

◆ CanControllerList

Can_ControllerType** Can_ConfigType::CanControllerList

List of enabled Controllers

◆ CanMaxControllerCount

uint8 Can_ConfigType::CanMaxControllerCount

MaxCount of Controller in Controller List

◆ MailBoxList

Can_MailboxType** Can_ConfigType::MailBoxList

MB array for all controllers

◆ MaxMbCnt

uint32 Can_ConfigType::MaxMbCnt

MaxMbCount in MB list in all controller

◆ MaxBaudConfigID

uint32 Can_ConfigType::MaxBaudConfigID[CAN_MAX_CONTROLLER]

Max Baud Config Index in BaudRateConfigList in all controller

◆ DmaPrms

Can_DmaPrms* Can_ConfigType::DmaPrms

Reserved for Future use, currently unused parameter

◆ CanReadBackRegPID

uint32 Can_RegisterReadbackType::CanReadBackRegPID

MCANSS PID Register

◆ CanReadBackRegSTAT

uint32 Can_RegisterReadbackType::CanReadBackRegSTAT

MCANSS STAT Register

◆ CanReadBackRegCREL

uint32 Can_RegisterReadbackType::CanReadBackRegCREL

Auto Bus On Time Register

◆ CanReadBackRegENDN

uint32 Can_RegisterReadbackType::CanReadBackRegENDN

Endianess MCAN_TEST value Constant "0x8765 4321"

◆ CanReadBackRegCTRL

uint32 Can_RegisterReadbackType::CanReadBackRegCTRL

MCAN CTRL Register

◆ CanReadBackRegDBTP

uint32 Can_RegisterReadbackType::CanReadBackRegDBTP

MCAN DBTB Register

◆ CanReadBackRegRWD

uint32 Can_RegisterReadbackType::CanReadBackRegRWD

MCAN RWD Register

◆ CanReadBackRegCCCR

uint32 Can_RegisterReadbackType::CanReadBackRegCCCR

MCAN CCCR Register

◆ CanReadBackRegNBTP

uint32 Can_RegisterReadbackType::CanReadBackRegNBTP

MCAN NBTP Register

◆ CanReadBackRegTDCR

uint32 Can_RegisterReadbackType::CanReadBackRegTDCR

MCAN TDCR Register

◆ CanReadBackRegGFC

uint32 Can_RegisterReadbackType::CanReadBackRegGFC

MCAN GFC Register

◆ CanReadBackRegSIDFC

uint32 Can_RegisterReadbackType::CanReadBackRegSIDFC

MCAN SIDFC Register

◆ CanReadBackRegXIDFC

uint32 Can_RegisterReadbackType::CanReadBackRegXIDFC

MCAN XIDFC Register

◆ CanReadBackRegRXF0C

uint32 Can_RegisterReadbackType::CanReadBackRegRXF0C

MCAN RXF0C Register

◆ CanReadBackRegRXBC

uint32 Can_RegisterReadbackType::CanReadBackRegRXBC

MCAN RXBC Register

◆ CanReadBackRegRXF1C

uint32 Can_RegisterReadbackType::CanReadBackRegRXF1C

MCAN RXF1C Register

◆ CanReadBackRegTXBC

uint32 Can_RegisterReadbackType::CanReadBackRegTXBC

MCAN TXBC Register

◆ CanReadBackRegTXESC

uint32 Can_RegisterReadbackType::CanReadBackRegTXESC

MCAN TXESC Register

◆ CanReadBackRegTXEFC

uint32 Can_RegisterReadbackType::CanReadBackRegTXEFC

MCAN TXEFC Register

◆ CanConfigSet

const struct Can_ConfigType_s CanConfigSet
extern

CAN Configuration struct declaration.

◆ CanConfigSet_PC_CanController_0

const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_0
extern

CAN Controller Configuration Pre Compile struct declaration.

◆ CanConfigSet_PC_CanController_1

const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_1
extern

CAN Controller Configuration Pre Compile struct declaration.

◆ CanConfigSet_PC_CanController_2

const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_2
extern

CAN Controller Configuration Pre Compile struct declaration.

◆ CanConfigSet_CanController_List_PC

const struct Can_ControllerStruct_PC* CanConfigSet_CanController_List_PC[CAN_NUM_CONTROLLER]
extern

CAN Controller Pre Compile Configuration List.

◆ CanConfigSet_CanHardwareObject_List_PC

const struct Can_MailboxStruct_PC* CanConfigSet_CanHardwareObject_List_PC[CAN_NUM_MAILBOXES]
extern

CAN Mailbox Pre Compile Configuration List.

◆ Can_MsgmemRAMBaseAddr

const uint32 Can_MsgmemRAMBaseAddr[CAN_MAX_CONTROLLER]
extern

Base Address of the can peripherals.

◆ Can_MCANSSBaseAddr

const uint32 Can_MCANSSBaseAddr[CAN_MAX_CONTROLLER]
extern

◆ Can_MCANCoreRegBaseAddr

const uint32 Can_MCANCoreRegBaseAddr[CAN_MAX_CONTROLLER]
extern

◆ Can_MCANECCAggrRegBaseAddr

const uint32 Can_MCANECCAggrRegBaseAddr[CAN_MAX_CONTROLLER]
extern