4.12. GPT¶
4.12.1. About This Document¶
Document Title |
User Guide of MCAL GPT Driver |
Document Version |
Version 1.5 |
Company |
Texas Instruments |
Document Name |
GPT User Guide |
4.12.2. Revision History¶
Version |
Date |
Revision History |
Status |
|---|---|---|---|
Version 1.0 |
26 April 2022 |
Initial Release |
Approved |
Version 1.1 |
05 Aug 2022 |
Updated AM263 to AM263x |
Approved |
Version 1.2 |
23 Dec 2022 |
GPT Example application testing procedure is added |
Approved |
Version 1.3 |
8 May 2023 |
GPT Example application testing procedure updated |
Approved |
Version 1.4 |
12 Jun 2023 |
Updated as per HTML format. |
Approved |
Version 1.5 |
25 Aug 2023 |
Document release version column removed |
Approved |
4.12.3. Table of contents¶
4.12.4. Acronyms and Definitions¶
Acronyms and Definitions Used are presented in below table.
Acronyms |
Descriptions |
|---|---|
BSW |
Basic Software |
DET |
Default Error Tracer |
GPT |
General Purpose Timer |
MCU |
Micro Controller Unit |
OS |
Operating System |
Definitions |
Descriptions |
|---|---|
Timer channel |
Represents a logical timer entity assigned to a timer hardware |
Target Time |
Something as per requirement occurs once this time value reached. |
Ticks |
Defines the timer resolution, the duration of a timer increment |
4.12.5. Functional Overview¶
4.12.5.1. Brief Overview¶
This document describes the functionality, API and configuration of the AUTOSAR BSW module GPT.
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Pre-Compile, Post-build |
Vendor ID |
GPT_VENDOR_ID (44) |
Module ID |
GPT_MODULE_ID (100) |
Supported Platform |
AM263x |
The GPT module initializes and controls the internal General Purpose Timer(s) (GPT) of the microcontroller. The GPT driver provides services and configuration parameters for
Starting and stopping hardware timers
Getting timer values
Controlling time triggered interrupt notifications
Note that the conversion between timer ticks provided by GPT and actual time value is not done by GPT. User software must take care of it. The tick duration of a timer channel depends on channel specific settings (part of GPT driver) as well as on system clock and settings of the clock tree controlled by the MCU module. The brief overview on GPT module is given below:
4.12.5.1.1. GPT Driver Architecture¶
The following figure shows where the GPT is in the AUTOSAR architecture.
fig1: GPT in AUTOSAR architecture.
4.12.5.1.2. Initialization¶
The driver GPT is initialized by calling Gpt_Init(), with parameter ConfigPtr referencing a runtime configuration set. After de-initializing the module, that is calling Gpt_DeInit(), it can be initialized again.
4.12.5.1.3. States¶
Each GPT channel has up to five different states, depending on its configuration and running state as described below
GPT_UNINITIALIZED: GPT channel is not initialized and not counting.
GPT_INITIALIZED: GPT channel is initialized with Gpt_Init() and not counting.
GPT_RUNNING: GPT channel is initialized and running (counting).
GPT_STOPPED: GPT channel is initialized but not counting (stopped).
GPT_EXPIRED: GPT channel is expired (timer overflowed). This state will be applicable in timer one shot mode where after encountering overflow timer stops.
The figure below taken from the AUTOSAR specification shows the state transitions for different function calls and events:
fig2: GPT channel states and state transitions
4.12.5.1.4. GPT channel modes¶
The GPT channel can be configured in “one-shot mode” or in “continuous mode”.
One-shot mode: In one-shot mode timer stops counting after overflow (when timer value matches to target value set by Gpt_StartTimer).
Continuous mode: In continuous mode if the timer has reached the target time (timer value = target time), the timer will continue running with the value “0” at next timer tick.
GPT channel mode can be selected through configuration structure Gpt_ConfigType.
4.12.5.1.5. GPT operating modes¶
The GPT channels can be configured in normal mode. In this mode, GPT channel will be initialized with Gpt_Init(). In this mode, interrupt notifications will be allowed if enabled through configuration.
fig3: GPT driver modes
4.12.5.1.6. GPT starting/stopping channel counting and reading count¶
The GPT channel starts counting after calling Gpt_Init() . The count value (target time in ticks) is passed to Gpt_StartTimer() function. GPT channel will start counting till target time is reached. Depending on channel mode it will stop (one-shot mode) or roll over (continuous mode) after target time is reached. GPT channel can be explicitly stopped by calling function Gpt_StopTimer(). This will stop channel from counting and disable all its interrupts notifications.
To read channel count when channel is running functions Gpt_GetTimeElapsed() and Gpt_GetTimeRemaining() can be used. As name suggests these give time elapsed after starting timer and time remaining to reach target time respectively. Below snapshot from GPT MCAL spec shows working of these two functions.
Please note that general-purpose timers doesn’t keep track on amount of time that has overflowed by above two functions and the time overflow is always considered absolute and not relative.
fig4: Time Elapsed and Time remaining for a timer channel
4.12.5.1.7. GPT interrupt notifications¶
GPT driver supports enabling and disabling interrupt notifications for GPT channels through Gpt_EnableNotification() and Gpt_DisableNotification() functions. For getting notification from channel, a pointer to notification function should be passed through configuration structure during initialization. In case notification function not available Gpt_EnableNotification() will return an error. Also, it is important to note that interrupt notifications are only enabled when device is in normal mode. In sleep mode interrupt notifications are disabled if they are not wakeup capable (and not enabled for wakeup).
Once interrupt notifications are enabled GPT channel after counting till target time will generate interrupt and channel ISR will be called. This ISR will determine whether to call notification function or wakeup function depending on which one is enabled beforehand. It is responsibility of user software to register these ISR with MCU before starting channel.
4.12.5.2. Supported and Not Supported Features¶
IP Supported Features |
AUTOSAR Supported Features |
Not Supported Features |
|---|---|---|
Free running 32 bit up counter |
Initialization and de-initialization of all GPT channels. |
Predefined timers are not supported. |
Auto reload mode (can be used for continuous counter operation) |
Starting and stopping of counting for individual channels. |
Sleep and wakeup is not supported. |
Support dynamic Start / Stop counter operation |
Getting elapsed and remaining counter value |
|
Programmable clock dividers (2n, where n = [0-8]) |
Enabling/disabling counter triggered interrupt notifications. |
|
2 timers modules could be operated in cascaded mode to provide 64bit counter |
One shot and continuous mode. |
|
Programmable interrupt generation on overflow, compare and capture |
||
Programmable clock source |
||
Supports 3 basic functional modes Timer mode, Capture mode & Compare mode |
4.12.5.3. Assumptions¶
None
4.12.5.4. Limitations¶
None
4.12.5.5. Design overview (Link to the Architecture document and Design Document)¶
Will be updated in future release
4.12.5.6. File Structure¶
Description of static files is provided below:
Static source and header files |
Description |
|---|---|
Gpt.h |
Contains the API’s of the GPT driver to be used by upper layers |
Gpt_Priv.h |
Contains data structures and Internal function declarations |
Gpt_Irq.h |
Contains ISR function declaration |
Gpt.c |
Implementation of the API’s for GPT driver |
Gpt_Priv.c |
Contains Internal Functions Definitions |
Gpt_Irq.c |
Contains ISR function definitions |
Description of generated files is provided below:
Plugin Files |
Descriptions |
|---|---|
Gpt_Cfg.h |
Contains the base addresses, Precompile switches, Macros for channels, counters etc. |
Gpt_PBcfg.c |
Contains all channels Post-Build Configuration parameters |
Gpt_Cfg.c |
Contains all channels Pre-Compile Configuration parameters |
The below diagram shows the files structure for the GPT driver.
fig5 :GPT header file include structure
4.12.6. Deviations to requirements (Requirement Traceability)¶
4.12.6.1. Module Requirements¶
Will be updated in future release
4.12.6.2. Deviation of requirements against AUTOSAR specification requirements¶
Will be updated in future release
4.12.7. Integration Details¶
4.12.7.1. Dependency on Other Software Modules¶
4.12.7.1.1. MCU¶
The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL as well as the internal clock domains which is connected to the GPT unit. The GPT module also supports an internal divider which can be changed at configuration time using the ‘prescale’ member of Gpt_ChannelConfigType structure to configure the actual GPT functional clock.
Note that Module GPT will not take care of settings which configure the clock and PLL for channels in its init function. This must be done by the MCU module.
4.12.7.1.2. Port¶
The GPT module does not require any PORT configuration. Hence there is no dependency on PORT module.
4.12.7.1.3. OS¶
An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table.The GPT module may use AUTOSAR OS to suspend and restore global interrupts.
4.12.7.1.4. Error Handling module¶
4.12.7.1.4.1. DET¶
The module GPT depends on the DET (by default) to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch “Enable Development Error Detection” on the tab “General Settings” within the module GPT. The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.
AUTOSAR requires that API functions shall check the validity of their respective parameters. These checks are for development error reporting and can be enabled or disabled.
Type of Error |
Relevance |
Related Error Code |
Value |
|---|---|---|---|
API service called without module initialization |
Development |
GPT_E_UNINIT |
0x0A |
API service is called when timer channel is still busy |
Development |
GPT_E_BUSY |
0x0B |
API service for initialization is called when already initialized |
Development |
GPT_E_ALREADY_INITIALIZED |
0x0D |
API parameter checking: invalid channel |
Development |
GPT_E_PARAM_CHANNEL |
0x14 |
API parameter checking: invalid value |
Development |
GPT_E_PARAM_VALUE |
0x15 |
API parameter checking: invalid pointer |
Development |
GPT_E_PARAM_POINTER |
0x16 |
API parameter checking: invalid mode |
Development |
GPT_E_PARAM_MODE |
0x1F |
4.12.7.1.4.2. Runtime Errors¶
Type of Error |
Relevance |
Related Error Code |
Value |
|---|---|---|---|
API service called when timer channel is still busy (running) |
Development |
GPT_E_BUSY |
0x0B |
API service called when driver is in wrong mode |
Development |
GPT_E_MODE |
0x0C |
4.12.7.1.4.3. DEM¶
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus().
The errors reported to DEM are described in the following table:
Error Code |
Description |
|
|---|---|---|
Assigned by DEM |
GPT_E_HARDWARE_ERROR |
This error is raised when issued when GPT Timer register reset fails. |
4.12.7.1.5. Callback Notification¶
This section describes notification functions which are passed to GPT driver as a target function. The target function is usually a call-back function. The names of these functions are not fixed and can be changed. At its configurable interfaces the GPT defines notifications that can be mapped to callback functions to respective channels. Function pointer to callback function (for non-wakeup notification) should be defined in Gpt.h with Gpt_NotifyType datatype. There should be separate notification call back function for each timer channel which is configured as Gpt_Channel_Notify<channelnumber>. Example: Gpt_Channel_Notify5 for channel 5
4.12.7.2. Hardware - Software - API name mapping¶
For interrupt notification and wakeup, ISR are provided in GPT driver. There is one ISR for each timer channel. Depending on mode of timer it will call notify function. The interrupt service routines shall be mapped to the interrupt sources of the respective GPT unit interrupt. The supported ISR’s are part of the Gpt_Irq.h file.
Following are timer modules with its respective ISRs for each channel in AM263x:
Timer |
ISR |
|---|---|
RTI0 |
Gpt_Ch0Isr() |
RTI0 |
Gpt_Ch1Isr() |
RTI0 |
Gpt_Ch2Isr() |
RTI0 |
Gpt_Ch3Isr() |
RTI1 |
Gpt_Ch4Isr() |
RTI1 |
Gpt_Ch5Isr() |
RTI1 |
Gpt_Ch6Isr() |
RTI1 |
Gpt_Ch7Isr() |
RTI2 |
Gpt_Ch8Isr() |
RTI2 |
Gpt_Ch9Isr() |
RTI2 |
Gpt_Ch10Isr() |
RTI2 |
Gpt_Ch11Isr() |
RTI3 |
Gpt_Ch12Isr() |
RTI3 |
Gpt_Ch13Isr() |
RTI3 |
Gpt_Ch14Isr() |
RTI3 |
Gpt_Ch15Isr() |
4.12.7.3. Scheduling Strategy¶
4.12.7.3.1. SchM¶
Beside the OS the BSW Scheduler provides functions that module GPT calls at begin and end of critical sections.
4.12.7.3.2. Critical Sections¶
There is only one kind of critical sections in this driver. Within these sections all read /modify/write accesses to internal GPT status variables must be protected. Therefore, switching to tasks that also access GPT must be avoided and all GPT interrupts must be suspended.
4.12.8. API Description¶
4.12.8.1. Description of the API’s(Can be referred to Api Guide spec)¶
Refer the AUTOSAR SWS for API documentation and Type definition.
4.12.8.2. API’s with Service ID¶
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Gpt_GetVersionInfo |
0x01 |
Gpt_Init |
0x02 |
Gpt_DeInit |
0x03 |
Gpt_GetTimeElapsed |
0x04 |
Gpt_GetTimeRemaining |
0x05 |
Gpt_StartTimer |
0x06 |
Gpt_StopTimer |
0x07 |
Gpt_EnableNotification |
0x08 |
Gpt_DisableNotification |
4.12.8.3. Description on Non Standard API’s¶
Gpt_RegisterReadback API–This function is non-autosar based and is used to read the data in the registers of GPT if we keep GPT_REGISTER_READBACK_API Macro as ON.
4.12.9. Configuration Description¶
4.12.9.1. Configuration Variants¶
The GPT can be configured as Post-Build or Pre-Compile variant, using EB tresos tool.
Variants |
Generated Files |
|---|---|
PostBuild |
Gpt_PBcfg.c , Gpt_Cfg.h |
Pre-Compile |
Gpt_Cfg.c , Gpt_Cfg.h |
4.12.9.2. Parameter Description¶
4.12.9.2.1. Standard Configuration¶
Will be updated in future release
4.12.9.2.2. IP Specific Configuration¶
GptCounterBlkId |
This is the Counter block ID for the RTI modules. Each RTI module has 2 counter blocks that are defined in this configuration parameter. |
GptRegisterReadback |
Adds / removes the service Gpt_ConfigRegReadBack() function from the code. |
GptTypeofInterruptFunction |
To define type of ISR function. |
GptPrescaler |
Prescaler value is defined to get the desired frequency. |
GptModule<module_number>CounterBlk0Frequency |
Specifies the tick frequency of the timer channel of counter block0 in Hz. |
GptModule<module_number>CounterBlk1Frequency |
Specifies the tick frequency of the timer channel of counter block1 in Hz |
GptDefaultOSCounterId |
Defines default Os Counter Id if node reference to OsCounter ref GptOsCounterRef is set |
GptOsCounterRef |
This parameter contains a reference to the OsCounter, which is used by the GPT driver |
GptTimeoutDuration |
GPT timeout - used in GPT busy wait |
GptDeviceVariant |
To Select SOC AM263x variant |
4.12.9.3. Symbolic Names deviations¶
None.
4.12.9.4. Configuration rules and constraints to enable plausibility checks¶
Will be updated in future release
4.12.10. Memory Mapping¶
Memory Mapping Sections |
GPT_CODE |
GPT_VAR |
GPT_VAR_NOINIT | GPT_CONST |
GPT_APPL_CODE |
GPT_PBCFG |
|
|---|---|---|---|---|---|---|
GPT_START_SEC_VAR_INIT_UNSPECIFIED (.data) |
x |
|||||
GPT_STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
|||||
GPT_START_SEC_CODE (.text) |
x |
|||||
GPT_STOP_SEC_CODE |
x |
|||||
GPT_START_SEC_VAR_NO_INIT_UNSPECIFIED (.bss) |
x |
|||||
GPT_STOP_SEC_VAR_NO_INIT_UNSPECIFIED |
x |
|||||
GPT_START_SEC_CONST_UNSPECIFIED(.rodata) |
x |
|||||
GPT_STOP_SEC_CONST_UNSPECIFIED |
x |
|||||
GPT_START_SEC_ISR_CODE (.text) |
x |
|||||
GPT_STOP_SEC_ISR_CODE |
x |
|||||
GPT_START_SEC_CONST_PTR (.rodata) |
x |
|||||
GPT_STOP_SEC_CONST_PTR |
x |
|||||
GPT_START_SEC_VAR_INIT_PTR (.data) |
x |
|||||
GPT_STOP_SEC_VAR_INIT_PTR |
x |
|||||
For application code used by GPT (like callback functions) |
x |
|||||
4.12.11. Memory footprint¶
Please refer Memory Footprint for more details.
4.12.12. Performance¶
Not Applicable
4.12.13. Example Usage¶
4.12.13.1. Steps to build and run example¶
GPT example application demonstrates the MCAL GPT driver features, which is referred from folder <MCAL_ROOT>/examples/Gpt.
This application can be built from the build folder by giving “gmake –s gpt_app PLATFORM=am263”.
Once the build is completed we get a binary file,which is loaded in our controller and executed.
4.12.13.2. Document external set up Information¶
None
4.12.13.3. Flow of the example application¶
After initialization of timer followed by starting of timer, a channel waits until the interrupt is received. Interrupt indicates that 2sec is completed for respective channel.
After receiving interrupt notification, it stops the current channel and starts next channel to execute the same process.
The provided example application of GPT is configured with a preload value of 1 which equates to around 10ns/tick for a 200 MHz RTI Clock input.
4.12.13.4. Configuration used to test this example¶
In Example program,total 12 channels are configured in AM263x.
Channels 5, 6, 9, 12, 13, 16 are configured in Continuous mode in AM263x
Channels 7, 8, 10, 11, 14, 15 are configured in one-shot mode in AM263x
Channels 1, 2, 3, 4 are not configured as RTI0 timer is being used for delay and OS counter purpose.
Each channel is configured to run for 2sec.
If preload is set as ‘1’ in configuration with 200 MHz RTI Clock input and if expected timer for each channel shall run for 1sec.
Then, Tick frequency = (200*10^6)/(1+1)
Tick frequency = 100MHz = 10ns
So,for every 10ns, counter will increase by 1.
For getting 1Sec delay timer should count upto 1sec/10ns times. i.e, 100*10^6 times.
So, 0x05F5E100 shall be passed to Gpt_StartTimer to produce 1sec delay.
4.12.13.5. Example Logs¶
AM263x
GPT_APP: Sample Application - STARTS !!!
GPT MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 100
SW Major Version : 9
SW Minor Version : 0
SW Patch Version : 0
----------------------------------------------------------------------------------
GPT_APP: GPTIMER Test Configuration
----------------------------------------------------------------------------------
Initializing channels
Post-Build variant is being used ..
------------------------------------------
GPT_APP: Running GPT Test for channel 4
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 4f
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 5 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27be4a
GPT_APP: Time Remaining Value = 0xba07231
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =4 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 5
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 6 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27be02
GPT_APP: Time Remaining Value = 0xba07287
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =5 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 6
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 7 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =6 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 7
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 8 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =7 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 8
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 9 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27bdfa
GPT_APP: Time Remaining Value = 0xba0728c
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =8 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 9
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 10 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =9 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 10
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 11 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =10 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 11
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 12 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27e00d
GPT_APP: Time Remaining Value = 0xba05080
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =11 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 12
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 13 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27e014
GPT_APP: Time Remaining Value = 0xba05075
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =12 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 13
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 14 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =13 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 14
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 15 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0xbebc200
GPT_APP: Time Remaining Value = 0x0
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =14 !!!
------------------------------------------
GPT_APP: Running GPT Test for channel 15
------------------------------------------
GPT_APP: Starting timer for 2 s
GPT_APP: Time Elapsed Value = 23
GPT_APP: Enable channel notification for this channel
GPT_APP: Wait for notification(approx. 2 seconds)
GPT_APP: GPT Test Notification Receiver channel 16 :)!!!
GPT_APP: Disable channel notification for this channel
GPT_APP: Wait till timer overflows, no notification should be received
GPT_APP: Time Elapsed Value = 0x27e011
GPT_APP: Time Remaining Value = 0xba0507e
Waiting for timer to overflow
Overflow happened no notification received
GPT_APP: Stop timer
GPT Test Passed for channel =15 !!!
GPT Test Passed for configuration!!
GPT Test Completed, njoy life!!!
GPT_APP: Sample Application - DONE !!!
GPT Stack Usage: 832 bytes
GPT Test Passed!!!
4.12.14. FAQ’s¶
None
4.12.15. Test Report (Link to test report)¶
Will be updated in future release.
4.12.16. References¶
Autosar SWS 4.3.1 will be updated in future release.
4.12.17. Disclaimer¶
Will be updated in future release.