4.11. FLS¶
4.11.1. About This Document¶
Document Title |
User Guide of MCAL FLS Driver |
Document Version |
Version 1.2 |
Company |
Texas Instruments |
Document Name |
AUTOSAR FLS User Guide |
4.11.2. Document Revision History¶
Version |
Date |
Revision History |
Status |
|---|---|---|---|
Version 1.0 |
26 April 2022 |
Initial Version |
Approved |
Version 1.1 |
30 June 2022 |
Version |
Approved |
Version 1.2 |
25 Aug 2023 |
Document release version column removed |
Approved |
4.11.3. Table of contents¶
4.11.4. Acronyms and Definitions¶
Acronyms and Definitions used are presented in below table.
Acronyms |
Descriptions |
|---|---|
BSW |
Basic Software |
DET |
Default Error Tracer |
FLS |
Flash Driver |
MCU |
Micro Controller Unit |
OS |
Operating System |
API |
Application Programming Interface |
HW |
Hardware |
SW |
Software |
4.11.5. Functional Overview¶
4.11.5.1. Brief Overview¶
This document describes MCAL FLS Driver functionality, its application interfaces and configuration details as per AUTOSAR version 4.3.1 .
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Pre-Compile, Post-build |
Vendor ID |
FLS_VENDOR_ID (44) |
Module ID |
FLS_MODULE_ID (92) |
Supported Platform |
AM263x |
The Flash Driver provides services for reading, writing, erasing flash memory for external Flash device.
4.11.5.1.1. FLS Driver Architecture¶
The FLS driver has architecture as shown in below figure from the AUTOSAR specification.
Figure 1: FLS in AUTOSAR architecture.
The below figure shows typical connection of the QSPI module to the external quad-SPI flash memory
Figure_2: QSPI connected to an external Quad SPI flash memory
4.11.5.1.2. Initialization¶
The driver FLS is initialized by calling Fls_Init() function and takes FlsConfigSet as input and Initializes Flash and QSPI. This will also make driver status to IDLE.
4.11.5.1.3. States¶
The Fls driver maintains states for:
MEMIF_UNINIT -> This is the state when hardware is not initialized.
MEMIF_IDLE -> when FLS driver initialized, it will go to IDLE state.
MEMIF_BUSY: In case of any on-going operation i.e., Erase OR read OR write, the state will be maintained as busy until the operation is completed.
MEMIF_BUSY_INTERNAL is not supported.
4.11.5.2. Features Supported and Not Supported¶
AUTOSAR features:
Supported |
Not Supported |
|---|---|
Only one QSPI instance will support |
Only one instance of Fls module supported at one time. |
Perform storage mode applications
|
Access To Address beyond 8MB is not supported in MemMap mode. |
Configure error detection (DET) |
DMA mode not supported |
Only normal mode is supported. |
Relevant features not supported
|
4.11.5.3. IP Specific features:¶
None
4.11.5.4. Assumptions¶
None
4.11.5.5. Limitations¶
Only 1S-1S-4S mode is supported for QSPI.
4.11.5.6. Design overview (Link to the Architecture document and Design Document)¶
Will be available in future release.
4.11.5.7. File Structure¶
Description of static files is provided below:
Static source and header files |
Description |
|---|---|
Fls.c |
Contains the pre-complier switches. |
Fls.h |
Contains the APIs of the FLS driver to be used by upper layers. |
Fls_Irq.h |
Contains ISR function definitions |
Fls_Cfg.c |
Contains device specific a function definition, data types and definations. |
Fls_NOR_<flash_device>.h |
Contains device specific configuration parameters. |
Fls_Brd_Nor_Qspi.c |
Contains internal functions and data structures. |
Fls_Qspi.c |
Contains internal functions and data structures. |
Fls_Brd_Nor.h |
Contains internal functions and data structures. |
Fls_Qspi.h |
Contains internal functions and data structures. |
Description of generated files is provided below:
Plugin Files |
Descriptions |
|---|---|
Fls_Cfg.h |
Contains the pre-complier switches. |
Fls_PBcfg.c |
Contains all Post-Build Configured parameters. |
Fls_Cfg.c |
Contains all Pre-Compile Configured parameters. |
Figure 4: FLS header file include structure
4.11.6. Deviations to requirements (Requirement Traceability)¶
4.11.6.1. Module Requirements¶
Will be updated in future release
4.11.6.2. Deviation of requirements against AUTOSAR specification requirements¶
Will be updated in future release
4.11.7. Integration Details¶
4.11.7.1. Dependency on Other Software Modules¶
4.11.7.1.1. The FLS Driver dependent modules¶
4.11.7.1.1.1. MCU¶
The Fls Modules expects the MCU modules to enable the QSPI clock through the configuration. Required parameter for clock enabling:
Module ID: MCU_CLKSRC_MODULE_ID_QSPI
Source ID: MCU_CLKSRC_4
Divider value: 4
4.11.7.1.2. PORT¶
The Fls Modules expects that pinmux is set correctly to configure the Data line, Chip select and Clock pins for QSPI module. This is done by the PORT driver.
4.11.7.1.3. MemIf¶
This implementation depends on MemIf module and uses its imported types such as MemIf_JobResultType, MemIf_ModeType and MemIf_StatusType.
4.11.7.1.4. Fee¶
This implementation depends on Fee module for callback notification to notify the module environment about job end and job error.
4.11.7.1.5. Error Handling module¶
4.11.7.1.6. DET¶
The module FLS depends on the DET (by default) in order to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch FLS_DEV_ERROR_DETECT = STD_ON in the Fls_Cfg.h
The following table represents the service IDs:
Service ID |
code |
Service |
|---|---|---|
FLS_SID_INIT |
0x00 |
Fls_Init |
FLS_SID_ERASE |
0x01 |
Fls_Erase |
FLS_SID_WRITE |
0x02 |
FLS_Write() |
FLS_SID_CANCEL |
0x03 |
FLS_Cancel() |
FLS_SID_GET_STATUS |
0x04 |
FLS_GetStatus() |
FLS_SID_GET_JOB_RESULT |
0x05 |
Fls_GetJobResult() |
FLS_SID_READ |
0x07 |
FLS_Read() |
FLS_SID_COMPARE |
0x08 |
FLS_Compare() |
FLS_SID_GET_VERSION_INFO |
0x10 |
Fls_GetVersionInfo() |
FLS_SID_BLANK_CHECK |
0xA |
FLS_BlankCheck() |
FLS_SID_MAIN_FUNCTION |
0x06 |
FLS_MainFunction() |
The errors reported to DET module are described in the following table:
Error Code |
Error Macro |
Description |
|---|---|---|
[0x01] |
FLS_E_PARAM_CONFIG |
API service called with wrong parameter |
[0x02] |
FLS_E_PARAM_ADDRESS |
API service called with wrong parameter |
[0x03] |
FLS_E_PARAM_LENGTH |
API service called with wrong parameter |
[0x04] |
FLS_E_PARAM_DATA |
API service called with wrong parameter |
[0x05] |
FLS_E_UNINIT |
API service used without module initialization |
[0x06] |
FLS_E_BUSY |
API called when module is busy |
[0x0A] |
FLS_E_PARAM_POINTER |
API called with a Null Pointer |
The run time errors reported to DET module are described in the following table:
Error Code |
Error Macro |
Description |
|---|---|---|
[0x07] |
FLS_E_VERIFY_ERASE_FAILED |
Erase verification (blank check) failed |
[0x08] |
FLS_E_VERIFY_WRITE_FAILED |
Write verification (compare) failed |
AUTOSAR requires that API functions check the validity of their parameters. The check in below table shows the various Development Error Reporting: Assignment of checks to services are internal parameter checks of the API functions. These checks are for development error reporting and can be enabled or disabled. The following table shows which parameter checks are performed on which services:
Check Services |
FLS_E_PARAM_CONFIG |
FLS_E_PARAM_ADDRESS |
FLS_E_PARAM_LENGTH |
FLS_E_PARAM_DATA |
FLS_E_UNINIT |
FLS_E_BUSY |
FLS_E_PARAM_POINTER |
|---|---|---|---|---|---|---|---|
Fls_Init |
x |
x |
|||||
Fls_Erase |
x |
x |
x |
x |
|||
Fls_Read |
x |
x |
x |
x |
x |
||
Fls_Write |
x |
x |
x |
x |
x |
||
Fls_Compare |
x |
x |
x |
x |
x |
||
Fls_BlankCheck |
x |
x |
x |
x |
|||
Fls_GetJobResult |
x |
||||||
Fls_GetVersionInfo |
x |
||||||
Fls_MainFunction |
x |
||||||
Fls_Cancel |
x |
4.11.7.1.6.1. DEM¶
FLS modules does not report DEM errors.
4.11.7.1.7. Callback Functions¶
The FLS driver does not provide any call back functions.
4.11.7.2. Main Functions¶
The function Fls_MainFunction perform the processing of the flash read, write, erase and compare jobs. When a job has been initiated, the FLS module’s environment shall call the function Fls_MainFunction cyclically until the job is finished.
4.11.7.3. Fls Set Erase Function¶
This function is called from example app based on the macros enabled in application itself. Implementation of this function is done to allow user to select one or more erase types based on the requirement. The function Fls_SetEraseType sets the parameters like data size, data_value, erase type(sector/block/chip), “typeoferase” for Fls_DrvObj, based on the erase type parameter passed to this function while calling from example app. These parameters are required in example app.
4.11.7.4. Callback Notification¶
Notifications:
This implementation depends on Fee module for callback notification to notify the module environment about job end and job error
4.11.7.5. Scheduling Strategy¶
4.11.7.5.1. SchM¶
This implementation requires one level of exclusive access to guard critical sections. Invokes SchM_Enter_Fls_FLS_EXCLUSIVE_AREA_0 (), SchM_Exit_Fls_FLS_EXCLUSIVE_AREA_0 () to enter critical section and exit.
4.11.7.5.2. Critical Sections¶
There is only one critical section in this driver. Within these sections all read /modify / write accesses to internal FLS status variables must be protected. Therefore, switching to tasks that also access FLS must be avoided and all FLS interrupts must be suspended. This is managed internally by Fls Driver
4.11.8. API Description¶
4.11.8.1. Description of the API’s (Can be referred to Api Guide spec)¶
Refer the AUTOSAR SWS for API documentation and Type definition.
4.11.8.2. API’s with Service ID¶
The following table presents the service IDs and the related services:
Autosar API’s Supported:
Service ID |
Service |
|---|---|
0x00 |
Fls_Init |
0x01 |
Fls_Erase |
0x02 |
FLS_Write |
0x03 |
FLS_Cancel |
0x04 |
FLS_GetStatus |
0x05 |
Fls_GetJobResult |
0x07 |
FLS_Read |
0x08 |
FLS_Compare |
0x10 |
Fls_GetVersionInfo |
0x0A |
FLS_BlankCheck |
0x06 |
FLS_MainFunction |
Autosar API’s not Supported:
Service ID |
Service |
|---|---|
0x09 |
Fls_SetMode |
Refer Autosar SWS for API description mentioned in above table.
4.11.9. Configuration Description¶
4.11.9.1. Configuration Variants¶
The Fls can be configured as Post-Build or Pre-Compile variant, using EB tresos tool.
Variants |
Generated Files |
|---|---|
PostBuild |
Fls_PBcfg.c , Fls_Cfg.h |
Pre-Compile |
Fls_Cfg.c , Fls_Cfg.h |
4.11.9.2. Parameter Description¶
Will be updated in future release
4.11.9.3. Configuration rules and constraints to enable plausibility checks¶
Will be updated in future release
4.11.10. Memory Mapping¶
Memory Mapping Sections |
Compiler Abstraction Definitions |
|||
|---|---|---|---|---|
FLS_CODE |
FLS_CODE_ISR |
FLS_VAR_NO_INIT |
FLS_CFG |
|
FLS_START_SEC_ISR_CODE (.text) |
x |
|||
FLS_STOP_SEC_ISR_CODE |
||||
FLS_START_SEC_VAR_NO_INIT_UNSPECIFIED (.data) |
x |
|||
FLS_STOP_SEC_VAR_NO_INIT_UNSPECIFIED |
||||
FLS_START_SEC_CODE(.text) |
x |
|||
FLS_START_SEC_CODE |
||||
FLS_START_SEC_CONFIG_DATA (.data) |
x |
|||
FLS_STOP_SEC_CONFIG_DATA |
4.11.11. Memory footprint¶
Please refer Memory Footprint for more details.
4.11.12. Performance¶
Will be updated in future release
4.11.13. Example Usage¶
4.11.13.1. Steps to build and run example¶
FLS example application demonstrating the MCAL Fls driver features is in folder <MCAL_ROOT>/examples/Fls.
This application can be built from the root folder by giving gmake –s fls_app PLATFORM=am263.
after the build is completed we get a binary file,which is loaded in our controller and executed.
4.11.13.2. Example Logs¶
[HSM_CLIENT] New Client Registered with Client Id = 0
Starting QSPI Bootloader ...
[BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 80.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size : 219 KB
[BOOTLOADER_PROFILE] Cores present :
r5f0-0
[BOOTLOADER PROFILE] System_init : 304us
[BOOTLOADER PROFILE] Drivers_open : 82us
[BOOTLOADER PROFILE] LoadHsmRtFw : 8768us
[BOOTLOADEFLS_APP: Job Ends: SUCCESS
FlsApp: Sample Application - STARTS !!!
FLS CHIP ERASE !!!
FLS_APP: Variant - Pre Compile being used !!!
FLS MCAL version info:8.6.2
FLS MCAL Module/Driver:92.44
FLS_APP: DATA SIZE TEST is 0x10000
FLS_APP: Offset is 0x0
FLS_APP: Erasing
FLS_APP: Erasing full chip..please wait..
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Blank Checking
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Writing
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Reading
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Write Compare
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Read Compare
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP:
FLS_APP: Job Cancel
FLS_APP: 1. Writing
FLS_APP: 2. Canceling
FLS_APP: Job Canceled (SUCCESS) !
FLS_APP:
FLS_APP:
FLS_APP: ---------- FLS Sample application Done !! ----------
FLS_APP:
4.11.14. FAQ’s¶
None
4.11.15. Test Report (Link to test report)¶
Will be updated in future release
4.11.16. References¶
Autosar SWS 4.3.1 will be updated in future release.
4.11.17. Disclaimer¶
Will be updated in future release