4.8. PORT¶
4.8.1. About This Document¶
Document Title |
User Guide of MCAL PORT Driver |
Document Version |
Version 1.0 |
Company |
Texas Instruments |
Document Name |
PORT User Guide |
4.8.2. Document Revision History¶
Version |
Date |
Revision History |
Status |
|---|---|---|---|
Version 1.0 |
13 Oct 2023 |
Initial Version |
Approved |
4.8.3. Table of contents¶
4.8.4. Acronyms and Definitions¶
Acronyms and Definitions used are presented in below table.
Acronyms |
Descriptions |
|---|---|
BSW |
Basic Software |
DET |
Default Error Tracer |
ADC |
Analogue Digital Converter |
MCU |
Micro Controller Unit |
OS |
Operating System |
API |
Application Programming Interface |
HW |
Hardware |
SW |
Software |
4.8.5. Functional Overview¶
4.8.5.1. Brief Overview¶
This document describes MCAL PORT Driver functionality, its application interfaces and configuration details as per AUTOSAR version 4.3.1 .
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Pre-Compile, Post-build |
Vendor ID |
PORT_VENDOR_ID (44) |
Module ID |
PORT_MODULE_ID (124) |
Supported Platform |
AM263px |
PORT module shall provide the service for initializing the whole PORT structure of the microcontroller. This driver specification is applicable for on-chip ports and port pins.
4.8.5.1.1. PORT Driver Architecture¶
The following figure shows where the PORT is located in the AUTOSAR architecture
Figure 1: PORT in AUTOSAR architecture.
4.8.5.1.2. Initialization¶
Port_Init API initializes the PORT driver and does pin configuration of specified PORT PIN Id’s. Port_Init also enables all pins for specified module selected in the config structure passed to Port_Init.
4.8.5.1.3. States¶
No state is maintained in the PORT driver.
4.8.5.2. Features Supported and Not Supported¶
AUTOSAR features:
IP Supported Features |
AUTOSAR Supported Features |
Not Supported |
|---|---|---|
Configuring the pins for rising and/or falling edge, specified for each GPIO pin. |
The PORT Driver module shall initialize the whole port structure of the microcontroller. |
None |
Configuring the GPIO signal conditioning chain
|
The PORT Driver module shall allow the configuration of different functionality for each port and port pin. e.g. ADC, SPI, DIO etc. |
None |
Enabling all pins of specified peripheral for given mode of operation. This option provides a way configuring all pins for a peripheral for required mode of operation. |
The PORT Driver module shall provide additional configurations for the MCU port/port pins:
|
None |
The PORT Driver module shall provide a number of optional configurations for the MCU ports and port pins (if supported by hardware):
|
None |
4.8.5.3. Assumptions¶
None
4.8.5.4. Limitations¶
The Pins which are configured as GPIO, the parameter “PortInputOverrideCtrl” and “PortOutputOverrideCtrl” should be as disabled.
Figure 2:Configuration settings.
4.8.5.5. Design overview (Link to the Architecture document and Design Document)¶
Will be available in future release.
4.8.5.6. File Structure¶
Description of static files is provided below:
Static source and header files |
Description |
|---|---|
Port.h |
Contains the API’s of the PORT driver to be used by upper layers. |
Port.c |
Contains the implementation of the API’s for PORT driver. |
Port_Priv.c |
Contains Internal functions definition of PORT driver. |
Port_Priv.h |
Contains Internal functions declaration of PORT driver. |
Description of generated files is provided below:
Plugin Files |
Descriptions |
|---|---|
Port_Cfg.h |
Contains the Precompile switches, Symbolic names of PortPin. |
Port_PBcfg.c |
Contains all pins Post-Build Configured parameters |
Port_Cfg.c |
Contains all pins Pre-Compile Configured parameters |
Figure 4: PORT header file include structure
4.8.6. Deviations to requirements (Requirement Traceability)¶
4.8.6.1. Module Requirements¶
Will be updated in future release
4.8.6.2. Deviation of requirements against AUTOSAR specification requirements¶
Will be updated in future release
4.8.7. Integration Details¶
4.8.7.1. Dependency on Other Software Modules¶
PORT driver doesn’t depend on other peripheral drivers
4.8.7.1.1. Error Handling module¶
4.8.7.1.1.1. DET¶
The module PORT depends on the DET (by default) in order to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch PORT_DEV_ERROR_DETECT = STD_ON in the Port_Cfg.h
AUTOSAR requires that API functions shall check the validity of their respective parameters. These checks are for development error reporting and can be enabled or disabled.
The errors reported to DET module are described in the following table:
Error Code |
Error Macro |
Description |
|---|---|---|
[0x0A] |
PORT_E_PARAM_PIN |
Invalid Port Pin ID requested |
[0x0B] |
PORT_E_DIRECTION_UNCHANGEABLE |
Port Pin not configured as changeable |
[0x0C] |
PORT_E_INIT_FAILED |
API Port_Init service called with wrong parameter. |
[0x0D] |
PORT_E_PARAM_INVALID_MODE |
API Port_SetPinMode service called when mode is unchangeable. |
[0x0E] |
PORT_E_MODE_UNCHANGEABLE |
API Port_SetPinMode service called when mode is unchangeable. |
[0x0F] |
PORT_E_UNINIT |
API service called without module initialization |
[0x10] |
PORT_E_PARAM_POINTER |
APIs called with a Null Pointer |
The run time errors reported to DET module are described in the following table:
4.8.7.1.1.2. DEM¶
There are no DEM errors.
4.8.7.1.1.3. Callback Notification¶
There are no Callback Notifications.
4.8.7.2. Hardware - Software - ISR API name mapping¶
The PORT module doesn’t have interrupt service routines.
4.8.7.3. Scheduling Strategy¶
4.8.7.3.1. SchM¶
Beside the OS the BSW Scheduler provides functions that module PORT calls at begin and end of critical sections.
4.8.7.3.2. Critical Sections¶
There is only one kind of critical sections in this driver. Within these sections all read /modify / write accesses to internal MCU status variables must be protected. This is handled internally in the driver by invoking SchM_Enter_Port_PORT_EXCLUSIVE_AREA_0()/SchM_Exit_Port_PORT_EXCLUSIVE_AREA_0().
4.8.8. API Description¶
4.8.8.1. Description of the API’s (Can be referred to Api Guide spec)¶
Refer the AUTOSAR SWS for API documentation and Type definition.
4.8.8.2. List of API’s¶
The following table presents the list of API’s:
Service ID |
Autosar API’s Supported Service |
Autosar API’s not Supported Service |
|---|---|---|
0x00 |
Port_Init |
|
0x01 |
Port_SetPinDirection |
|
0x02 |
Port_RefreshPortDirection |
|
0x03 |
Port_GetVersionInfo |
|
0x04 |
Port_SetPinMode |
Refer Autosar SWS for API description mentioned in above table.
4.8.8.3. Description on Non Standard API’s¶
Port_DeInit API
This function is Non- Autosar based and is used to de-initialize port module.
4.8.9. Configuration Description¶
4.8.9.1. Configuration Variants¶
The PORT can be configured as Post-Build or Pre-Compile variant, using EB tresos tool.
Variants |
Generated Files |
|---|---|
PostBuild |
Port_PBcfg.c , Port_Cfg.h |
Pre-Compile |
Port_Cfg.c , Port_Cfg.h |
4.8.9.2. Parameter Description¶
Will be updated in future release
4.8.9.3. Symbolic Names deviations¶
None.
4.8.9.4. Configuration rules and constraints to enable possibility checks¶
Will be updated in future release
4.8.10. Memory Mapping¶
Memory Mapping Sections |
PORT_CODE |
PORT_VAR_ZERO_INIT |
PORT_PBCFG |
|---|---|---|---|
PORT_START_SEC_VAR_INIT_UNSPECIFIED (.data) |
x |
||
PORT_STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
||
PORT_START_SEC_CODE (.bss) |
x |
||
PORT_STOP_SEC_CODE |
x |
||
PORT_START_SEC_CONFIG_DATA |
x |
||
PORT_STOP_SEC_CONFIG_DATA |
x |
4.8.11. Memory footprint¶
Please refer Memory Footprint for more details.
4.8.12. Performance¶
Not Applicable
4.8.13. Example Usage¶
4.8.13.1. Steps to build and run example¶
PORT example application demonstrating the MCAL PORT driver features is in folder <MCAL_ROOT>/examples/Port.
This application can be built from the root folder by giving gmake –s port_app PLATFORM=am263.
Once the build is completed we get a binary file, which is loaded in our controller and executed.
4.8.13.2. External set up Information¶
PORT module is tested using CC board (PROC111E2).
4.8.13.3. Configuration used to test this example¶
Pin configurations : Following pins are configured as a GPIO and used in example application to test.
Pin Ball Number |
Pin Signal Name |
|---|---|
C15 |
GPIOGH_120 |
4.8.13.4. Example Logs¶
CLANG compiled : portApp: Sample Application - STARTS !!!
Port Driver version info:8.6.2
Port Driver Module/Driver:124.44
Pin Value for channel 0 : 1
Dio_FlipChannel(channel_0)
Pin Value for channel 0 : 0
Dio_FlipChannel(channel_0)
Pin Value for channel 0 : 1
Pin Value for channel 0 : 0
Dio_FlipChannel(channel_0)
Pin Value for channel 0 : 0
PORT Test Passed!!!
4.8.14. FAQ’s¶
None
4.8.15. Test Report (Link to test report)¶
Will be updated in future release
4.8.16. References¶
Autosar SWS 4.3.1 will be updated in future release.
4.8.17. Disclaimer¶
Will be updated in future release.